How to avoid the financial loss due to power factor penalties when integrating solar power

This audio was created using Microsoft Azure Speech Services

I recently worked on the integration of solar production into a small industrial building project. In the process, I discovered an interesting fact: The integration of solar production can have a negative impact on the overall power factor (PF) of the electrical installation and may lead to penalties if corrective measures are not taken.

On this particular project, before the installation of the solar production the power factor was averaging 0.96, which is above the minimum value of 0.93 fixed by the energy provider. But by integrating solar production, the power factor decreased significantly, to 0.8, which is much lower than the defined threshold. In fact, because the solar system was producing and providing active energy only, less active energy was required from the grid for the same amount of reactive energy. Because power factor is defined as the ratio between the active power and the total power, when the active power demand from the grid went down, the power factor for the grid connection decreased accordingly.

Cost of Power Factor

Solutions to power factor penalties due to solar production

However, there is an easy way to avoid power factor penalties when integrating solar production that does not require installing additional power factor correction equipment. By regulating the inverter set point, the solar inverters can provide not only active but also some reactive power. This regulation can be arranged through power measurements at the photovoltaic installation and at the connection point to the grid using a control system that calculates and communicates the appropriate set point value to the inverters.

In the example above, a minimal reduction of the active power produced by the solar system enabled the global power factor of the electrical installation to be raised to the expected value.

Power Factor

At Schneider Electric, we have developed an algorithms-based solution that enables correction of the power factor rapidly and with high accuracy. This patented methodology provides the optimal operating point of the solar production system regarding the power factor of the electrical installation.

To learn more about the impact of solar integration on power factor, watch “How to avoid power factor penalties due to photovoltaic production.” This short explanation is part of a new series of videos prepared by Schneider Electric’s technical communication group.

An overview of the series and a full playlist is also available.

Learn more on electrical installation design for installations with local production in Chapter P of the Electrical Installation Guide.

Tags: , , , , ,

Conversation

  • Saeed Ahmed

    5 years ago

    A nice video. With nice explanation and example.

  • Waqas Khan

    4 years ago

    I learned a lot from your article. A very valuable experience.

  • Patrick Kobou Ngani

    4 years ago

    Thank you for the very informative article.
    I’m from the university of Luxembourg and my group is developing a similar solution in order to locally improve the hosting capacity of the grid. We would like to know what you think about our solution. how can we best discuss about it?
    Best regards

Comments are closed.