Improve reliability by modernizing switchgear in low and medium voltage networks

Do you have a strategy for modernizing or replacing your aging Low Voltage and Medium Voltage electrical switchgear?

A reliable, safe, easily maintainable power network is more crucial than ever because downtime can cost millions of euros per hour. Proper switchgear and switchboard maintenance combined with modernization can aid in improving reliability.

Keep in mind, modernizing and upgrading your low voltage and medium voltage switchgear equipment doesn’t have to mean demolishing the existing infrastructure. You can choose to replace the existing electrical installation with new equipment or you can pinpoint where you will benefit from upgrades, retrofitting, or modernization, which generally are more cost-effective and less disruptive than buying new equipment.

How can you update your switchgear infrastructure and why would you want to?

There are many issues to consider, including the following:

  • Safety: Electrical switchgear failure, which is more likely with older equipment, can cause serious injuries and damage.
  • Switchgear lifespan: The switchgear lifespan has been extended from 10-30 years, on average, to sometimes up to 50-60 years like in nuclear plants, but industry standards and technology offerings are evolving at a faster rate. This challenges companies to modernize an antiquated system while ensuring reliability.
  • Cost savings: Modernizing existing electrical switchgear, rather than replacing it, will save both physical equipment costs as well as time and labor.
  • Maintenance costs: Maintenance costs and the risk of product failure rise as the product ages. You may be able to reduce maintenance costs by modernizing.
  • Spare parts availability: The availability of spare parts must be examined. If spare parts are no longer readily available, it may be time to modernize.
  • Urgency of modernization: The criticality of the affected processes must be assessed and prioritized when determining what needs to be modernized.
  • Improved reliability: Reliability is key for cost savings and preventing downtime.
  • Technology and improved capabilities: New technology provides more capabilities, better performance, and reduced maintenance requirements.
  • Workflow disruption: Consider the cost and inconvenience of downtime. It is possible for modernization to be performed with minimal downtime and production stoppage.
  • Capital costs: Although long-term cost savings can be anticipated, it is also important to consider the sometimes substantial capital costs.

Consider areas where your business needs to improve and if modernizing your switchgear can help you reach those goals while also becoming more reliable.

Tags: , , , , ,

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.