Zencelo Switch for Your Modern Home

Zencelo Switch is one of the Schneider Electric’s top-range switches. It is the world’s first full-flat switch designed aesthetically to perfection. The product’s Simplicity and Clean design are the two features that catches the eye.

One can now buy this switch from Schneider Electric’s e-commerce platform. Iso-motionpress or Impress—the patented mechanism enables the switch dolly to remain static, during On and Off. Thereby, filling a smaller space on the wall.

The Zencelo range is corrosion resistant, heat resistant and impact resistant. These full-flat switches are built for those who use electromechanical switches.

These switches will add an elegant touch to your home walls. Check out the complete range of switches and sockets here.

#schneiderelectric