Anilesh Kaduthanum
Anilesh Kaduthanum
Senior Principal, Offer Compliance - New Energy Landscape
Anilesh Kaduthanum holds a Bachelor’s degree in EEE from Mysore University. With over 25 years of experience in the field of LV switchgear, Anilesh has multiple papers, case studies, and 2 patents in his name.
Having worked with organizations like L&T and Schneider Electric, Anilesh has handled various projects covering switchgear, control gears, switchboards, fuses, and microgrid inverters for design & certifications.
Anilesh is a member of the BIS ET07 technical committee and represents IEC SC23E WG1 and WG2 as an expert from India. He has been deeply involved in driving the Aluminum Task Force set up under SC121A WG2, which was...
Show more
Show less
biography for Anilesh Kaduthanum
Anilesh Kaduthanum holds a Bachelor’s degree in EEE from Mysore University. With over 25 years of experience in the field of LV switchgear, Anilesh has multiple papers, case studies, and 2 patents in his name.
Having worked with organizations like L&T and Schneider Electric, Anilesh has handled various projects covering switchgear, control gears, switchboards, fuses, and microgrid inverters for design & certifications.
Anilesh is a member of the BIS ET07 technical committee and represents IEC SC23E WG1 and WG2 as an expert from India. He has been deeply involved in driving the Aluminum Task Force set up under SC121A WG2, which was instrumental in developing and proposing the introduction of usage of aluminum conductors as an alternate of copper inside IEC 60947 series of standard. Anilesh meets with various consultants, partners, and specifiers to showcase the importance of compliance to Indian/International Standards and the safety benefits it brings to the end customers.
Additionally, he is a certified internal auditor for ISO 17025, a certified ASTA Observer, and a recognized Expert under the Schneider Electric Electrifier Program.
In his current role, Anilesh is responsible for conformity assessment for New Energy Landscape solutions from Schneider Electric globally. His passions include venturing into new technologies driving LV protection products and standardization.
Articles
Zone Selective Interlocking (ZSI) – The intelligent way for right protection

Zone Selective Interlocking (ZSI) – The intelligent way for right protection
- 4 min read
- Rachna Verma & Anilesh Kaduthanum
Bloggers you may also like
Schneider Electric India

Schneider Electric India
Most recent post: Liquid cooling and approval readiness for a sustainable data centre in India
Guest Blogger

Guest Blogger
Most recent post: Cooling orchestration software: A welcome addition to AI data center operations
Robert Cain

Robert Cain
Most recent post: The mission continues: How veterans and military spouses are building careers at Schneider Electric