Zone Selective Interlocking (ZSI) – The intelligent way for right protection

Imagine a fault occurs in your electrical distribution system. Your first instinct is simple: clear the fault as quickly as possible.

After all, faster fault clearing means:

  • Lower thermal stress on cables
  • Reduced mechanical forces on equipment
  • Less damage to the network
  • Improved personnel safety

In a modern electrical distribution system, speed is only half the story. The real challenge is balancing fault protection with continuity of power. Nobody wants an entire plant or data center to lose power because of a fault on a single feeder. This is why engineers use selective coordination, where only the circuit breaker closest to the fault trips while the rest of the system remains energized.

Traditionally, this is achieved using combinations of Current & Time discrimination. These methods work exceptionally well…until a very specific situation occurs.

Consider the arrangement below.

Suppose a short-circuit occurs in between circuit breakers CB1 and CB2 as shown.

A graph showing a short-circuit occurring between two circuit breakers, labelled CB! and CB2.

Because CB1 has been intentionally programmed with a time delay to maintain selectivity with downstream breakers, it patiently waits before tripping.

Unfortunately, the fault isn’t waiting.

During those extra milliseconds:

  • Fault current continues flowing
  • Equipment experiences higher thermal and electrodynamic stress
  • Arc-flash energy increases
  • Cable damage becomes more severe
  • Equipment life is reduced

Ironically, the breaker closest to the fault is the one waiting the longest. Wouldn’t it be better if CB1 immediately knew there was no downstream breaker capable of clearing the fault? That’s exactly what Zone Selective Interlocking (ZSI) does.

The magic behind ZSI

Instead of relying only on preset time delays, ZSI allows electronic trip units to communicate with one another. Using two simple pilot wires, upstream and downstream circuit breakers continuously exchange information.

Think of it as a conversation between breakers.

Downstream breaker: “I’ve detected the fault. Stay back—I will handle it.”

Upstream breaker: “Understood. I’ll wait and act only if you don’t.”

This simple exchange changes everything.

How ZSI works

Each electronic trip unit has two communication signals.

ZSI output

When the breaker detects a short circuit or earth fault:

  • HIGH → Fault detected; sends a restraint signal upstream.
  • LOW → No fault detected.

ZSI input

The breaker listens to downstream devices.

  • HIGH → A downstream breaker has detected the fault, so apply the programmed time delay.
  • LOW → No downstream breaker has claimed the fault, so trip immediately.

What happens during a fault?

Case 1 – Fault downstream of CB2

  • CB2 detects the fault and immediately sends a HIGH signal to CB1.
  • CB1 receives the restraint signal and intentionally delays its trip.

CB2 clears the fault instantly. Only the affected feeder is disconnected. The rest of the system continues operating.

Exactly what selective coordination is designed to achieve.

Case 2 – Fault in between CB1 and CB2

Now the fault is located between CB1 and CB2. CB2 never detects the fault. Therefore, no HIGH signal is sent upstream.

CB1 receives no restraint signal.

It immediately recognizes that the fault lies within its own protection zone and trips without waiting for its programmed delay.

The fault is cleared in the shortest possible time.

No unnecessary delay. No excessive fault energy. No compromise in system coordination. This is the real intelligence behind Zone Selective Interlocking.

In critical facilities such as data centres, hospitals, industrial plants, and commercial buildings, ZSI enables engineers to achieve what was once considered a trade-off: maximum protection without sacrificing power continuity.

Experimental validation of ZSI

To demonstrate how ZSI improves protection, we conducted a real laboratory experiment using two MasterPact MTZ ACB at our R&D Labs, Bangalore INDIA

Circuit BreakerModelRating (In)Trip UnitIrIiIsdtsd
ACB CB1 ‘A’ (Upstream)MTZ2-32 H23200 AMicrologic 7.0X0.5In (1600 A)2In (6400 A)2Ir (3200 A)100 ms
ACB CB2 ‘B’ (Downstream)MTZ1-16 H31600 AMicrologic 2.0X0.5In (800 A)–2Ir (1600 A)–

Test scenario

A graph showing that a 4000 A short-circuit fault was intentionally created at Point X, located between CB1 ‘A’ and CB2 ‘B’.

A 4000 A short-circuit fault was intentionally created at Point X, located between CB1 ‘A’ and CB2 ‘B’.

Experiment 1: Without ZSI

What happened?

  • CB1 ‘A’ detected the 4000 A fault.
  • However, because its short-time delay was set to 100 ms, it waited before tripping.
  • CB2 ‘B’ correctly remained closed since it did not detect the fault.

Observation

Although the fault was already identified, the network continued to experience fault current during the programmed delay period.

Result – Trip after approximately 100 ms

Experiment 2: With ZSI enabled

A picture showing an experiment where a 4000 A short-circuit fault was intentionally created between CB1 ‘A’ and CB2 ‘B’, with Zone Selective Interlocking enabled.

Now the same experiment was repeated after enabling Zone Selective Interlocking.

What happened?

  • CB1 ‘A’ detected the same 4000 A fault.
  • Since no downstream breaker requested a time delay, the ZSI logic automatically overrode the programmed 100 ms delay.
  • CB1 ‘A’ tripped immediately.
  • CB2 ‘B’ remained closed throughout the test.

Observation

Instead of waiting for the preset delay, the breaker operated in only 60 ms. The oscilloscope waveforms clearly demonstrate the impact of ZSI.

Oscilloscope waveforms showing the impact of Zone Selective Interlocking
With ZSI
Oscilloscope waveforms showing the impact without Zone Selective Interlocking
Without ZSI

At Schneider Electric, we offer a broad portfolio of LV Circuit Breakers equipped with ZSI.

  • MasterPact Air Circuit Breakers
    • with MicroLogic 2.0X, 5.0X, 6.0X, 7.0 X trip units
    • with MicroLogic 2.0A, 5.0A/P/H, 6.0A/P/H trip units
  • ComPacT Moulded Case Circuit Breakers
    • with MicroLogic 5.3E, 6.2E trip units

Zone Selective Interlocking isn’t simply another protection feature. It is a smarter way of thinking about protection. Rather than asking, “How fast can I trip?”

ZSI asks and ensures, “Which is the right breaker to trip—and how quickly should it respond?”

That small difference in philosophy makes an enormous difference in system reliability, equipment protection, and operational continuity.

Add a comment

All fields are required.