Don’t risk motor damage: 4 reasons to choose the right protection

Since their invention in the late 19th century, electric motors have become essential in our daily lives and industrial operations. From small appliances like coffee grinders to high-speed marvels such as Shinkansen bullet trains, motors power almost everything around us. While many people take motors for granted, industrial engineers and machine builders know that even a minor motor failure can cause costly downtime and disrupt operations. This is why motor protection is so important. Protecting motors from overloads, short circuits, and electrical faults ensures consistent performance, reduces maintenance costs, and extends equipment life.

Why motor protection circuit breakers are important

A common question is, “Why do we need a dedicated motor protection circuit breaker (MPCB)? Can’t a standard circuit breaker do the job?” Motors are different from general electrical loads. They experience high inrush currents, inductive loads, and thermal stresses that standard breakers are not designed to handle effectively. While Miniature Circuit Breakers (MCBs) are useful for general circuits. They cannot provide the specialized protection motors need, especially for motors under 15 kW, which make up about 80% of motors worldwide.

Choosing dedicated motor protection devices like MPCBs safeguards the motor against both overloads (thermal protection) and short circuits (magnetic protection). Unlike standard MCBs, MPCBs respond precisely to motor conditions, preventing damage, ensuring reliability, and maximizing lifespan. In the next sections, we will discuss four key reasons why MPCBs are the ideal choice for effective motor protection.

Now, let’s look at four important reasons that you should choose MPCBs for motor protection.

Benefits of using MPCBs for motor protection

1. Standards matter when it comes to circuit breakers

When comparing standards related to MCB and MPCB, it’s clear there are some important differences:

  • MPCBs are certified under IEC 60947-4, which is the relevant standard for motor protection. However, since they are fundamentally circuit breakers, they are also certified under IEC 60947-2.
  • MCBs are typically certified under IEC 60898-1 (residential applications), though many are also certified under IEC60947-2. This is an important point: IEC 60898 is not intended for industrial environments. For example, it defines ambient temperature as 30 ⁰C, which is far too low for a typical factory setting. Even if you did choose an MCB which is certified under the correct standard, MCBs have no compensation for ambient air temperatures – a feature that is standard with Schneider MPCBs. This can cause nuisance tripping, with all the associated costs of downtime.

2. Optimal short circuit performance

Now let’s look at the performance of the devices under a short-circuit. First, a C-curve MCB is designed to trip between 5-10 times the rated current, whereas MPCBs are designed to trip at 12 times the rated current. The first reaction of many people to this is that the C-curve MCB is more sensitive and therefore superior but let me explain why that’s not accurate.

You’re dealing with an induction motor for which you expect to see an initial surge of current 8-10 times the rated current, by design. That’s why the MPCB, which is specifically designed for this application, is designed to trip at higher currents – to avoid nuisance tripping. With the advent of high-efficiency IE3 and IE4 motors in the market, this problem is exacerbated as these motors have higher starting currents.

Some try to get around this by selecting the MCB based not on the rated current but on the trip current, i.e. they oversize the MCB to compensate. This can work to protect the motor from short-circuits but introduces issues under overload conditions, which I will discuss later.

A D-Curve MCB, on the other hand, will work for short-circuit protection. However, you can’t get a coordinated motor starter with any MCB, so it’s not a perfectly safe solution.

Second, the short-circuit breaking capacity of MCBs is generally restricted to 10 kA, which is often too low for industrial environments. Compare this with MPCBs that can offer up to 100 kA breaking capacity, which ensures that the motor starter and the motor remain safe and operable even in demanding conditions.

3. Overload performance

The most common faults that we see in motors are overload faults, accounting for over half the total motor failures worldwide. It’s here that the MPCB really shines over the MCB. The table below shows the tripping behavior of an MPCB under overload conditions, as defined by trip classes in IEC60947-4.

MCBB

Now let’s look at a similar table for MCBs.

MCB

As you can see, there’s a clear difference. Repeated overloads of 50% or more can seriously damage the motor. The MCBs are clearly not going to trip fast enough to protect the motor windings. In addition, if you look at the last column, the issue becomes even more apparent. The C-curve MCB treats this as a short circuit and the D-curve trips within one minute, whereas the MPCB is much more sensitive and trips within 10s. Coming back to my earlier point, if you oversize the C-curve MCB to compensate for its lower tripping current, you end up running a huge risk of not protecting the motor at all under overloads.

4. Sensitivity to phase failure

There’s one more problem with using an MCB for motor protection – it’s not sensitive to phase failures. A phase failure in a motor is a serious issue that causes a surge in current in the other phases, again leading to overheating and damage to the winding. The MPCB will detect this as being equivalent to an overload in the other phases and trip as per the table above – the MCB will not.

In conclusion, an MCB is not adequate to protect your motor and using just an MCB is fraught with risk. Apart from this, an MPCB is easier to select as the motor ratings are clearly declared on the product itself. It is possible to tune it to your particular application with an accurately adjustable reference current. The operating life of an MPCB is also typically much higher than an MCB.

As a pioneer in motor management applications, Schneider Electric has invested in building possibly the widest range of MPCBs in the market with the TeSys GV family, which is available up to a 500 A rating. Additionally, a full set of selection tables, coordination tables, and application-specific selection guides help you to choose the best possible protection for your motors, wherever they may be used.

Conversation

  • Very clear and good presentation. I will use some of these examples in my presentation to come.

  • First, thanks for your helpful information regarding application of MPCBs over MCB.
    However, I have two questions that I have faced over my career as electrical engineer in the field of power plants BOP.
    1. What are the current limiting specifications of MPCBs in comparison to MCCBs? As you know it helps on reducing the cable size downstream to the motor.
    2. When it comes to larger motors (>15kw) what is the better solution MPCB or MCCB with additional contactor and thermal relay?
    I would be very grateful if you could give me some insight into this matter 🙏
    Sincere thanks in advance for your time and consideration.

  • Thanks for your comment and I’m glad you found this useful. The answer to your question is quite involved and detailed so I will connect with you directly to answer.
    The short answers are: The key determinant to protect the system as a whole (motor, cables, installation) is “coordination”. You can read more about that here:
    https://blog.se.com/machine-and-process-management/2018/11/15/coordinated-motor-starters-the-right-choice-for-reduced-downtime-and-increased-safety/
    In general, due to design differences – MPCBs offer a better protection for motors as they are designed for coordination, whereas MCCBs are designed for cable protection.

    For your second question -all things being equal, the MPCB+OLR is a smaller footprint, so is preferred.

Comments are closed.