Why is Power Connection Integrity Such a Hot Topic?

This audio was created using Microsoft Azure Speech Services

Even power connections that are perfectly installed tend to loosen over time; avoiding this can head off serious problems

Our previous post in this series discussed how important it is for installers to use the correct torque when tightening power connections, and some of the reasons these connections are prone to loosening over time. We also described technology that incorporates spring elements to maintain the integrity of the connection over the long term. In this post, we explain why keeping the power connection tight is so important, and what happens without this type of protection.

Elements of a good connection

Making a good connection at the contactor or circuit breaker, where electrical power is being supplied, begins with the selection of the proper type and size of cable. Preparing the cable includes removing the specified amount of insulation—not too much, but not too little, either—as well as twisting the cable end and sometimes adding surface treatment as appropriate, as illustrated in image 1.

Image 1 Power Connection. Source: Schneider Electric, 2018

The idea behind this careful preparation of the cable end is to ensure that a tight mechanical connection can be made, which is one advantage of screwed connections. Although spring connections offer convenience for the installer, threaded connections provide a means to ensure the specified connection pressure is attained. Such a tight connection serves two purposes: It helps make the electrical resistance as low as possible at the connection and it prevents the cable from being pulled out of the connection, such as during a short circuit.

As noted in our previous post, screw connections have a specified installation torque to ensure the proper mechanical clamping force is achieved. Breakaway bits are available to make it easy to get that part right.

But thermal changes, creep, and external vibrations all can lead to looseness in the connection over time which is detrimental for several reasons. Perhaps most importantly, any looseness in the connection increases its resistance. That also can accelerate oxidation of the conductor, which further increases resistance. Such an increase in resistance can quickly lead to overheating.

Controlling the Joule effect

Any increase in the resistance of a connection can lead to serious problems because of the Joule effect, which is that current passing through a conductor generates heat based on the resistance of the conductor. Simply put, the Joule effect kicks in when resistance goes up, for whatever reason, whether it is a loosening of the connection (lower pressure applied) or an increase in oxidation on the surface of the conductors (which adds resistance in the current path), or both. As the resistance increases, more heat is generated even though the current may not increase. How much heat depends on the amount of current passing through the circuit, because the Joule effect is a product of the resistance times the square of the current, as illustrated in image 2.

Image 2: Thermal Analysis. Source: Schneider Electric, 2018

Overheating = bad

When overheating does occur and is discovered early on, it can serve as a warning that something in the connection is amiss and should be investigated. Frequently, the problem can be remedied simply by retorquing the connection. However, because the temperature of a connection is directly related to the current passing through the connection at the time of testing, testing and observation must be done when the circuit has been operating at its normal operating level for some time. Even then, the current may not be high enough to generate overheating.

The bottom line is that overheating at connection points is indicative of a bad situation. One way to avoid the loosening that leads to overheating is to buy only high-quality products assembled from high-quality components, including the cable termination hardware.

Through its spring-loaded pressure maintenance capabilities, Schneider Electric’s EverLink technology ensures that full contact is maintained in power connections even as material creep occurs. To learn more about this technology, click here.

Our next blog post in this series will further discuss ways to check for local overheating, and what to do about it.

Tags: , , , , , , ,

Conversation

  • Hope your next in this series focuses on IR windows as this is still the most economical and safe way to find these problems. By the way, we make the IR windows that Schneider uses in most of their equipment…

Comments are closed.