How to choose the right surge protector?

Why are surge protectors important?

A surge protective device is essential for safeguarding electrical equipment from voltage spikes caused by lightning, faulty wiring, or switching. It diverts excess voltage away, protecting sensitive electronics like computers, TVs, and appliances.

Choosing the right surge protective device (SPD) and protective circuit breakers involves considering a wide range of parameters related to types of SPDs, circuit breaker arrangements, and risk assessment.

How to choose a surge protector: Three considerations

Now that we’ve established that SPDs should be at the heart of a lightning protection system, it’s time to think about how to choose the right surge protection. Easier said than done. Here are some rules of thumb for how to choose a surge protection device (SPD):

  1. Familiarize yourself with types, or categories, of SPDs.
  2. Assess the risk of lightning strikes and discharge capacities.
  3. Use the right devices to protect the surge protection itself.

To protect a distribution switchboard, you need only install a Type 2 SPD with discharge capacity In>5kA.(8/20).

1. Understanding types and categories of surge protective devices

Surge protective devices are grouped into various types and categories according to their purpose and where they are installed within an electrical system. The main categories are Type 1, Type 2, and Type 3 SPDs.

Type 1 SPDs are installed at the start of the electrical system, like the main distribution board, and are built to manage high-energy surges caused by direct lightning strikes. Type 2 SPDs, which are commonly used at distribution switchboards, protect against residual surges and switching transients, making them ideal for internal electrical protection. Type 3 SPDs are installed close to sensitive equipment, offering fine protection for electronic devices from lower-level surges. Choosing the correct type depends on the system design and the level of protection needed.

2. Risk assessment for choosing a surge protector

Assessing risk is generally a complex, painstaking process. A good starting point is to think about what kinds of areas are most and least at risk. You can then consider the type of SPD best suited to the kind of building you’re planning to protect – if it has a single service entry switchboard.

Lightning strikes 90% of the earth. The high lightning areas are on land located in the tropics. Areas with almost no lightning are the Arctic and Antarctic, closely followed by the oceans which have only 0.1 to 1 strikes/km2/yr.

However, even if the density of strikes (Ng) doesn’t look risky, many countries like France, for example, include Ng in its national standard NF C 15-100. Indeed lightning can be dangerous for your electrical installation and is taken into account by global standards.

One or two tips for risk assessment

Use European HD 60364-5-53, for example. Some countries make it compulsory to use this standard when considering surge protection for big and/or highly sensitive buildings like industrial facilities, hospitals, and data centers.

Otherwise, bear this rule of thumb in mind: always install a Type 2 surge protection. If the distance between the surge protector and the equipment to be protected is greater than 10 meters, then add a Type 2 or Type 3 SPD, close to the load to be protected.

3. Protect your surge protection devices

Although SPDs don’t trip, the following end-of-life scenarios are possible:

  1. Thermal runaway caused by the constant excessive constraints of an SPD not exceeding its lightning attributes could lead to the slow destruction of internal components.
    The disconnection of the SPD is provided by a thermal fuse associated with the electronic components (MOVs) inside the SPD.
  2. A short-circuit due to exceeding the maximum flow capacity or due to a fault under 50hz from the electrical distribution network (e.g., break of neutral, phase-neutral inversion). The disconnection of the SPD is provided by an external or integrated short circuit protection device like a circuit breaker, for example.

Although you may have to choose an external circuit breaker, more and more manufacturers incorporate them in the same enclosure.

You should choose a circuit breaker according to the short circuit current of the building where the SPD is installed. For example, a disconnection circuit breaker with a short-circuit breaking current lower than 6kA is suitable for a residential building. For an office, it is usually 15kA or 20kA.

But determining matches is a delicate business, many parameters need to be considered while selecting the external short-circuit protection (Breaking capacity, Lightning current withstand, Coordination with upstream protection)

That’s why we suggest you reference our Design Guide which will allow you to more easily select the right disconnection circuit breaker.

What is the best wattage for a surge protector?

The best wattage for a surge protector depends on the total power consumption of your connected devices. To determine the appropriate surge protector, follow an surge protection device selection guide and calculate the combined wattage of your equipment. Typically, choose a surge protector with a higher wattage rating than your total consumption to ensure adequate protection. Knowing how to select a surge protection device ensures safety and prevents damage from power surges.

Make an informed choice with our Surge Protection Device Selector

Check out our Surge Protection Device Selector to better know about choosing the right surge protection and circuit breakers for the right application.

And watch this video to learn how to select a surge protection device with the product selector.

How to choose a surge protector? Use our Surge Protection Device Selector

Conversation

  • hello didier,
    can you explain a bit more why it’s better to protect your SPD with circuit breaker instead of fuse ?
    thanks for your clarification

  • The email invite for the survey said that I would be entered into a raffle but I was never asked for my contact information.

    • Hi Mark,
      We apologize for this issue. Your name is submitted into the list of potential winners and we appreciate your patience and response to this matter. Good luck!
      Jennifer

  • Thank you for the survey and helping us understand…..We do have power surges, and the power shuts off for ten minutes, sometimes only on and off
    or longer….then reset everything.

  • Is Class-II SPD is suitable for Home System. If yes, which SPD we use like model, power etc. we have 220v 3 phase system in our region.

  • Hi Didier,
    In a building, we have main LVSB, floor main DB, and terminal DB’s, is it required to install SPD in all switchboards, distribution boards, IT power distribution boards?
    Thanks!
    David

  • i use NW800A TP ACB (Masterpack ) Schneider make for my main L.T panel . please suggest me Is NW800A ACB required for separate SPD for our system safety protection?

Comments are closed.