Smart Home vs Smart Building: What’s the Difference?

A lot of discussion is happening regarding the transformative values of the Internet of Things (IoT) in home and building automation. The growing need for low-cost sensors and wireless technologies is prevalent and is changing the indoor environment (where you work and live) for the better.

Both smart building and smart home automation; they have several things in common which include climate control, lighting automation and security and fire safety. Even though there are a few things in common, both of them require different communications infrastructure to make it work. Few things that set them apart from each other are:

 Building Size and Structure

Here the physical environment plays a significant role due to its impact on the quality of the wireless radio link. When talking about small-scale home entertainment that comes with simple structures and fewer obstacles present minimal challenges that lead to short-range technologies. Let’s say you have wi-fi connection issues in some parts of your house, and it can be easily rectified by just one extender.

But on the other hand, when it comes to commercial buildings that are present in widely spread campuses or structurally dense industrial facilities, here, short-range solutions will not help the cause due to the area coverage. 

Power Requirements

To begin with, in-home automation low power wireless connectivity is an add on, not a necessary requirement. Why do you wonder? Well, that’s because most devices are conveniently placed near the power outlets, but there are only a handful of endpoints. So technically, yes, you can connect all of your smart home devices to the internet using your current wireless network- without thinking about its power-hungry nature.

Now, on the other hand, for commercial and industrial facilities, they are not placed anywhere near the power supply, and even if they are, wiring that many sensors are too expensive and not manageable.

 Legacy Radio Systems

One of the many challenges faced by the wireless communication systems that function in the license-free spectrum is an in-band ratio. It is globally present, especially the 2.4 GHz frequency band – it is widely accepted amongst the existing radio technologies which include Bluetooth, wi-fi, Zigbee among others. The bandwidth issue at a home network might seem less crucial, given the small number of connected devices. On the contrary, for industrial IoT buildings, the risk regarding electromagnetic interference is significant.

We would like to conclude by saying that despite their similarities in certain situations, the smart home and building architecture consists of different technical, network connectivity, and engineering requirements. When talking about smart buildings, the challenges you might face in network range, power and scalability mean that industries need to look beyond established short-range and mesh solutions in the market. In the end, what you opt for regarding the connectivity choice can make or break your IoT structure.