This audio was created using Microsoft Azure Speech Services
Smart home automation refers to a device, appliance, or system that can connect to a common network, which is independent and remotely controlled. When you bring your home and technology together, it can be referred as “connected home.” For instance, lights, switches, audio speakers, thermostats, security cameras are connected to a common system and can be controlled from your smartphone (through an app) or via touch screen device.
With smart home automation, you can explore the world of high-tech functionality and luxury that wasn’t necessarily possible in the past. As technology progresses, the possibilities for consumers’ home automation increases too.
Some of the advantages that come along with smart home automation are:
1) Manage your home devices from one single place: The convenience factor here is gigantic, especially if you live with your parents. To be able to control all the devices at your home through an interface is a huge step forward for technology and home management. To enjoy this freedom, all you need to do is, use an app on your smartphone or tablet, which makes it easier to access the functionality you always wanted for your home.
2)Flexibility and freedom for all new devices and appliances: Smart homes have the reputation of being flexible when talking about the accommodation of new devices and appliances. It doesn’t matter how state-of-the-art your appliance might look like today, and there will be newer and more efficient models as time goes by. And, after a point of time, you will add more devices and replace the older ones or even discover new technology that will accompany your indoor and outdoor spaces.
3)Better and safer home security: For anyone with small children or staying with elderly parents, this is a feature that is highly useful. When you incorporate both security and surveillance together into your smart home network, your home security will reach another level. If you are looking for a company that you can trust with the same, then you can opt for Schneider Electric.
Wiser is their home automation service that will help turn your house into a Smart Home, which makes every switch (turn into remote control switch), appliance, and CCTV cameras, in your home a connected device. You can connect motion detectors, surveillance cameras, automated door locks, and other tangible security measures throughout your home and can activate them from one mobile device.
4)Controlling the functions of your home remotely: The possibilities of being able to control your home functions remotely is immense. For instance, if the weather outside is hot, you can easily bring down the temperature of your home. Through your app, you can turn on the air conditioner. In addition to that, you can even check if you left the lights on and ensure that you turn off your electronic items while you’re away.
5)Increase in energy efficiency: Depending on how you utilise your smart-home technology, it is possible to make your place more energy-efficient. For instance, you can have control over the heating and cooling of your house with the help of a smart programmable thermostat, which can learn your schedule and temperature preference and even suggest the best energy-efficient settings throughout the day. You can also control the lights and switch the motorised shading to morning mode or your lights can turn on or off when you enter or leave your
Related Article : What Is Home Automation and How Does it Work?
Conversation
Shaylee Packer
4 years ago
As you mentioned, when you have smart home automation, you can control all of your home devices from one place. My brother recently purchased a home, and he wants to make it a smart home, with the lights and such connected to his phone. I will have to share this article with him, and see what he thinks.
Lightomated
3 years ago
Thank you for the information about the advantages of smart home automation. A smart home allows homeowners to control appliances, thermostats, lights, and other devices remotely using a smartphone or tablet through an internet connection. Smart homes can be set up through wireless or hardwired systems. Smart home technology provides homeowners with convenience and cost savings.