Navigating challenges with modular low-voltage system solutions

In an industrial operation, every decision made today lays the foundation for tomorrow’s success. The demands for flexibility, safety, and efficiency constantly grow, and businesses need systems that can evolve alongside them. This requires solutions that meet current needs and adapt to future challenges.

A SIAL engineer stands in front of a modular low-voltage system, with their back to the camera.
Modular low-voltage systems prioritize scalability and flexibility in their design.

Modern, modular, low-voltage (LV) systems are an ideal answer. They allow companies to customize their electrical infrastructure to suit their business strategies, meet rigorous safety standards, and maintain operational efficiency—all while being adaptable for future needs. These systems can have up to 30% less carbon footprint and up to 30% less space needed. They also enable predictive maintenance via thermal monitoring, reducing maintenance costs by up to 30%.

Let’s explore how modular low-voltage systems can address critical challenges in industrial processes and enhance operational performance.

Navigating complexities: Overcoming electrical challenges with low-voltage systems

At SIAL Ingeniería, we often see industrial companies that face significant challenges with their electrical distribution systems. As a Schneider Electric EcoXpert partner, we recognize that no one knows their business challenges better than our clients, and we listen. They need flexibility and scalability to adapt to operational needs and future expansions without significant overhauls. Safety is another concern, as systems must protect equipment and personnel from potential faults and hazards. Minimizing operational downtime is critical, as even brief interruptions can affect productivity. Lastly, our clients look for long-term durability and cost-effectiveness. This means they need solutions that reduce maintenance needs and lower the total cost of ownership.

Key benefits of modular low-voltage systems

Modular low voltage (LV) systems are designed with flexibility and scalability in mind, making them the ideal tool for industrial operations that want to optimize their electrical infrastructure. These systems bring several core benefits that address the most pressing challenges industries face today:

  1. Fast installation and cost management: Pre-fabricated modules can be assembled on-site, which reduces construction time and accelerates operational readiness. Clients select only the modules and features they need. This way, businesses can manage costs effectively, avoiding unnecessary expenditures and ensuring that investments align with specific project requirements.
  2. Customization and flexibility: A tailored approach to electrical distribution is vital. Whether expanding operations or integrating new technologies, these systems allow businesses to customize configurations to meet their needs. The ability to quickly scale systems up or down ensures that companies can adapt without significant overhauls or downtime disruptions.
  3. Enhanced safety: Modular systems are built with advanced safety features like internal arc containment, thermal monitoring, flame-resistant materials, and pressure relief vents. Compliance with international standards such as IEC 61439 and IEC 61641 ensures that these systems meet rigorous safety and performance criteria, reducing risks for both equipment and personnel.
  4. Operational efficiency: Reduced downtime allows businesses to maintain and upgrade components without halting operations. Advanced monitoring and control capabilities provide real-time data, allowing industries to optimize energy use, identify inefficiencies, and reduce maintenance costs. This operational efficiency directly contributes to improved productivity, preventive maintenance, and profitability.
  5. Compliance with global standards: Operating in multiple regions or countries means adhering to many regulatory standards. Compliance with international standards ensures modular LV systems can be implemented without modification, saving time and resources. Standards like IP54 guarantee that electrical distribution systems meet rigorous performance and safety criteria. This offers peace of mind for companies working in complex industrial landscapes. Compliance future-proofs electrical systems and prepares them to meet new regulatory requirements as they evolve
  6. Scalability for future growth: Legacy LV systems can be rigid and expensive to upgrade. They often need costly overhauls to accommodate new technologies or expansion. However, modular LV systems prioritize scalability in their design.
    As operational needs change, businesses can easily add or remove components to match their specific requirements. Whether integrating renewable energy sources or adding new layers of protection, modular systems allow for incremental adjustments without requiring complete system rebuilds. This scalability reduces initial investment and ensures businesses are prepared for future innovations and sustainable growth as they move toward decarbonization and energy efficiency.
  7. Renewable energy integration: Easy integration helps companies transition towards greener energy without extensive modifications to existing infrastructure. By facilitating the use of renewable energy, these systems reduce carbon emissions and help organizations meet sustainability and decarbonization goals.

Bringing it all together: A proven solution

BlokSeT is the perfect example of how modern low-voltage electrical distribution systems can meet today’s demands while anticipating future needs. Designed to comply with rigorous safety standards such as IEC 61439 and IEC 61641, BlokSeT enhances operational safety and ensures long-term flexibility and scalability.

Its modular design allows businesses to easily upgrade and expand their infrastructure without significant overhauls. This reduces downtime and optimizes operational efficiency. By integrating advanced safety features like internal arc containment, BlokSeT helps businesses safeguard their assets and personnel while staying compliant with international regulations.

Sustainability and the future of low-voltage electrical systems

As sustainability becomes a top priority for industries globally, modular LV systems are crucial in optimizing energy management, reducing energy losses, and integrating renewable energy sources, allowing for integrated, real-time connected devices to track energy consumption and address inefficiencies in real-time, reducing their environmental impact.

A modular design also extends the system lifespan, minimizes waste, and supports incremental upgrades. This allows businesses to meet sustainability targets while avoiding significant overhauls. By incorporating energy-efficient components like power factor correction and efficient load management, LV systems improve operational efficiency and contribute to global decarbonization efforts.

Modular LV systems like BlokSeT are the future of industrial operations

Our goal is to provide customized, scalable electrical systems that solve today’s challenges and prepare our clients for the future. To learn more about how SIAL Ingeniería can help modernize your organization’s electrical infrastructure, visit  www.sial-ingenieria.com.ar and submit an inquiry to explore options tailored to your business. Or visit Schneider Electric’s BlokSeT range for more solution information.

The EcoXpert Partner Program is unique in its industry and made up of a best-in-class, global ecosystem of expertise. Trained and certified by Schneider Electric, EcoXpert partners digitize and electrify our world for a more sustainable future.

The path to net-zero is about delivering solutions for sustainable, resilient, efficient, and people-centric buildings. For our EcoXpert partners, this unveils immense growth opportunities through the transition to end-to-end portfolio sales that will resolve our customers’ most critical needs. For our shared customers, this means that together with our EcoXpert partners, we will drive the building industry transformation and help our customers survive and thrive today – and tomorrow.

Visit the EcoXpert webpage to learn more.

ABOUT SIAL INGENERIA

SIAL Ingeneria is a company dedicated to the development, integration, and execution of industrial electrical projects and automation of machines and processes. With over 20 years of experience in the Argentinian market, SIAL builds low-voltage equipment with the highest Master EcoXpert Power Distributor qualification from Schneider Electric SA.

Add a comment

All fields are required.