The stability of power grids supplying energy to our homes and businesses is emerging as a critical success factor for maintaining both physical and economic security. Regardless of the electric grid size—a microgrid with several hundred users or a regional grid with millions of users—grid complexity is on the rise. Trends such as the sharp increase in Internet of Things (IoT) devices and digital solutions that tax large and small grid capacities, a growing installed base of renewable energy generation, and the proliferation of distributed energy resources (DER) behind the meter at the grid’s edge, are all contributing to this complexity.
Unfortunately, the electric design of existing grids has not been optimized to accommodate these new behaviors. Local and national grids are experiencing significant changes in energy flows. In the past, the energy consumption pattern was easy to interpret. At around 6:00 p.m. rates of energy consumption were high and not much energy was consumed during the night. Now, businesses, hospitals, and homeowners, for example, may be producing energy at midday with solar panels. An increasing quantity of electric cars are also consuming energy in the middle of the night to recharge their batteries. Energy prices that sometimes change minute-by-minute are also altering where and when enterprises choose to consume the most energy. This makes the flow of energy within grids more volatile. Instead of traditional top down energy distribution, grids must deal with bidirectional energy flows which change throughout the day and night.
To accommodate the changing nature of the grid, stakeholders are investing in both technology and manpower to better forecast short-term evolution of electricity in their operation. Without accurate consumption forecasting, nodes within the grid can become saturated with energy demand that is too high which, in turn, can lead to grid failures and blackouts.

Why AI digital solutions can improve forecasting accuracy
This is where we at Predictive Layer, a Schneider Electric Technology Partner, offer support. Electrical utilities and microgrid managers need to forecast, with high accuracy and speed, short-term grid energy consumption across the geography of their grids. We have developed an artificial intelligence (AI) engine to address the new layers of grid network complexity.
Today most large grids deal with the challenge of energy consumption forecasting by assigning teams of mathematicians to automate and scale the forecast. Should the parameters of energy consumption change—an extreme weather event, or a societal event where many people are forced to work from home—those complex mathematical models have to be rapidly reworked in order to align with the new reality. When thousands of grid network nodes are involved, the task becomes too complex to execute in a rapid fashion—even for the best mathematicians. The task is also challenging for microgrids and smaller local grids who typically have few human resources to dedicate to forecasting.
An AI-driven forecasting engine learns from both past energy consumption patterns and from real time live situations. For example, the changes that are taking place within a grid (like the addition of new transformers in a location) and the intricate nuances in energy consumption demand automatically are fed into the model on an ongoing basis. This includes data from transformers, information about the behavior of subscribers connected to the network, and information surrounding weather-related and calendar date-based patterns of consumption.
Benefits include less downtime and lower operational costs
The AI engine learns how to better forecast what is happening every day, everywhere within the confines of the grid, and continues to get smarter as it processes more data. At each point of the day or night it can generate, on behalf of grid operators, local schedules of how much energy should be delivered to designated locations and expected volumes of energy coming in or out. The AI forecasting tool also automatically reconfigures itself as changes occur across the grid. If a new enterprise suddenly turns the lights on in a new facility within a geography, the engine can recalculate that the energy consumption peak will now occur at 4:00 p.m. rather than at 6:00 p.m. in that area.
Instead of a team of people generating 10 forecasts of what is happening in each of their regions, the software can generate thousands of such forecasts in minutes. These forecasts can account for every locality within the grid. (In New York state, for example, there may be 10,000 transformers in the entire network that distribute energy to users.)
The benefits of having access to such an automated system include less network downtime, better operational management and cost control, and higher efficiency of electricity distribution. The tool also makes it easier to manage a crisis where rapid changes in consumption require immediate actions. The goal is to sustain the level of customer expected quality and uptime regardless of the changes that are taking place across the grid.
Get more information about AI and grid forecasting
To learn more about how digital solutions such as artificial intelligence tools can better manage grid consumption forecasting:
- Review our Predictive Layer website.
- Find us on the Schneider Electric Exchange platform, a global network of experts and peers in energy management and automation.
- Read our two-part blog series:
- Part 1, “Changes in Energy Resources Marketplace Behaviors Usher in New Era of AI-driven Price Forecasting” reviews the reasons why the marketplace has evolved and explains how new energy trends are impacting pricing complexity across the industry.
- Part 2, “Why Utilities Are Using AI Digital Solutions to Reinvent the Science of Price Forecasting” highlights some of the advantages utilities and other energy stakeholders can accrue when they deploy an AI-driven forecasting model.
You can also use Schneider Electric Exchange to collaborate and co-innovate on trending topics like AI and innovative solutions by joining any of hundreds of Exchange communities.
Learn more about energy management solutions
Want to see how Predictive Layer, a Technology Partner of Schneider Electric, is helping to optimize energy consumption with the use of AI-based software? Read some of our energy case studies on the Predictive Layer website or on the Schneider Electric Exchange website. Learn more about accurate forecasting data models for the Energy industry.

Schneider Electric Exchange
Schneider Electric Exchange is the first open business platform dedicated to solving real-world sustainability and efficiency challenges. Connect with more than 56,000 registered members and a global network of experts and peers in energy management and automation, listen to webinars and podcasts, view content in the Schneider Electric Knowledge Center, or visit open communities, such as Industrial Automation.