The EU Energy Efficiency Directive and its impact on CIOs, data centre owners and operators

In my role as sustainability leader for EcoStruxure IT, I have the unique vantage point of seeing how the IT and Data Centre industry is changing to limit its impact on the environment.

Data centres are voracious energy consumers, accounting for nearly 2.7% of European electricity usage it is expected to reach 3.21% by 2030. Reducing their environmental footprint and operational costs is becoming a priority and many CIOs, data centre owners and operators, and IT professionals are increasingly adopting energy efficiency tools and strategies.

The European Union’s Energy Efficiency Directive (EED) is a comprehensive legislative framework aimed at reducing energy consumption and promoting energy efficiency across various sectors. The recast in 2022 brings into focus data centres. The Energy Efficiency Directive plays a crucial role in setting a baseline for energy consumption to drive energy efficiency improvements and addressing the growing environmental impact of these facilities. The directive has 12 chapters, 17 annexes, and mentions “data centre” 48 times. Task Reports have been added since the release of the directive in September, companies are waiting on the final version of the Directive. I will summarize the key provisions for data centres as it reads today. Data centre owners and operators will be expected to report on metrics specified by the Energy Efficiency Directive starting May 2024.

The impact of the EU Energy Efficiency Directive on data centres and CIOs.

How the EU Energy Efficiency Directive affects data center CIOs

The EU Energy Efficiency Directive impacts data center CIOs by setting stringent energy performance standards that drive improvements in data center energy efficiency. CIOs will need to consider adopting advanced technologies and optimize operations to comply with these regulations, which include energy audits and reporting requirements. Adhering to the directive not only ensures regulatory compliance but also enhances operational efficiency and reduces costs, contributing to overall sustainability goals.

Key provisions of the Energy Efficiency Directive for data centres

  1. Mandatory Reporting: Data centre operators with a total rated power of at least 500 kilowatts (kW) are required, per the Energy Efficiency Directive, to publicly report their energy performance data annually. This data includes energy consumption, PUE (Power Usage Effectiveness), temperature set points, waste heat utilization, water usage, and use of renewable energy.
  2. Waste Heat Utilization: Data centres with a total rated power exceeding 1 MW must utilize their waste heat for heating purposes or other energy recovery applications unless it is technically or economically unfeasible. This promotes the circular economy and reduces the need for fossil fuels.
  3. Renewable Energy Integration: Data centres should prioritize the use of renewable energy sources for their electricity consumption. This effort helps to reduce the carbon footprint of data centres and contribute to a more sustainable energy mix.
  4. Optimizing Energy Consumption: Data centre operators must implement energy efficiency measures to reduce their overall energy consumption. This includes optimizing cooling systems, using more efficient IT equipment, and adopting virtualization and server consolidation techniques.

Directive goes beyond EU companies, it will have an impact on companies outside of EU

Foreign companies operating within the EU are required to comply with these directives. They must take steps to improve energy efficiency in their operations, which could involve making changes to their facilities, equipment, and processes.

Data centre operators can implement IT efficiency tools like DCIM (Data Centre Infrastructure Monitoring) that monitor and optimize the performance of their IT equipment. DCIM can aggregate and report on PUE, total energy consumption with breakdowns by subsystems and even carbon emissions. Operators will be able to set baselines and start accumulating reports and will be able to use the reports to visualize inefficiencies, unnecessary power consumption and improve overall system efficiency. Companies that comply with the EU Energy Efficiency Directive will reap a variety of benefits almost immediately.

The role of energy efficiency in data center management under new EU regulations

Under new EU regulations, data center energy efficiency is crucial for effective data center management. These regulations mandate improvements in energy use, requiring data centers to implement advanced cooling systems, optimize power consumption, and conduct regular energy audits. By focusing on data center energy efficiency, organizations can meet regulatory requirements, reduce operational costs, and enhance sustainability, ensuring their data centers operate within the new regulatory framework while minimizing their environmental impact.

Benefits of implementing EU Energy Efficiency Directive requirements

The companies that comply with the directive will see benefits including:

  • Reduced Energy Costs: Data centres can lower their operational expenses by implementing Energy Efficiency Directive requirements, optimizing energy consumption and adopting efficient technologies.
  • Environmental Protection: Improved energy efficiency reduces greenhouse gas emissions and contributes to a more sustainable data centre industry.
  • Enhanced Resiliency: Improved energy efficiency reduces the strain of data centres on the grid, contributing to a more resilient infrastructure and grid.
  • Enhanced Competitiveness: Energy-efficient data centres gain a competitive edge by reducing operating costs and demonstrating a commitment to sustainability.
  • Improved Public Image: Data centres that meet EED requirements project a positive image of environmental responsibility and align with public concerns about climate change.

DCIM is a great tool to report on the directive. Schneider Electric is invested in supporting you with the evolution of its DCIM solution. Learn more about our DCIM solution – EcoStruxure IT by visiting our DCIM software page

Add a comment

All fields are required.