This audio was created using Microsoft Azure Speech Services
At the Xperience Efficiency 2013 event in early June in Washington, D.C., Schneider Electric announced that its Energy University program now has more than 350,000 registered users. At the event, I caught up with Michelle Souza, program manager for Energy University, to learn more about the program.
It was launched in 2006 as the Data Center University Program, Souza says. In 2012, after Schneider Electric acquired APC, it was merged into the broader Energy University program.
Two main “colleges” comprise Energy University, Data Center and Energy Efficiency. Together, they offer more than 200 courses, each of them free of charge and vendor and product neutral, Souza says. All the courses take less than an hour to complete, usually 30 to 45 minutes.
Courses are eligible for education credits recognized by more 20 organizations, she says, including the U.S. Green Building Council, the IEEE, the American Council On Renewable Energy (ACORE) and HIMSS.
Two different certifications are also available through Energy University, Souza notes. The Data Center Associate certification requires 14 courses before students are eligible to take the exam. Once you pass it, you’ll be certified in areas including power, racks, cooling, cable and monitoring.
The other certification, Professional Energy Manager, was launched last October in partnership with the Institute of Energy Professionals (IEP). Since then, more than 40 professionals have been certified through the program in the growing energy management field.
“Certification is a great tool for improving one’s career path and to help climb the ladder steps quickly,” Dhinesh Kumar Ganesan, a PEM certified through the program, said in a statement issue by Schneider Electric. “The Professional Energy Manager exam will certainly add value, qualifies my knowledge and will increase my profile rate among other professionals.”
Schneider Electric also announced at the Xperience Efficiency event that it will be adding new courses over this year and building a new category of industry topics to complement the Data Center and Energy Efficiency curriculum. The first will be released in the third quarter, targeting the ISO 50001 energy management system framework.
Altogether, professionals have taken more than 500,000 Energy University courses to date, and with good reason. As Souza notes: “The program is completely free of charge. It’s hard to turn down free education.”
Conversation
abdelmonem
9 years ago
dear sir,
i am certified professional energy manager (PEM) from IEP by energy university and i pass all courses .
i searching about job with Schneider in the same field and i have 11 years experience.
name :- abdelmonem kamal
work in saudi arabia
iya davidlivingstone
9 years ago
how can I advance my electrical certificate course with energy university?
Tom Clune
9 years ago
Greetings,
Energy University offers over 200 courses to help you advance your knowledge in Energy Efficiency. All courses are free of charge and taken at your own pace online. We also offer the Professional Energy Manager exam which enables efficiency-minded professionals to address today’s growing energy concerns, such as cost, availability, and environmental impact. Certified individuals can advocate for efficiency as a means of reducing costs and improving business performance; recommend appropriate solutions; and monitor and sustain efficiency gains.
Additional information regarding the PEM exam as well as a course catalog can be found on the Energy University site, http://www.myenergyuniversity.com
Mina Wassef
7 years ago
Dear sir,
I’ve a problem with my certificates of the completed courses, as when I click on the course certificate icon to open my certificate, a new tab is opened with the following message:
“File does not exist: ISO 50001_ Maximizing Your Energy Efficiency Through Proven Standards_Nicolas.pdf (102) More info”
This happens with all certificates.
Jae Wiss
7 years ago
Hi Mina. I am sorry for the delay in response. I checked with my colleagues and it seems that this was a technical glitch that has since been corrected. You should be all set.
Royal Emmanuel
7 years ago
Pls am from Nigeria and want to know what qualification do i required to be enlisted in the online curses. Thank you