From switchboards to smart buildings: The quiet revolution powering Australia’s electrification push

In the electrical room of a mid-tier office building, an unremarkable, outdated switchboard hums quietly. It’s inconspicuous, yet a vital part of the annual $5.6 trillion investment in the global energy transition—a quiet shift transforming Australia’s buildings into dynamic, data-driven ecosystems. The future of electrification is being shaped in switchboards, where analog panels are being revitalised as digital nerve centers.

Australia’s commercial building industry is at a key turning point. Sustainability requirements are becoming stricter. Tenants are asking for smarter, more sustainable spaces. Energy prices are climbing rapidly. However, many buildings remain rooted in infrastructure designed for a very different time. That’s where modern switchboards come in—the hidden backbones of smart buildings, integrating energy monitoring, heating, ventilation, and air Conditioning (HVAC) systems, and Electric Vehicle (EV) readiness into the core of a commercial property. And while many owners view these upgrades as costs rather than opportunities, at GSTEC, we believe it’s time to shift perspectives. Electrification is an investment, not an expense and it forms the foundation of a building’s long-term competitive advantage.

people sitting in front of a bank of monitors with graphs and charts
Australia’s commercial building industry is at a key electrification turning point

Switchboards: No longer a panel, but a platform

The electrification transformation began with a nudge. Recent updates to Australian switchboard manufacturing standards are forcing long-overdue upgrades. But compliance is just the floor—the ceiling is game-changing efficiency.

Switchboards have evolved from basic distribution panels into intelligent, connected systems. Once simply routing power and protecting circuits, they’re now becoming IoT-enabled nodes at the heart of smart buildings. A fully digitized, IoT-capable switchboard can do more than monitor loads. It can segment consumption by system or tenant, support predictive maintenance, identify power quality issues in real-time, and integrate seamlessly with energy management systems (EMS) and building management systems (BMS) platforms. The result is improved visibility, faster response times, and a stronger foundation for efficiency, compliance, and future-ready performance.

One standout example is Aurora Place, a 49,000 m² tower in Sydney’s CBD. GSTEC led a seamless upgrade of the BMS/EMS and main switchboards, complete with Schneider Air Circuit Breakers, without disrupting tenants over 41 floors. The result was improved tenant comfort, higher energy ratings, and peer acknowledgement, including the 2022 Schneider EcoXpert Global Project of the Year and the 2023 NECA NSW Commercial Medium Award.

Fragmented projects, fragmented outcomes

We’ve found that the best outcomes start in the design room. In too many buildings, upgrades unfold in silos: electrical teams manage one track, mechanical contractors another, and energy reporting is bolted on late. The result is often systems that don’t talk to each other, and performance that underdelivers.

We regularly encounter this fragmentation. HVAC upgrades may proceed without digital infrastructure. EMS platforms arrive too late to capture meaningful data. EV readiness gets treated as a separate project altogether. When GSTEC is involved early, these threads are aligned from the start. Electrical and mechanical upgrades become part of one strategic playbook, and complexity is reduced before it ever takes root.

From compliance to strategy: Making the case for investment

Because budgets can be tight, it’s important to work smarter. Switchboard upgrades are often seen as unremarkable, a response to aging gear or shifting standards. But, when positioned strategically, they unlock a great deal more.

Bundled with HVAC renewals or sustainability retrofits, modern switchboards enable segmentation, performance tracking, and energy visualization. They support compliance, National Australian Built Environment Rating System (NABERS) targets, Environmental, Social, and Governance (ESG) goals, and long-term asset value.

So, reframing CapEx is key. These aren’t sunk costs; they will be revenue drivers. A building’s stronger energy profile leads to higher occupancy rates, longer lease terms, lower risk, and even lower insurance premiums.

HVAC meets energy management: The integration advantage

At GSTEC, our strength lies in our capacity to link mechanical and electrical systems into a single, intelligent network. That’s especially true for HVAC-linked switchboards, where mechanical upgrades provide the perfect opportunity to integrate digital capabilities.

Through equipment-level metering on pumps, fans, and chillers, GSTEC enables real-time energy tracking. That data feeds into building management systems, where it powers strategies like load scheduling, peak shaving, and predictive maintenance.

Think of the switchboard not as an isolated upgrade, but as the brainstem of a smarter organism where every system contributes to a coordinated whole—and where electrification strategies can be implemented seamlessly.

Reporting isn’t optional anymore

Energy reporting has evolved from a compliance checkbox into a business asset. Tenants want transparency. Investors want performance. Regulators want proof.

But effective reporting begins with infrastructure. GSTEC designs architectures that integrate smart meters with EMS and BMS platforms, transforming raw data into live dashboards and predictive insights. Whether benchmarking against NABERS or tracking emissions in real time, the visibility is immediate and actionable.

For building owners, this meets mandates, yes, but also builds trust, helps secure premium leases, and stays ahead of the market’s next evolution.

One strategy, not three projects: A roadmap for modernization

Modernization efforts are often treated as separate line items: switchboards here, HVAC there, and EV readiness somewhere down the road. But the buildings that succeed are those that tie these threads together.

Here’s the roadmap GSTEC recommends:

  1. Start with the switchboard
    It’s where visibility, compliance, and future-readiness begin.
  2. Bundle electrical and mechanical upgrades
    Align investments to optimize efficiency and reduce disruption.
  3. Design for tomorrow’s loads
    Prepare now for EV infrastructure, solar, and energy storage—even if they’re not installed yet.
  4. Engage integrators early
    Get systems talking from day one, not during post-construction fixes.
  5. Build with data in mind
    Smart metering and EMS platforms turn consumption into insight—and insight into value.
  6. Start small, prove value
    Pilot metering on high-load circuits to build a business case for broader rollout.

Early collaboration is the key to smarter, more future-ready buildings. Whether you’re tackling aging infrastructure, planning for EV readiness, or seeking stronger NABERS performance, GSTEC can help you connect the dots. Contact us to explore our approach and see how smart electrification can unlock new value for your building. 

The EcoXpert Partner Program is unique in its industry and made up of a best-in-class, global ecosystem of expertise. Trained and certified by Schneider Electric, EcoXpert partners digitize and electrify our world for a more sustainable future.

The path to net zero is about delivering solutions for sustainable, resilient, efficient, and people-centric buildings. For our EcoXpert partners, this unveils immense growth opportunities through the transition to end-to-end portfolio sales that will resolve our customers’ most critical needs. For our shared customers, this means that together with our EcoXpert partners, we will drive the building industry transformation and help our customers survive and thrive today – and tomorrow.

Visit the EcoXpert webpage to learn more.

Add a comment

All fields are required.