According to the International Energy Agency, buildings (commercial, residential, and new construction) account for nearly 40% of global greenhouse gas emissions. While commercial buildings alone contribute a smaller share (~6.6%), they remain a significant source of energy consumption. Within these facilities, HVAC systems are a substantial energy draw, responsible for 24–40% of total energy use. That makes HVAC a prime target for energy savings, especially as building owners face mounting pressure to meet net-zero targets and avoid costly non-compliance penalties.
But improving HVAC efficiency isn’t as simple as turning a dial. Many systems rely on complex hydronic networks where managing water pressure, temperature, and flow is a delicate balancing act. That’s where pressure-independent balancing control valves (PIBCVs) and smart actuators come into play. They offer a powerful, intelligent solution that boosts performance and comfort and can also deliver energy savings of 20% or more.

What is a smart actuator?
A smart actuator is an advanced device that combines traditional actuation with control algorithms, connectivity features, and support for external sensing, enabling it to perform intelligent control functions directly at the valve level.
When applied to Pressure Independent Balancing Control Valves (PIBCVs), smart actuators manage hydronic flow and thermal energy delivery with high precision. These actuators continuously monitor variables such as flow rate, temperature differential, valve position, and energy consumption. These often use connected sensors like supply and return temperature probes. With this data, they can implement advanced strategies like Delta T Management to maintain optimal coil performance. It can also prevent issues such as low Delta T syndrome, which can reduce system efficiency and overburden central equipment.
Smart actuators also offer diagnostic features that detect problems like control loop instability, valve blockage, or improper flow rates early. This enables proactive maintenance and reduces downtime. An additional benefit is the availability of spare input/output (I/O) points on some models. These can be used to connect and monitor other HVAC-related variables—such as differential pressure, occupancy sensors, or pipe temperatures. This further extends the actuator’s role in overall system management.
Smart actuators: The perfect partner for PIBCVs
A major advantage of these devices is their ability to communicate using open protocols like BACnet or Modbus. This makes integration with building management systems (BMS) seamless. Through these protocols, smart actuators transmit a wealth of real-time data, including energy metrics, system performance trends, alarms, and diagnostics. This transparency enables facility managers to monitor system health continuously, fine-tune performance, and respond quickly to anomalies or inefficiencies.
Beyond data sharing, smart actuators contribute to fault prevention by identifying conditions such as stuck valves, abnormal flow rates, or temperature imbalances before they escalate into system failures. Some models can even trigger automated responses or alerts when thresholds are breached, supporting predictive maintenance, and reducing unplanned downtime.
Additionally, smart actuators can be remotely configured through the BMS to operate in different control modes—such as Power Control, or Delta T Management—without the need for manual intervention. They also allow dynamic adjustment of the PIBCV’s design or maximum flow rate remotely. This provides the flexibility to adapt zone capacity based on occupancy patterns or seasonal loads. This level of control supports adaptive strategies, simplifies commissioning, and enhances the long-term efficiency and reliability of the hydronic system.
Using analytics to maintain critical cooling
They are especially valuable in environments with critical heating and cooling demands, such as data centers. In these settings, maintaining consistent cooling is essential. Computer equipment generates significant heat and must stay within specific temperature ranges to operate efficiently and avoid thermal damage. Data centers typically rely on computer room air conditioning (CRAC) units that must run continuously, 24/7/365, leaving no room for downtime.
PIBCVs provide localized stability to the CRAC water distribution system in these conditions. Using an associated smart actuator, data can be collated and used for advanced analytics to identify and remediate potential issues. This ensures high uptime. In fact, many CRAC units built by original equipment manufacturers (OEMs) include PIBCVs and smart actuators as a core part of their technology. However, they can also be added during the design and installation phases if they are not part of the core equipment package.
Discover how our valves and valve actuators can help you achieve your goals for cost savings, energy efficiency, and streamlined operations.
Or, if you’re ready to make a purchase, visit iPortal by Schneider Electric to get started.
Add a comment