Didier Fulchiron
Didier Fulchiron
Didier Fulchiron started his career as test engineer in the high power laboratory of Merlin-Gerin. Afterwards, he went through several positions in the design teams for MV switchgear, and also spent some years as product manager for utilities protection relays and RTUs. These positions brought him many opportunities to discuss with users, and to write technical communications.
He became involved in standardisation late in the 90's, and this part of the job took more and more importance along the years.
Articles

Want a Safe, Reliable Electrical Distribution System? Start Early.
- 5 min read
- Didier Fulchiron

Electrical Distribution Safety and Reliability: Get it Right from the Start
- 3 min read
- Didier Fulchiron

Play it safe with medium voltage equipment installations
- 2 min read
- Didier Fulchiron

“Arc flash” vs. “internal arc resistance” – a tale of two terms
- 3 min read
- Didier Fulchiron
Bloggers you may also like
Joe Richard
Senior Director of Offer Management
Most recent post: Why SF₆-free switchgear is becoming a board-level grid modernization decision
Gregoire Wendling
Product Owner Air Circuit Breaker
Most recent post: Welcome to the new era of simple, modern, and safer power: Digital-ready air circuit breakers
Braheem Santos
Healthcare Segment Lead
Most recent post: Virtual environments – transforming healthcare design, build, and operations