How digitalization is bringing critical power distribution out of the dark

In the face of rising competition and mandates to improve operational efficiency, large commercial buildings and mission-critical facilities need to keep power distribution systems running safely, reliably, sustainably, and in compliance with regulations. If you’re running a facility like a hospital, data center, or industrial plant, several hidden risks make these goals even more challenging.

The digitalization of electrical systems is helping reveal these risks and meet operational goals. This proven technology is available today. Still, if you’re like most organizations, you’re continuing to ‘work blind’ without the deep insights that a digitally-connected power distribution system can deliver. Not convinced? Let’s first take a look at those risks.

Risks to safety and uptime

With electrical system issues recognized as the cause of 22% of all fires, finding sources of overheating should be a priority. In hospital operating theaters, insulation faults can put lives at risk, so specialized monitoring should be put in place. If a power outage occurs, power must be restored quickly to ensure occupant safety and restore operations. Studies show power quality issues cause up to 40% of business downtime, causing massive costs in lost productivity and equipment replacements. You need tools that can help you identify when conditions are deviating outside of safe parameters before things become critical.

Risks to energy and operational efficiency

The US Department of Energy believes that buildings can be made 80% more efficient with the right technologies, even ‘net-zero’ if using onsite renewables. However, energy waste will remain hidden and renewables not fully leveraged without detailed visibility into everything from billing, consumption, and energy production. Maintaining power and building systems is another big hit to the bottom line, up to 35% of a building’s lifetime costs. Condition-based predictive maintenance can improve operational efficiencies, saving up to 20% annually. But this requires putting more powerful analytic capabilities in the hands of facility teams and enabling new levels of collaboration with expert services.

Risks to compliance

The need to meet emissions regulations and corporate sustainability goals is becoming more common. Healthcare facilities are often required to test backup power systems regularly. And every organization should ensure their energy provider is complying with power quality clauses of their contract. These requirements are onerous to manage without simple, effective analysis and reporting tools. To acquire the necessary data means depending more on connected systems, which raises the risk of cyberattacks.

The new era of intelligent power

Due to a lack of visibility into power and equipment conditions, most critical facilities are unaware of these risks. Many new and legacy facilities still use only a rudimentary level of technology to help prevent power system failures and minimize operational costs, usually on a reactive rather than proactive basis.

Fortunately, there are now cost-effective ways to digitalize your power system fully. You may even have many smart devices in place already, such as digital power meters and smart circuit breakers. You just need to get them connected and working together with analytic applications to deliver the customized, actionable information each of your team needs at their desktops and mobile devices.

The payback for doing this can be very large and the period very short, especially when considering all dimensions of ROI that you can achieve. For example, you’ll uncover lots of opportunities to optimize energy use and cut costs, but you’ll also get earlier warnings of risks, recover faster from problems, streamline maintenance and reporting, and boost the performance and lifespan of your equipment. And cybersecurity best practices will give you peace of mind.

This has been the first in a three-post series. To learn more, download our white paper ‘Bringing critical power distribution out of the dark and into a safer, more reliable, and sustainable future. For more information on our innovation power solutions, you can visit our web page.

Editor’s Note: This post was originally published on August 18, 2018, and has been recently updated for accuracy and comprehensiveness.