Big challenges call for serious solutions

Efficient and effective operation of today’s electric energy distribution network is a lot different than managing a bulk power transmission network or, for that matter, a previous-generation distribution network.

Today’s distribution management technology must deal with meshed and radial, balanced and unbalanced networks with rapidly- and continuously-changing topologies and demand profiles. To meet reliable energy goals, it must offer advanced functionality such as Volt/VAR optimization, fault management (FLISR), near-term load forecasting, and support for distributed energy resources and highly variable renewables.

Enter the Advanced Distribution Management System, the ADMS – not your father’s distribution management system.

To perform the functionalities necessary for reliability under today’s distribution network challenges, the ADMS precisely defines a network model that –

  • represents all elements involved in distribution system operations and reflects the as-operated state of the network, typically based on the as-built state maintained by an enterprise Geographic Information System (GIS)
  • uses telemetered network data and applies high-performance data management for quick and efficient analysis
  • includes a very fast load flow algorithm that can resolve an unbalanced network, using ever-changing data telemetered from the field

The ADMS seamlessly merges this modeling with a field-proven distribution SCADA system that dependably manages the field data and an outage management system (OMS) that supports the creation of switching orders. This integration creates a unified and secure solution that provides dispatchers, engineers, and others who operate and manage the network with a single control room interface, even as the network grows.

And, it supports distributed energy, enabling the utility to grow and accommodate the renewable generation key in a sustainability strategy. Watch for my next post, for more on ADMS.