Arresting the surges in lightning strikes


There is widespread ignorance of lightning protection systems, which are often inadequate or non-existent. Surge protection devices like surge protectors lies at the heart of effective, comprehensive lightning protection systems. We consider why.

Lightning is the single biggest cause of damage to and destruction of electrical and electronic equipment in industrial facilities, commercial buildings, and homes. The fact is borne out by stats from insurance companies worldwide and telecom operators like France Telecom. The US National Lightning Safety Institute compiled a list of the costs and losses attributable to lightning in 2008.

Types of lightning strikes and transients

Lightning causes damage because it generates electrical transients (very short-lived events) like overvoltage and power surges and strikes.

Direct lightning strikes can generate millions of volts and hundreds of thousands of Amps and high-level overvoltage transients. They may seriously a buildings’ physical structure, electric distribution system, and cause fires. And the electromagnetic pulse energy of a lightning strike can affect electrics and electronics 2 kilometres away!

Indirect lightning strikes are one, though not the only, cause of low-level transients. Strikes in the vicinity of a building and on powerlines lead to overvoltage induced by the electromagnetic fields from the lightning current. Though typically less damaging than direct strikes, they are enough to melt electronic circuitry.

Switching inductive, capacitive and resistive loads also generates harmful overvoltage.

Ignorance of lightning protection

Both professionally and personally (as a member of the French Lightning Protection Association (APF), my number one concern is to raise awareness of lightning. Although I have been a member for well over 15 years, I still wonder at the widespread ignorance. The vast majority of homes have no lightning protection at all. And many residential and commercial buildings, built as late as the 1990s, have no surge protection devices. These became compulsory only in 2005 with the introduction of international standard EN 62305.

EN 62305
Part 1, General Principles, is an introduction
Part 2 defines risk-assessment-based level of lightning protection
Part 3 describes damage caused to life and structures
Part 4 addresses electrical and electronic systems within structures.

Confusion between primary lightning and surge protection devices

One misconception that needs to be urgently dispelled is the widespread confusion between lightning rods and surge arresters. People think they the same thing. Consequently, they believe that lightning rods protect buildings and their occupants. They don’t. At least not fully and not on their own.

A lightning rod is a primary lighting protection device – along with overhead earth wires and Faraday cages. It is a metal rod perched on the roof of a building that provides a low-resistance path to earth. It is connected to a down-conductor which runs electric currents down to a nearby conductive grid buried in the ground.

Primary protection, however, means partial protection. The lightning rod’s conductive grid is connected to the primary busbar in the switchboard, so lightning current flows from the ground into a building’s power distribution system.

Nor do lightning rods protect against surges arising from the induction effect of lightning’s electromagnetic field or from strikes to overhead lines or into the ground nearby.

That is where surge arresters (also known as surge protection devices [SPDs]) come in.

How surge arresters work

Surge arresters protect power distribution and telecommunication systems from high voltage surges caused by lightning strikes. They arrest surges currents at their point of installation, discharging them to earth so that they bypass critical equipment.

Used together with lightning rods, surge arresters form a building’s lightning protection system.

Surge arrestors also afford protection against overvoltage resulting from constant self-inducted and capacitive load switching. And because electronics are ever more critical and ubiquitous, surge protective devices play a twin role : they protect microprocessors against wear-and-tear and lightning.

Types, or class, of SPDs and their circuit breakers

You may have heard contractors and other electricity professionals talk about “classes” or “types” of SPDs. Different types and combinations thereof are installed in different protection zones to meet different needs. Let’s briefly consider Types 1 and 2.

  • Type 1 arresters are generally installed in the service entrance switchboards to protect low-voltage equipment from direct lightning strike overvoltage.
  • Type 2 SPDs should be fitted to all the distribution panels that serve critical equipment. They afford protection against the residual effects of lightning strikes and switching overvoltage.

To avoid any risk of permanent overvoltage which would short-circuit and damage a switchboard, the surge protective device must itself be protected by a disconnection circuit breaker (MCB).

Ideal lightning protection system

Part 4 of EN/IEC 62305 made surge protectors compulsory in buildings where lightning rods are installed. The most comprehensive lightning protection system should therefore comprise :

    • A lightning rod
    • A surge arrestor
    • A circuit breaker

 

Conversation

  • What kind of lightning arrester to be installed in an overhead catenary system in a railway. thanks

    • Hello
      Please refer to the new standard EN50526-1:2012 where the right SPD specifications are described. BR

  • Dear sir,
    Please , suggest ,in 33kv outdoor s/s at O/G end of underground cable,does lightening arrestor require?

    Regards,

    P P Tiwari

    • Hello
      Sorry but I focused the article on Low Voltage electrical distribution network. I’m not specialist on HV. Please refer to SPD HV standard ANS C 62 11

  • Hi there,

    What would be the typical voltage levels that an indirect lightning could produce? I notice that SPD Type II devices can provide protection levels from 2.6kV, would that then be the typical voltage level of an indirect strike?

    Kind regards

    Karlos

Comments are closed.