Why Manufacturing Sector still Relies on SCADA for Operations?

Supervisory Control and Data Acquisition (SCADA) can be explained as a control system architecture that employs the functions of computers, networked data communications, and graphical user interfaces to facilitate high-level process supervisory management. It additionally uses other external devices such as a programmable logic controller (PLC) and discrete PID controllers to monitor the process plant or machinery. The use of SCADA software has also been acknowledged for management and operations of project-driven-process in major industries.

SCADA systems are essential for modern business. In fact, SCADA systems normally allow a business to function far more efficiently and safely, and at a significantly lower cost. These systems offer real-time details, which further cements itself as one of the top regulatory systems. Key industries utilising this technology include water and wastewater management, oil & gas, and power utilities. Other industries include telecom and aquaculture as well. Some of the fundamental benefits of using this system in your manufacturing business can be elucidated below:

Cost

The manufacturing industry deals with ageing infrastructure and the escalating cost of ownership. So, a real-time lens with a software adept enough to harness an increasing volume of data helps minimize downtime, shutdowns and facilitates preemptive maintenance issues. This is essential in negating capital expenditure, while – at the same time – maximising asset performance.

Adaptability

As the industrial landscape continues to advance and organisations re-invent themselves with a focus on making themselves future-ready, adaptability and flexibility are extremely relevant for continued efficiency and long-term functionality. The ability to scale systems to create virtual representations is also a key factor to help organizations deploy a cost-effective step-wise approach to digital transformation.

Risks

Ensuring SCADA software is relevant and in line with changing industry standards and guidelines will continue to be one of the most critical factors in securing vital infrastructure and helping to negate cybersecurity risks and other haphazard situations in the cyber world.

Support

In the age of such change and evolution, making sure that an active support agreement is present is not only the clearest insurance policy you could have in helping to maximise the value of existing SCADA investments, but also assures that as operations grow through digital transformations, support and advice is present – especially when it is required.