This audio was created using Microsoft Azure Speech Services
If you are a technology junkie, you must have heard of the term IoT. It has taken the world by storm and has sparked so many conversations. But for those who don’t know what IoT is, it stands for the Internet of Things, where everything from household chores to industrial practices can be made at the touch of a button. All you have to do is connect devices with automated systems as they help in gathering information, analysing and creating necessary action. IoT is an umbrella term, and Industrial internet of things comes under it which mainly focuses on the manufacturing sector.
It has the potential to amplify output and efficiency. Since the commencement of IIoT, a behavioural shift has been across industries. Therefore, it does not restrict itself to hardcore technology but has extended its arms to other sectors like Agriculture and retail. IIoT can permeate into the manufacturing industry so rapidly because the products, markets, and processes have a high inclination to adopt it quickly and show maximum results. Also, the number of devices and applications to be connected can be customised as per the need.
Some of the facts you need to know before diving in the pool of Industrial internet of things
- Machines that are equipped with IoT can transmit operational information to the end user. It also helps operation managers and factory heads to manage the factory units and take advantage of process automation and optimisation. Along with this, a digitally connected group will establish a better line of commands and help identify key result areas (KRAs) for managers.
- Industrial Internet of Things (IIoT) has opened many doors, as the technology is so advanced it will improve the process cycle time and provide data security. Another way it has helped the employees is by HMI. It is a system which acts as a link between the human operator and the machine. HMI software are usually controlled by a human operator who then helps you interact with the device. Its primary purpose is to solve the issues faced by the operator and provide with an on-premise solution.
- The Industrial Internet of things connects the heavy machinery to make operations viable. The next-gen manufacturing equipment uses built-in sensors and sophisticated programming to perform. One of these benefits includes predictive maintenance. Predictive analytics can forecast potential issues before they happen and take preventive measures.
- Another added advantage of automating the industry sector is bringing into force the SCADA It helps in gathering, monitoring and real-time process data from the connected physical interface. Also, record events and data into a machinery log file. Moreover, it Directly interacts with devices such as sensors, valves, pumps, motors, and more through HMI software.
- IoT can also help improve overall workers safety and security in the plant by monitoring the Key Performance Indicators (KPIs) of health and safety, like the number of injuries and illness rates, near-misses, short- and long-term absences, vehicle incidents and property damage, etc. Thus, effective monitoring ensures better safety.