How Mivan construction is changing the game for homebuilders

When you think about building a new home, images of bricklayers and wooden frames probably come to mind. There is, however, a faster, more efficient method revolutionizing the construction industry. We’re talking about Mivan construction, a technique that’s proving to be a real game-changer for homebuilders everywhere in India.

For instance, Mivan construction has proven to offer total cost savings of about 12.5%. Introduced by the European-based Mivan Company Ltd. in 1990, this method may significantly impact Indian real estate in the coming years.

 homebuilders

What is Mivan construction?

Mivan construction is a method that utilizes aluminum formwork to create a sturdy, uniform structure quickly and efficiently. The process involves assembling pre-engineered aluminum panels to build the walls, floors, and ceilings of a building. Concrete is then poured into this mold, and once it sets, the formwork is removed, leaving behind a robust structure.

Why is Mivan construction important for homebuilding?

Not only is Mivan construction economical and timesaving, but it also brings several other benefits to the table, including:

  1. Speed and efficiency: Traditional construction methods can often take several months or even years to complete a single home. Mivan construction, on the other hand, significantly reduces construction time. Since the formwork can be reused and the process is streamlined, multiple units can be built simultaneously, making it ideal for large-scale housing projects.
  2. Quality and consistency: One of the biggest challenges in construction is ensuring that each unit is built to the same high standard. With Mivan construction, the use of aluminum formwork ensures that every wall, floor, and ceiling is uniform and precise. This consistency translates to higher-quality homes that require less maintenance over time.
  3. Cost effectiveness: While the initial investment in aluminum formwork might be higher than traditional materials, the long-term savings are substantial. The speed of construction reduces labor costs, and the durability of the structures means fewer repairs and renovations are needed down the line.
  4. Sustainability: Mivan construction is also more environment-friendly compared to traditional methods. The precision of the formwork reduces waste material, and the use of concrete and aluminum, both of which are recyclable, makes this method more sustainable.
  5. Safety: The durability of structures built using Mivan construction makes them more resistant to natural disasters like earthquakes. This is particularly important in areas prone to seismic activity, providing homeowners with an added layer of security.

Meet Miluz Lara: The switches and socket outlets made for modern buildings and Mivan construction

With the residential construction industry in India grappling with ever-increasing delays and workforce shortages, Mivan construction offers a swift and efficient alternative. However, its popularity comes with challenges—like the need for compatible electrical installation solutions for its thinner walls. These solutions are not widely available in the market just yet.

Miluz Lara, our new range of switches, sockets, and advanced connectivity devices are made to tackle this challenge as it is specifically designed for modern buildings with thinner walls, such as those using Mivan construction. Made in India, this range has been rigorously tested to provide top performance in local environments and conditions.

Key features of Miluz Lara:

Perfect compatibility with Mivan construction: Our Miluz Lara switches are designed to fit seamlessly in newer (40 mm) and conventional (50mm) metal boxes. They also feature a unique volcanic curve design that provides ample wiring space, making them perfect for Mivan construction.

Enhanced aesthetics: Their dew-drop-inspired design not only looks beautiful but also prevents dust and dirt accumulation, ensuring your space remains both functional and stylish.

Unmatched durability: Crafted with durable copper, the Miluz Lara range is built to last. Each product is tested to withstand up to 200,000 clicks, which equates to about 30 years of use at 15 clicks per day.

Improved safety: Safety is paramount which is taken care by the features like “no single pin insertion” in sockets, IP20, etc. Also, the use of material like thermoplastic makes it fire resistant.

Better connection: This range is fully compatible with the Wiser™ smart home system that can optimize energy usage and help homeowners live more comfortably.

Innovative functions: Miluz Lara switches offer the latest in smart home technology, including air quality indicators, voltage surge protectors, and USB A+C connectivity.

Improving modern living spaces

At Schneider Electric, we’re dedicated to making homes more comfortable and functional with our innovative solutions. Our latest offering, the Miluz Lara range, embodies this commitment with features designed for modern homes.

With our solutions, we aim to create spaces that are not just functional but also more comfortable for homeowners and profitable for builders.

To learn more about our solution, visit our website.

Add a comment

All fields are required.