Why is my energy bill so high and how do I fix it?

If you’re wondering why your energy bill is so high, you’re not alone. Many areas have seen higher energy bills, and according to the U.S. Energy Information Administration, electricity prices have risen faster than the rate of inflation since 2022, and they are forecasted to continue increasing through 2026.

In my decade or so of working in the residential energy sector, I can tell you that this is a dramatic spike. Fortunately, there are several solutions that help, especially for homeowners looking ways to reduce home energy bills.

In this article, I’ll explore 3 reasons why energy bills are spiking and introduce a major energy-saving tip you probably haven’t heard about.

Why is my energy bill so high? An explanation

1. Current events

There are many reasons why electric bills are higher these days. We’re dealing with supply-chain issues, geopolitical conflict is affecting energy prices, and extreme weather events – like those that impacted the Texas grid – are becoming more frequent. All have an effect on your higher energy bills, whether with increased consumption or increased price.

2. Higher rates on additional energy consumption

But there’s another, often unexpected reason for higher energy bills: higher rates on that extra consumption. With most household items, the more you buy, the more you save per unit – hence, the logic of bulk purchases. But electricity is different.

The reason why your energy bills are so high is that the more electricity you use, the more you pay per unit of electricity. So, if your energy bill is twice as high as usual, it’s not simply because you used twice as much electricity. It’s more likely that your utility is charging you more per kilowatt hour for that extra energy beyond your typical base rate.

If your typical electricity usage is 900 kWh per month, and your average cents per kWh is $0.15, you would pay something around $135 per month.

Let’s say recently you’ve used 30% more energy, or 1,170 kWh. If your utility starts charging you a higher rate of $0.25 cents per kWh anywhere above 1,000 kW, you’ll end up paying $192.50. But $192.50 is far more than 30% – the amount of additional energy consumed – it’s 42.5%. That extra 12.5% is what we experts in the industry call a “double whammy.”

 Under 1,000 kWOver 1,000 kW
Electricity consumption900 kWh1,170 kWh
Rate: Cents per kWH$0.15$0.15 (and $0.25 for 170 kWh)
Total electric bill$135$192.50
The increased rates charged for per kilowatt hour of extra energy beyond your base rate are one reason why your energy bills could be so high.
Percentage increase in your electricity consumption (kWh)30%
Percentage increase in your electric bill ($)42.5%

3. Energy waste

Another reason your energy bill could be so high is that you’re wasting a lot of energy. According to the Department of Energy, Americans could be spending up to $400 annually on wasted energy. To reduce home energy costs, keep reading to learn how you can better monitor and regulate energy usage in your home.

Ways to save energy at home that go beyond the basics

Most of us know about common ways to save energy, so I won’t spend much time telling you to turn off the lights.

However, one question I hear often is, “Do you really save energy by unplugging appliances?” The short answer to that is, “Yes.” According to the Lawrence Berkeley National Lab, standby power accounts for as much as 10% of your total home energy use – another reason why your energy bill may be so high.

Many homeowners underestimate the impact of appliances on energy bills. When it comes to appliances, my advice is to balance effort and reward. Unplugging your cell phone charger may only save a few cents a month, so you could let that go. But there may be an old heater or spare TV in your basement that’s eating up $10 a month. In addition, upgrading to ENERGY STAR-rated models and maintaining HVAC systems can help lower energy bills.

How to discover hidden electricity waste

But wait, how would you ever notice this basement energy hog? What about other sources of waste? Unless you want to look up the power draw for each one of your electronics, it’s going to be tough to make informed decisions about how to save energy, either through unplugging appliances or other actions.

There’s an easier way to do this. It involves something called a home energy monitor. The Schneider Energy Monitor (formerly Wiser Energy™ Home Power Monitor) is special because it can measure electricity use for each device in your home. The Schneider Energy Monitor combines an app with an internet-connected smart device that easily clips onto your home’s electrical panel.

The cool thing about the Schneider Energy Monitor is that it can make even your 25-year-old dishwasher “connected.” The system’s machine learning detects the dishwashers’ unique electrical signature, and then tracks it whenever it turns on and off. It’s like a wearable fitness tracker, but for your home.

Once it learns your home’s devices, it monitors when they turn on/off, how long they run, and how much electricity each one uses. From there, you can set monthly savings targets, spot energy waste, and estimate your next energy bill. It answers the main question of this blog post, “Why is my energy bill so high?” by showing you exactly where you’re using energy, and thereby demystifying your bill.

In the video below, a Schneider Energy Monitor user explains how the system works. He used the app to find energy waste hiding in unexpected places, such as a refrigerator that was drawing extra energy. The culprit? A failing compressor.

Understand why your energy bill is high with real-time monitoring from the Schneider Energy Monitor

How to reduce energy bills and minimize unexpected expenses

Homes are full of surprises. An oven gets left on. An AC unit fails right before a heat wave. Your teenager sneaks home after curfew. In each of these cases, the Schneider Energy Monitor gives you clues to the mysteries. The app allows you to:

  • Receive custom alerts when an oven is left on, a refrigerator door is left open, and other safety or nuisance issues
  • Predict and detect appliance problems (e.g., a furnace that takes three ignition cycles to start instead of one, a clogged filter) before they fail
  • See an activity log of your home’s energy use (like when exactly did the garage door open last night when your teenager got home?)

The basis for smarter home energy decisions

Until now, there were still so many unknowns when it comes to your electric bill.

Fortunately, with technology like Schneider Energy Monitor, you can finally begin to see what’s going on with each appliance and why your energy bill might be so high. Armed with that intel, you can make better decisions about what appliances to unplug, what light bulbs to replace, what appliances need servicing, and so much more.

For a deeper dive into the world of reducing energy bills, visit the Schneider Energy Monitor page. You’ll find product information, app features, and other handy information.

Find more cost saving tips to lower your energy bill in our next blog:

Conversation

  • Same house, same IoT items, electric bill is 60% lower this year for only one reason….brand new HVAC system, went from older SEER 12 to SEER 19 made all the difference.

  • Hi my son moved in in March and my electricity bill has doubled or tripled. How can I figure out what happened?

Add a comment

All fields are required.