Every organization sits on a goldmine of operational data—especially within its electrical and energy systems. Beneath the hum of daily operations, meters and sensors record thousands of data points every second. Yet for most companies, this information remains untouched, an invisible drag on efficiency and profitability. This dark data is one of business’ most underused assets. When analyzed and applied, it becomes a strategic driver of resilience, sustainability, and profitability.
Energy data is a new strategic currency for decision-makers across the enterprise. Studies suggest that as much as 80% of operational data is never analyzed or acted upon. For electrical systems, this means missed opportunities to reduce costs, strengthen uptime, and accelerate sustainability goals. Connecting the dots turns scattered data into actionable insights through integration, artificial intelligence (AI), and cross-team collaboration.

What is dark data?
For the sake of simplicity, dark data is information from connected devices that isn’t actively used. In energy systems, dark data often appears as:
- Meter logs that are collected but never correlated
- IoT or submeter streams left uncommissioned
- Time-series data disconnected from metadata (like production schedules or occupancy)
- System registers or diagnostics never integrated into analytics
However defined, the waste is staggering. Unused data costs businesses an estimated $3.1 trillion annually in lost revenue and productivity. That’s money and opportunity left on the table.
What keeps operational data in the dark?
One major barrier to utilizing operational data is organizational silos. Across industries, 98% of companies report that their data is siloed, with 69% identifying their data as being trapped. Facilities teams manage energy consumption, HR tracks headcount, finance handles utility bills, and sustainability groups focus on reporting. Each department has its own view, but without collaboration, the full picture is never realized.
Resourcing is another obstacle. Even when teams have access to the right data, they may not have the time or tools to analyze it effectively. In many cases, systems are left unmanaged as experienced staff retire and new employees are never trained to use them. Information is collected but forgotten, creating blind spots that only widen over time.
The result is a paradox: companies hold more data than ever before, but without a strategy in place to utilize it, they are operating as if the insights don’t exist.
The AI advantage
The rise of artificial intelligence (AI) is beginning to change the equation. With the help of AI, data analysis that once took months of manual effort can now be achieved in minutes. AI can rapidly digest vast amounts of energy data, surfacing anomalies, trends, and opportunities that would otherwise go unnoticed.
The impact becomes even greater when AI is paired with metadata. Imagine overlaying occupancy levels, production schedules, or high-demand periods on top of energy consumption data. Suddenly, spikes and dips start to make sense. Inefficiencies can be pinpointed, maintenance needs anticipated, and energy strategies refined with precision.
This is not about replacing human expertise but amplifying it. AI frees teams from the drudgery of data collection and correlation, allowing them to focus on interpreting insights and making better decisions.
Turning dark data into daylight: A strategic roadmap
When organizations shine a light on their hidden data, they unlock benefits across multiple dimensions. Here are 6 steps to convert latent data into actionable information:
1. Audit what you already have
Start light. Assemble utility bills, meter logs, and historical datasets. Even data you think is “boring” can unlock insights when combined.
2. Overlay metadata
Add context—such as production volumes, shift timing, occupancy, and weather—to give structure and meaning to raw numbers.
3. Look for early correlations
Simple cross-checks (e.g. energy per unit produced) often reveal patterns or outliers ripe for investigation.
4. Prioritize quick wins
Target a high-impact zone (e.g. one facility or system) and prove value early. These successes build momentum.
5. Roll out AI in phases
Utilize machine learning to scale anomaly detection, predictive maintenance, and usage modeling—but integrate it gradually, refining models with domain-specific feedback.
6. Embed a data-centric culture
One of the biggest shifts is in leadership mindset. Energy data must be viewed like capital or talent—not a byproduct, but a strategic resource.
By implementing this roadmap, energy data becomes more than an operational detail. Instead, becomes a lever for financial, operational, and reputational value that can transform business outcomes.
The strategic value of energy data
Used strategically, it provides valuable insights that inform decision-making across the business, supporting cost savings, reliability, and sustainability goals. In this way, energy data shifts from being a byproduct of operations to a key resource for achieving competitive advantage and long-term success.
Why it matters now (and in the near future)
- Competitive differentiation. As more businesses adopt ESG and energy targets, those who can connect usage to action will outpace those still in the dark.
- Regulatory and carbon risk. Data storage and digital operations have carbon and compliance costs. Slashing dark data isn’t just efficiency—it’s decarbonization.
- Rising compute demands. The cost and scale of compute and storage infrastructure are ballooning: enterprises must extract maximum value from existing data stores.
A mindset shift for leaders: Looking ahead to daylight
The biggest barrier to effectively utilize this data is often not technical but cultural. Too many organizations assume that energy consumption “is what it is” and can’t be changed, so why pay attention? Nothing could be further from the truth
The shift in thinking must be this: Energy data is not a byproduct, it’s a resource. Like capital or talent, it demands active management. When leaders treat it as such, they move from reactive decision-making to proactive strategy.
Over the next 2–3 years, organizations that convert dark data into daylight—not just in energy, but across their entire systems—will outpace their peers in resilience, margin, and sustainability.
By breaking down silos, applying AI-driven analysis, and fostering cross-team collaboration, they can unlock value that many competitors overlook.
Your data holds hidden potential—Schneider Electric can help you bring it into the light. Contact our team to learn how.
Add a comment