Simplifying the new IEC TS 62271-320: A specifier’s guide

Introduction to IEC TS 62271-320 

The newly published IEC TS 62271-320 is a valuable tool for consulting engineers working with high voltage switchgear. It brings structured guidance on environmental performance, aligning with regulations that are increasingly being introduced. Focused on Environmentally Conscious Design (ECD) and Lifecycle Assessment (LCA) including material efficiency, it enables engineers to embed sustainability into projects from the start.  

By following this standard, consultants can ensure that each stage of a product’s lifecycle – from manufacturing to end-of-life – is assessed using consistent, comparable methods.  

Understanding Lifecycle Assessment (LCA) 

At the heart of the standard lies Lifecycle Assessment (LCA), which quantifies a product’s environmental impact – especially climate change impact category, commonly referred to as greenhouse gas emissions – across its full life. IEC TS 62271-320 ensures that comparisons between products are based on functional performance, not just technical requirements, allowing fair benchmarking and better decision-making when precautions for comparability are taken into account.  

This LCA framework covers every phase of the product journey, helping engineers create more sustainable, efficient designs.  

Environmentally Conscious Design (ECD) 

IEC TS 62271-320 promotes eco-design by integrating principles that reduce waste and pollution and improve material and energy efficiency as defined by the horizontal guide IEC Guide 109. It encourages a holistic design approach, addressing environmental impacts throughout the whole lifecycle.  

It also aligns environmental goals with product standards, giving engineers a harmonized path to sustainable switchgear development.  

the-image-presents-a-graph-featuring-improvement-strategies

Product-specific rules and harmonization 

The specification introduces product-specific rules (PSRs) that ensure LCAs are accurate, reliable, and consistent. By harmonizing with broader LCA common rules (PCR) from standards such as IEC 63366, which reached consensus among 100% of involved countries at the latest stage before publication, these specific rules (PSRs) simplify compliance and improve transparency.  

Engineers can use this structure to compare products fairly and to benchmark performance against industry-wide environmental expectations.  

Extrapolation rules and material declaration 

To account for product and location variations, extrapolation rules help adjust LCA results based on parameters like weight, electrical resistance, energy mix, or carbon emission of electricity mix, etc. This ensures assessments remain precise even across product families and within product ranges. 

The standard also reinforces the material declaration of regulated substances, ensuring transparency in the substances used and helping comply with international environmental regulations.  

Mission profile and reference service life 

A key feature of the standard is defining a mission profile that considers operating conditions of a product, as well as its reliability and durability, in accordance with the reference service life used for LCA.  

Understanding real-world usage conditions allows for better design decisions and improved lifecycle performance.  

Material efficiency: CO2e and avoided emissions. 

High-voltage equipment is an important part of the infrastructure used to transport or distribute electricity. It is expected to have a long service life, which mainly justifies the 40 years considered as reference service life for LCA. Therefore, material selection at design stage and end-of-life phase are crucial for material efficiency, as considered in this specification. Recovery aspects related to recycling rate and recycled material content are considered as potential loads and benefits beyond the LCA system boundary. 

Conclusion

IEC TS 62271-320 equips specifiers with practical tools to design and assess high voltage switchgear in line with today’s sustainability demands. By adopting this standard, consulting engineers can ensure their projects are not only compliant but also forward-looking and environmentally responsible.  

Stay Updated
If you want to keep up with the latest developments in standards and regulations, be sure to visit our website regularly for news, insights, and expert analysis: https://www.se.com/ww/en/partners/consultant-engineers/

Add a comment

All fields are required.