Which Smart-UPS battery is right for you?

Imagine this: it’s a typical workday at home, and you’re in the middle of creating an urgent report on your PC or laptop. Suddenly, the power goes out. Even though it was less than a minute, your computer goes dark, and you lost all your unsaved work. Frustration sets in as you realize that because you do not have a backup power source, all of your day’s productivity is completely lost. To make matters worse, you’re going to have to start all over again.  

Or perhaps you’re running your small business, processing orders, tracking supplies and all the other things that go into a good business. The numerous demand on your system causes a brief power outage. Your essential devices – networking equipment, phones, computers, POS systems and more are left vulnerable. You start to worry about the success and longevity of your business. 

These scenarios highlight a common issue many face: the lack of a reliable backup power solution. Whether it’s for your business or home, the need for uninterrupted power is critical. That’s where APC by Schneider Electric’s uninterruptible power products come in. Our Smart-UPS Line Interactive and Smart-UPS Online solutions ensure that your devices stay powered during outages, protecting your work, your home, and your peace of mind. But which solution is right for you? Whichever solution you choose, know that it begins with APC, the brand that consistently sets the industry standard with over 40 years of trusted excellence. 

Smart-UPS Online vs Smart-UPS Line Interactive  

The first step is to define uninterruptible power supplies, commonly known as UPS. UPSs are essential devices that provide backup power when the main electrical supply fails and ensures your critical systems remain operational. Not only that but a UPS can sidestep system downtime or be safely shut down during power outages, preventing data loss. While Smart-UPS Line Interactive and Smart-UPS Online both provide them, Smart-UPS Line Interactive provides a more cost-effective solution for home users, small/medium businesses and others looking for power protection. For those that have more at stake, Smart-UPS Online offers a higher level of protection, but at a higher cost due to its double-conversion function that provides cleaner power.  

The Smart-UPS Line Interactive models are a core portfolio known for their efficiency and cost-effectiveness. They offer reliable output power and utilize automatic voltage regulation (AVR) to correct minor power fluctuations without switching to battery power, enabling a longer battery life. They also provide battery power during brief interruptions, such as brownouts or power spikes, to ensure continuous power is delivered to your equipment. These units are advantageous for small-to-medium businesses, with easy installation and maintenance, to ensure your equipment is always protected.   

The Smart-UPS Online models provide the highest level of power protection available. They provide pure sine wave output power by utilizing a double-conversion method. The units convert incoming AC power to DC power, then back to AC power, to continuously deliver clean power to your equipment. They also feature zero transfer time between switching from incoming power to battery power, ensuring there is no equipment downtime. This methodology makes them ideal for applications with sensitive and critical equipment, such as data centers and healthcare facilities.  

Which Smart-UPS is right for your business? 

In addition, determining the type of UPS you need, you also need to consider the application and general power conditions at your site.  

If input power is stable and free from frequency or voltage distortion, and the connected equipment is not extremely sensitive or critical (like point-of-sale terminals or network equipment), then Smart-UPS Line Interactive systems will fit your needs. They offer reliable power and easy management. The need to save money while still performing at the highest quality possible is a major reason to choose Line Interactive.  

For environments and equipment with higher sensitivity and critical operations, Smart-UPS Online systems are the optimal choice. These systems are designed to provide the highest level of protection against power disturbances. Despite their higher cost, they offer unparalleled protection and advanced features, such as double-conversion technology, which ensures a continuous and clean power supply. For these reasons and more, this makes them ideal for supporting critical applications such as data centers, medical equipment, and high-end servers.  No matter which option you choose, the only thing that you’re going to lose is the anxiety of watching a day’s work accidentally go bye-bye. For more information on which battery is right for you, utilize our UPS Selector.

Tags: , , ,

Add a comment

All fields are required.

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.