Why waste your energy?

Automation systems reliably and effectively build quality products. To do so requires energy, the quantity of energy is determined by its design efficiency (equipment and process) but also by the operational efficiency (equipment health and quality of plant operation).

There are many factors that influence the energy consumption which makes it a rich source of information about the operation of the plant. Many companies choose rather than find its value to accept energy as a cost required to deliver their production.

These customers are “wasting their energy”. Are you?

Energy the forgotten variable

To say industrial companies are wasting their energy is not to say that their process is not efficient. Improvements in equipment selection and process on industrial sites has resulted in significant reductions in energy intensity (consumption per unit of production). It is to say that they are failing to leverage the potential benefits that can be achieved by unleashing energy data within their control systems.

Most automation systems work by applying “effective control” (meets or exceeds production targets) to a “design efficient” (efficient equipment and process) system.

Modelling this as a control loop shows the relationship between the output required by the controller and the effort applied or energy consumption within the process. The energy consumption is an effective measure of the effort required to execute the process.

While output information is available in most control systems, it is rarely analyzed. At best, the total energy controlled by the outputs is displayed on energy dashboards to show plant efficiency. Energy information can be much more effective when brought into the automation system to ensure the efficient operation of the control system.

Energy Aware Control Systems

Adding energy data to ensure efficient operation of the control system is not about slowing production. Energy measurement provides insight on how efficiently the plant systems are operating. Doing so allows more production by avoiding downtime and lowers cost through reduction of inefficient operational periods.

To ensure there is no loss of production “efficient control” is added as a child control loop to the existing effective control. The efficient control works by monitoring the effort which is being applied to the process for a given task and comparing this to previous expectations. The output of the controller is focused on the selection of more efficient paths or engaging the operator to resolve process inefficiencies as they occur.

Energy analysis at the automation system level removes the load on operators of monitoring energy values directly but enables the effect of many energy dashboard metrics, which are constantly monitored. It also allows timely action to be taken or appropriate people to be notified directly when overconsumption is occurring.

An example:

The impact of an energy aware control system can be seen on systems as simple as a pair of pumps emptying a sump. In this case the energy consumption is a combination of the efficiency of the pumps and of the piping system and so can detect issues across the complete system.

  • The wearing of pump components results in additional energy consumption for the same task over time. While many control systems try to simulate running the most recently serviced pump, energy measurement allows the selection of the most energy efficient pump and in doing so will reduce pumping costs.
  • The ability to quantify the decay in efficient operation of a pump can build a business case for lower maintenance or longer lasting components.
  • Maintenance of the pumps will improve efficiency; however failure to improve indicates a failure of the maintenance action (parts or execution). Running with ineffective equipment will require more effort and increase the chance of equipment failure.
  • Pump systems involve manual valves and draw water. A manual valve left not fully opened or a partially blocked input will increase energy consumption and detect situations that are not currently known.

Energy represents the effort being used in production. Increases in effort represent current inefficiency and potential future failure. An energy aware control system leverages energy data to detect problems before traditional measurement. Shouldn’t your operation be one step ahead?

Conversation

  • One of the ways of generating energy saving projects may have some parallels with Peter’s ideas: Why waste your energy?

    The method is deceptively simple. Your walk through the facility in a purposeful way. You notice devices that are wired or plumbed to use energy. If the device is running, ask: “Is this thing producing something of value right now?” It’s surprising how many things are “on” and consuming power and just waiting to do something productive, yet doing nothing of value at this exact moment. Example: a hydraulic system operates intermittently and with considerable on/off cycles. The hydraulic pump runs continuously. It does something of value (say) 70% of the elapsed time. The operators have become used to this and consider it normal. But when the equipment is idle, the pump still runs with no real value output. While it is running, it generates heat and causes the reservoir to warm until a cooling fan comes on to maintain the oil temperature. Now, we have two devices running. If enough heat is rejected, the a/c too will run and that makes 3 devices. What if we could more closely match the pump to the actual production? Possible energy savings. It might require a design upgrade to capture the savings. This may require additional resources but it’s still a possible project.

Comments are closed.