Power outages: Assess costs and risks before the lights go out

The recent Texas winter storm was a clear reminder that power outages are one of the leading causes of unplanned downtime for businesses, and that translates directly into lost revenue. So, taking steps to mitigate the impact of power outages should be considered an essential part of business continuity, and justifying the time and energy needed to address this challenge starts by understanding the costs associated with power disruptions and outages.

Like many other business decisions, coming up with an appropriate battery backup power protection strategy means assessing the risk of an outage as well as the cost of downtime. Let’s begin with the last part of the equation first.

city skyline

The cost of unplanned downtime

Estimating the cost of downtime means taking into account both direct and indirect costs. Direct costs are fairly straightforward, including:

  • Lost wages for employees who can’t be productive
  • Revenues that can’t be captured when systems are down, such as for retail establishments
  • Overtime wages to check or fix systems after the outage
  • Losses from damaged equipment
  • Time spent restarting equipment after an outage

The exact amount of the loss you might face will depend on various factors, including how much you pay employees, whether you use a lot of expensive equipment that may be damaged if not properly shut down and so on.

Indirect costs are a bit more difficult to quantify but include such things as:

  • Reduced customer satisfaction, as customers generally don’t like it when resources such as your web site are unavailable
  • Customers lost to competitors while your company was down
  • Damaged brand reputation
  • Negative public relations

You also have to determine whether the cost of downtime changes as the outage continues. For some companies, such as retail stores, the loss will continue at roughly the same rate for the duration of the outage. Others may experience little direct loss for a short outage because revenue is simply delayed, not lost completely. But those same companies may be subject to losses related to reduced customer satisfaction and brand reputation hits if the outage drags on.

With an assessment of the cost of downtime in hand, now you need to understand how probable it is that a power outage will occur at any given site, which represents your level of risk. The risk profile involves two variables: frequency and duration of events. The result of this exercise will help you determine how much power protection you need to help you ride through power outages of various durations without a significant business loss.

Access power outage resources

Make sure you’re not caught off guard when the lights go out. Have a plan in place to enable business continuity. Check out the UPS Buying Guide to learn about various battery backup options for different applications in businesses and even in homes now that more people work from home.

Previously published on September 5, 2017, updated on March 18, 2021