The building that gives back: Microgrids, headroom, and returns

Summary
  • Microgrids are not limited to building owners with sustainability targets. Under the conditions modeled, they can provide a financially viable infrastructure investment while also improving use of the distribution grid.
  • Returns depend on building type, local tariffs, solar resources, and system design.
  • The strongest cases recover their cost within a decade and continue to perform as electrification increases.

A commercial building with rooftop photovoltaics and a controlled stationary battery can generate, store, and dispatch electricity. By reducing demand on the grid, it can also release capacity for other uses without additional cost to the network operator.

Our latest research models microgrid deployment across 65 use cases in 13 regions and five commercial building archetypes. The results show attractive economics for on-site generation and storage in nearly every case tested. They also show how a well-designed microgrid can change a building’s relationship with the grid by reducing net imports, flattening the load curve, and freeing distribution capacity for other uses.

Office skyscrapers with a sunlit reflection Glass-walled building reflecting trees. This is shot with a composition to look up from a lower place.

Scope of this analysis.  All findings below refer to microgrids combining rooftop PV and a controlled stationary battery (BESS), deployed on top of a baseline of electrified, efficient buildings. The microgrid controller is optimized to minimize the building’s electricity bill – grid headroom recovery emerges as an additional, zero-marginal-cost benefit to system operators.

Electricity systems face growing pressure. In the United States, aggregated winter peak load is forecast to rise by more than 20% over the coming decade, driven by AI infrastructure, transport electrification, and industrial reshoring. In Europe, electrification is accelerating while connection queues lengthen and grid investment lags demand. More transformers, wires, and generation will be needed. Buildings can also help by using existing capacity more efficiently.

Microgrids can help buildings consume electricity more efficiently while also providing local generation and storage.

1. Energy Headroom: The grid benefit inside every roof

Grid utilization – the ratio of actual annual energy flows through a distribution transformer relative to its rated capacity – is a measure of how efficiently existing infrastructure is being used. Most grids run well below their theoretical capacity for the majority of the year, because infrastructure is sized to handle peaks that materialize only occasionally. A building that reduces its net grid imports, hour by hour, across the year, contributes directly to improving that utilization ratio and freeing up capacity for new connections.

This is what our analysis calls energy headroom recovery: the reduction in the annual area under the load duration curve that a microgrid creates through self-consumption and battery dispatch. The results vary by archetype and location, but the direction is consistent across all 65 cases. Buildings with large roof areas relative to their floor area – secondary schools, strip malls, small hotels – achieve the greatest effect, with energy headroom recovery averaging 22% of site capacity and reaching up to 35% in the most favorable conditions.

Key finding: Up to 35% of site capacity recovered as energy headroom

Across the modeled cases, rooftop PV and stationary storage reduce annual net grid imports and flatten the load curve. Distribution operators could use the resulting headroom to support new connections or defer some network reinforcement.

→  High-irradiance markets with high pre-deployment load factors – such as India and Australia – show the greatest headroom gains
→  Power headroom also recovered in over 55% of cases, reaching up to 60% of the site grid limit where demand charges or subscribed power tariffs apply
→  Buildings with lower roof-to-floor ratios (hospitals, large offices) deliver 5–10% energy headroom – meaningful at scale, even if more modest per site

Source: Minier & Utrilla Bustamante, SERI, April 2026   ·   Rooftop PV + stationary BESS, optimized for bill minimization   1 / 3

Flattening the load curve can also reduce the ramping required from conventional generation during peak demand. When a building limits sharp increases in net load, it reduces the need for fast-responding generation, which is often fossil-fueled. This system benefit is not specifically priced in this study, but it increases as more microgrids are deployed.

2. Self-Consumption: When the roof pays the bill

The primary financial driver of a microgrid is self-consumption – the proportion of on-site solar generation that is used directly by the building rather than exported to the grid. Every kilowatt-hour consumed from the rooftop rather than purchased from the network avoids the full retail electricity price, including any applicable taxes, grid charges, and markup. The stationary battery extends this effect beyond daylight hours: it stores midday surplus and dispatches it during the evening, when grid prices are typically higher and solar production has ceased.

In markets where electricity tariffs include a demand charge or subscribed-power component, batteries can provide additional value. By limiting the building’s peak draw, a battery can reduce both energy costs and demand charges. The financial effect is strongest where solar resources are high, and tariff structures place a significant cost on peak demand.

Key finding · Local generation can reduce electricity purchases and peak demand

On-site PV reduces grid imports during daylight hours. A stationary battery can extend self-consumption into the evening and, where tariffs include a demand charge, reduce peak demand. Local tariffs and operating profiles determine the combined financial value.

Dual Two modeled value drivers: self-consumption and peak-demand management

All 65 Use cases meet the modeled investor hurdle rates across the five building archetypes and 13 regions

→  Battery dispatches stored PV energy during evening peak-price windows, maximizing the value of each unit generated on-site
→  Where demand charges apply – US, Canada, France, Spain, India – battery peak-shaving adds a compounding savings mechanism
→  Microgrid controller is optimized for bill minimization; grid headroom recovery is a free co-benefit, not a cost

Source: Minier & Utrilla Bustamante, SERI, April 2026   ·   Rooftop PV + stationary BESS, optimized for bill minimization   2 / 3

Where a building’s baseload is low relative to rooftop generation, some solar output may be exported to the grid. Sell-back tariffs can compensate the building for this electricity, but simultaneous exports from many buildings may create upstream congestion around midday. Our analysis conservatively assumes curtailment of excess exports. Future network-management tools and energy sharing between nearby buildings could retain more of this value.

3. The investment case across 65 use cases

For building investors, a central question is the time required for a microgrid to recover its cost. Across the cases studied, the results are broadly positive. The system is sized to maximize the investor’s return, subject to hurdle rates ranging from 3.2% for public hospitals to 7.1% for secondary schools. Grid benefits emerge from that investment design rather than serving as its primary objective.

Key finding · Returns exceed the modeled hurdle rate in nearly all cases

Microgrid investments exceed the relevant hurdle rates in nearly all 65 modeled use cases. The analysis also finds that systems sized for 2025 electric-vehicle demand remain effective under the 2035 demand scenario.

55% of cases show simple payback of 5 to 10 years – the dominant outcome across regions

25% of cases show payback below 5 years – concentrated in USA West, Canada, and the UK

→  USA West, Canada, and the UK show the highest profitability; hospitals show the lowest – reflecting public-sector financing assumptions, not the technology’s merit
→  Battery replacement modeled at 15 years or 6,000 cycles; no PV degradation cost assumed over a 30-year project lifetime
→  Microgrid sized for 2025 EV levels continues to deliver strong returns at 2035 penetration – the investment does not become obsolete as fleets grow

Source: Minier & Utrilla Bustamante, SERI, April 2026   ·   Rooftop PV + stationary BESS, optimized for bill minimization   3 / 3

Two factors may affect returns over time. Electricity prices in many regions have risen since the tariff data used in the model was collected, so payback periods based on 2021 actual commercially available prices may be conservative. The analysis also tests systems sized for 2025 electric-vehicle demand against projected 2035 demand and finds that performance remains robust without additional capital investment.

The analysis identifies three sources of value: energy headroom recovery, self-consumption savings, and financial returns over the project life. Building owners receive the direct financial benefit, while grid operators gain additional headroom. This alignment may help support microgrid deployment when both grid investment and private capital are constrained. To learn more access the report, Grid Relief from Smart Buildings.

Add a comment

All fields are required.