Solar energy is all set to play a key role in how we power our homes. However, climatic changes due to global warming are fast becoming one of our greatest challenges.
We are hoping for sustainable sources because non-renewable sources are responsible for several environmental risks. This led us either to further adoption of clean energy strategies. Among the clean energy strategies, solar energy stands ahead among most of the options as it offers a better solution in nearly every way possible.
In this blog post, we will discuss why is solar energy important in today’s world.
What is solar energy and how does it work?
First, what is solar energy? Solar energy is a renewable source of power that comes directly from the sun. It is harnessed using solar panels, which are made up of Photovoltaic (PV) cells. These cells absorb sunlight and convert it into electricity via the photovoltaic effect. When sunlight hits the PV cells, electrons move within the material, generating an electric current. This electricity, known as solar power, can then be used to run household appliances, industrial equipment, or stored in batteries for later use.
Solar power systems can be installed on rooftops, open land, or integrated into building structures. In addition to generating electricity, solar panels can also be used for heating applications, such as water and space heating. Since solar energy is abundant and readily available, it reduces dependence on fossil fuels, lowers utility costs, and helps cut carbon emissions.
Exploring different types of solar power systems
Solar power systems come in a variety of configurations, each designed to meet different energy needs for homes, businesses, and large-scale operations. All systems are built around solar panels that capture sunlight and convert it into usable electricity, but how this energy is stored or shared determines the system type.
- On-grid solar power systems
- These are directly connected to the utility grid. Excess electricity generated by the solar panels is exported back to the grid, often earning credits through net metering. They are cost-effective and ideal for reducing monthly energy bills, but they rely on the grid during power outages.
- Off-grid solar power systems
- Common in remote areas, these systems operate independently from the network. Batteries are used to store extra solar power for nighttime or cloudy conditions. They provide full energy independence but require a higher upfront investment due to storage needs.
- Hybrid solar power systems
- A combination of on-grid and off-grid technologies, hybrid systems include batteries while still connecting to the grid. They maximize savings, offer reliable backup during outages, and enable efficient use of solar panels throughout the day. Each system has its own advantages, allowing users to select the best solar power solution based on energy goals, location, and resilience needs.
Advantages of solar energy
1. Solar energy is renewable
To understand why is solar energy important, we must look at its environmental impact. Solar power is clean, renewable, and does not emit greenhouse gases.
Unlike fossil fuels such as oil, gas, and coal, which release carbon dioxide into the atmosphere when burned, solar panels have no emissions when generating electricity. Solar plants produce so much clean energy that they even supply excess power to the grid during peak production hours! Due to its low carbon footprint (less than 0.05 pounds per kilowatt hour), solar energy is considered one of the cleanest and green forms available today.
2. Solar energy cuts down on expensive utility bills
The cost of solar energy is an important consideration, but so are the savings. As per the Solar Energy Industries Association (SEIA), the average American homeowner could save $20,000 over a 30-year period by installing a solar array. The average one-time investment for home solar arrays is about $30,000, and 50 percent of that cost can be financed with a loan or lease option over 15 years.
The cost factor is important when understanding why is solar energy important. If you are considering going solar, now’s a great time to make the transition! Utility companies are offering incentives such as cashback and tax credits to offset some of these costs and make going green more affordable than ever.
3. Solar energy systems are extremely low maintenance
Solar energy systems are extremely low maintenance. They do not need to be cleaned or serviced and will last for decades without needing to be replaced. This is because solar panels are made of glass and aluminum, which are materials that stand up to the elements well over time.
4. Solar panels are versatile
To understand why solar energy is important, one must understand its versatility. Solar energy can easily be used to power your home. The installation costs vary, but the size of the system you need depends on how much solar energy you want to generate. For example:
- A rooftop installation requires no ground-based equipment or maintenance, and it takes up less space than ground-mounted systems. You can also use a free-standing structure like a garage or shed if there is not enough space on your roof for the array (or if several people want access to their own panels). However, installing panels on your roof may require structural changes, such as adding added support beams or modifying an existing roof configuration.
- Ground-mounted systems are typically larger than rooftop ones because they include a fixed framework for attaching multiple panels together in an array that spreads out over an area greater than 20 feet by 20 feet. Depending on what kind of property you have (e.g., flat land versus sloped terrain), there might not be enough room between trees/buildings/roads, etc., which could prevent this type from being a practical option.
5. Solar energy reduces greenhouse gas emissions
Solar energy reduces pollution or greenhouse gas emissions. It is a renewable energy source that minimizes impact on global warming. It uses a renewable resource, sunlight, to produce electricity in a way that reduces harm to the environment or contribute to global climate change.
How is solar energy harnessed?
Solar power is harnessed by using the natural light of the sun. It is converted into electrical power and used to power homes, businesses, and industries in more than 70 countries worldwide. Solar energy can be used to provide electricity to homes, businesses, and industries. It can also be used to provide heat for water, space heating, air conditioning, cooking, and refrigeration.
To harness solar power, you need a solar panel that converts sunlight into electricity. These are called photovoltaics (PV) or solar cells. The solar panels are usually mounted on top of a building’s roof or on an outdoor wall facing the sun. However, solar panel systems can also be installed on the ground in areas without room for rooftop panels.
Solar panels create direct current (DC) electricity that must be converted into alternating current (AC) before it can be used by your home appliances or equipment, such as lights or appliances that use AC electricity from the grid, like televisions and computers. You then store the DC electricity in batteries until it is needed by your household appliances or equipment, such as lights or appliances that use AC electricity from the grid, like televisions and computers.
Solar energy is important because it assists us in reducing our carbon footprint and living more sustainably. To understand why solar energy is important, we must understand its major benefits:
- It reduces greenhouse gas emissions
- It reduces dependence on fossil fuels
These two reasons are at the core of why is solar energy important to the world right now. By using solar power, you can reduce greenhouse gas emissions by more than half (which leads to less climate change and warmer temperatures). In addition, you are contributing to a cleaner environment for everyone around you.
Transition to solar energy today!
Solar energy is one of the best ways we can help our planet. We know it is better for us and future generations, but it also helps reduce carbon emissions and keeps us from contributing to climate change. So, it is time to consider how we use energy and ensure that we are using renewable resources like solar power as much as possible. We at Schneider Electric provide start-to-finish solar power plant solutions for centralized and decentralized installations. In addition, we offer energy production solutions that help fleets and power generation facilities function more effectively, reliably, and successfully. We employ a one-of-a-kind combination of innovation and skill to fulfill our customers’ electricity production needs.