Machine and Process Management

Intelligence, Connectivity, Efficiency – the new ICE Age in Energy Management!

29.5K views 47 9 2.2K

INFOGRAPHIC: Has your organization taken the Efficiency Quotient test?

10.5K views 27 26 1.4K

Contactor requirements for hoisting machines under IEC 60204-32 – Part 2

9.9K views 3 0 1.1K

Innovation on the DCS Object Model

12.4K views 26 2 1.5K

Schneider Electric and Cisco are Natural Partners in Delivering the Internet of Things

15.9K views 269 32 2.7K

Redundancy puts backbone into the ring topology

15.1K views 52 5 2.0K

GUEST POST: Trends in the wireless automation market – Part 2

23.0K views 10 21 3.1K

Water Use Cycle: As critical as Water Cycle itself

22.3K views 16 3 1.6K

Qualify for future funding and incentives through Strategic Energy Management (SEM)

9.6K views 0 0 1.4K

One size doesn’t fit all: The value of a highly differentiated SCADA offer

16.4K views 49 1 3.0K

3-D Printing creating changes in Industrial Automation

18.7K views 10 3 2.5K

GUEST POST: Trends in the wireless automation market – Part 1

15.4K views 20 12 1.5K

Autonomous Cranes in the Steel Industry: A Revolution Waiting to Happen

3.3K views 2 1 150

Asset Reliability is the first step in your Asset Performance Management (APM) Strategy

3.2K views 5 0 127

The Reality of Augmented Reality: A View From Austmine 2019

3.2K views 5 0 124

Modernizing Emergency Shutdown Systems Step 2: Build Consensus

3.1K views 2 0 52

Innovation is both the key and the challenge to efficiency improvement

3.0K views 1 0 217

Navigating the changing tides of the US steel industry

2.9K views 1 1 200

Demystifying Industry 4.0

2.9K views 2 0 73

Predictive Analytics in Mining and Metals: Whose Prediction is the Right One?

2.8K views 6 3 158

Sustainability is not a Dirty Word in Oil and Gas Anymore – Improving Sustainability through Digitization

2.8K views 1 0 86

The future of manufacturing: How Schneider and Microsoft are partnering to address the opportunities and challenges of artificial intelligence

2.8K views 5 0 90

Integrated power and process systems help in improving human capital

2.8K views 1 0 76

5 Things to Know About Machine Control

2.8K views 1 0 111