Machine and Process Management

Maintaining industrial productivity can be costly without a good roadmap

17.6K views 30 1 1.8K

Avoiding cyber attacks: An inside look at industrial security fundamentals

24.8K views 49 7 2.7K

Are you ALERT or just waiting dear M2M machine

4.4K views 0 0 680

Situational awareness: Man vs Machine

5.0K views 0 0 929

Shortening preparation time and reducing downtime in the pasteurization/sterilization process by optimizing control loop design

15.8K views 23 1 2.2K

Technology and digitization: our industry lost a battle, but how do we win the war ?

20.6K views 121 72 4.6K

Grow Grow Grow !

4.3K views 0 0 833

Managing the unknown

20.1K views 30 1 1.9K

Optimizing the manufacturing “clean-in-place” processes can result in big savings and help ensure food safety

16.5K views 8 24 2.9K

Schneider Electric’s Acquisition of Invensys and what it means for our System Integrator Alliance Partners

25.2K views 98 130 4.1K

Building a company greater than the sum of its parts

21.2K views 116 104 3.0K

Integration of secure power into the management system is the end goal

29.0K views 37 3 1.5K

Why Advanced Connectivity Controllers are Helping OEMs to Unlock the Power of Big Data

4.0K views 2 0 115

Why Assuring Machine Safety Has Suddenly Gotten Easier for Machine Builders

4.0K views 2 1 151

Industrial management and efficiency with the most widely used tools

4.0K views 0 0 232

Predictive Analytics Pilots That Work

4.0K views 1 0 198
IIoT in Oil and Gas Refining

How Manufacturing Sector is Shedding its Weight with New-Age Industrial Tools

4.0K views 0 0 260

How Digitized Oil and Gas Asset Management is Improving Productivity and Lowering Costs

3.9K views 3 0 161

HMI and its implications in advanced process controls

3.9K views 0 0 220

Electrical motors and their modern day role in industries

3.9K views 6 0 213

AC/DC: Is the Digital Transformation Music to the Ears of the Steel Industry?

3.9K views 2 2 148
manufacturing

As Manufacturers Retool for the Industrial IoT, Machine Builders Can Help by Integrating Industrial UPSs 

3.8K views 3 0 142

New Collaboration Opportunity Bringing Together Digital Innovators and Experts

3.8K views 1 0 122

How to get on the road to Smart Machines: The ABC’s of control interface ergonomics

3.8K views 2 0 322