This audio was created using Microsoft Azure Speech Services
With a global population trajectory of 10 billion by 2050, and the majority concentrated in urban areas, studies are estimating that $3.3 trillion of investment will be needed in infrastructure annually through 2030. Given that buildings currently account for 40 percent of global energy consumption, a massive number of new buildings will have an equally massive impact on the environment.
In light of these predictions, it’s critical that we find ways to make buildings even more energy efficient than the greenest structures are today. In my last post, we looked at how Building Information Modeling (BIM) technology is greatly contributing to this effort by helping designers include energy modeling as part of the design workflow, as well as helping improve efficiency and reduce waste in all steps of construction.
In this post, we’ll have a closer look at what is still needed from all stakeholders – from equipment manufacturers to designers to owners – to make energy modeling even more accurate and repeatable, while also giving facility teams a dynamic tool for improving operational efficiency after a building is constructed.
Simulating building performance
BIM solutions provide a range of powerful tools to simulate the mechanical, electrical, and plumbing (MEP) performance of a building. However, Building Energy Modeling (BEM) is only offered by a few BIM providers as an integrated capability, while most BEM tools are only available as standalone applications. BEM tools typically help assess:
- Energy demand
- Indoor environmental quality
- Carbon dioxide emission
- Payback periods of energy saving measures
In doing so the BEM tool can help evaluate whether the building design will meet energy regulations or certifications, such as LEED, BREAM, etc. But it has the potential to go beyond the design stage by modeling control of the building in actual operation.
Today, most energy modeling occurs when a building design is nearing completion using a separate energy model. However, if the BEM tool is integrated within the BIM application and workflow, this energy analysis can occur as early as the concept stage, allowing for more informed design decisions.
More information for more accuracy
Energy modeling tools use a range of parameters to estimate the energy performance of a building. Some of this information – e.g. building envelope, zones, rooms, structure, equipment, control scenarios – can often come directly from the BIM system. However, for comprehensive energy modeling, a more detailed level of information on energy characteristics is needed.
As noted in my last post, a BIM model is made up of various categories of ‘objects’, which include each piece of equipment in the building. Objects can include different levels of detail, often provided by the equipment manufacturer, which needs to be in a format the specific BIM system can understand.
For effective energy modeling, the designer needs to include the right amount of information about each piece of equipment, including at the very least: power consumption, or heating and cooling capacity (for HVAC equipment). The challenge is that there has been no established global standard for defining energy-related properties, though some work has already been underway by separate organizations in some countries, such as France, Germany, and Australia.
Further complicating things is the fact that BIM design typically uses multiple tools, each with a different focus, from the BIM tool used for the building model, to tools used for structural and MEP models, to the separate BEM tool for energy modeling. This requires data to be transferred between the BIM and BEM models, which is more difficult when the tools are not integrated.
Standards exist that enable the extraction and sharing of data between BIM and BEM tools, including the Industry Foundation Classes (IFC) and Green Building XML (gbXML). However, these require a middleware conversion utility, and there is room for potential errors along the way.
Connecting building modeling to real performance
Finally, the energy modeling offered by most BEM tools today only takes into account ‘passive’ elements, whereas true energy efficiency estimation must also take into account active control scenarios and real energy usage data. This is not currently a common capability of BIM.
For its recently completed Technopole building in Grenoble, Schneider Electric partnered with Autodesk to use its Revit BIM platform as ‘the operating tools for tomorrow’s building.’ Beyond helping coordinating construction, the process helped the building achieve LEED Platinum certification. It is also intended to reproduce real energy behavior, with the BIM system eventually being connected to the operating data of the building. As such, the model will help execute augmented virtual tours, manage spaces, perform scheduling in connection with the building management system (BMS), monitor and manage energy, and perform predictive maintenance.
In summary, today’s BIM solutions are helping the AEC industry and building owners move toward increasingly efficient building designs. However, to inform better decisions for subsequent designs, greater levels of energy-relevant specifications are needed from equipment manufacturers, and a better bridge is needed between BIM and actual energy performance once a building is in operation. These challenges can be overcome, but require the active participation of all stakeholders. For more information on this topic, download the white paper “Bridging BIM and BEM: the path forward to more efficient building design and operations”.
CONTRIBUTOR:
Steve Butler is currently Senior Industry Strategy Manager for MEP at Autodesk, where he has worked in various capacities for the past 14 years. He has enjoyed a varied career in MEP engineering and design, working for consultants, contractors and manufacturers.
Conversation
Taju
5 years ago
Currently, I am working on research which is about BIM for the energy of infrastructure projects. I wanted more information about these topics and I’d appreciate any help.
Thanks!
Glen
4 years ago
Very useful
Bertrand Lack
4 years ago
Thank you very much, Glen!