Monitoring Building’s Energy Use – EE Standards and Regulations to Optimize Energy Performance

Understanding a building’s energy use is more than just good business sense – under a number of jurisdictions around the globe, it’s becoming the law. From the European Union to Japan, India and some U.S. states, regulations are going into place that are intended to reduce building-related emissions of carbon dioxide and other greenhouse gases. These new rules require building owners to become more aware of the energy performance of their buildings’ heating, cooling, lighting and other systems. As I describe in this post, these rules are driving growing demand for Power Metering and monitoring Devices (PMDs) complying with the International Electrotechnical Commission’s Standard IEC 61557-12, as specifiers seek solutions for meeting these rules.

European Union requirements

Two directives developed by the European Union (EU) are among the farthest-reaching, internationally. The European Union’s 2006 Energy Performance of Buildings Directive (EPBD) and 2012 Energy Efficiency Directive (EED), are now the law across most of Europe and the United Kingdom. The latter is especially comprehensive, with a set of binding measures to ensure EU member states use energy more efficiently throughout the value chain, from production to final consumption. Metering equipment can monitor consumption and help facilities establish both baselines and targets under continuous improvement projects.

Both directives can be mapped to standards that address methodologies for conducting audits, and installing monitoring and measuring systems. Under the EED, for example, companies must either perform facility-wide energy audits on a regular basis or set up an energy-management plan, as shown in Figure 1. Organizations maintaining such an energy-management system are exempt from annual audit requirements because, in essence, such benchmarking is built into their regular business processes.

Figure 1 – EPBD and EED directives

Other regions have their own requirements. These include the U.S. state of California, where the California Energy Commission’s recently enacted revisions to its Title 24 energy-efficiency standard – now require building owners to separately meter lighting, air conditioning and other building energy demands. PMDs complying with IEC 61557-12 can help meet this requirement.

Guiding standards for a number of other regions are outlined in Table 1.

Green Building Certification Influence
LEED EB O&M USA
Title 24 USA, California
BREEAM-In-Use UK
NF HQE Exploitation France
CASBEE Japan
DNGB for Existing Building Germany
IGTC, GRIHA India

Table 1 – Green Building certification

 

ISO 50001 (and its related set of standards as stated in Table 2) remains one of the most used standards to improve the Energy Efficiency of plants.

APPLICATION ASSESSMENT STANDARDS OR RULES METHODS STANDARDS PRODUCT STANDARDS

ISO 50001

Energy Management Systems – Requirements with guidance for use

ISO 50006

Energy Baseline (EnBs) & Energy Performance Indicators (EnPIs)

IEC 60364-8-1

Low voltage installations – Part 8-1: Energy Efficiency

EN 17267

Energy measurement and monitoring plan – Design and implementation – Principles for energy data collection

EN 50600-2-2

Information technology – Data center facilities and infrastructures – Part 2-2: Power distribution

Power Meters

IEC 61557-12

Power Metering and Monitoring devices (PMD)

See related posts:

Post1 Post2

Gateways, energy servers, data loggers

IEC 62974-1

Monitoring and measuring systems used for data collection, gathering and analysis –

Part 1: Device requirements

Table 2 – ISO 50001 related set of standards, as defined in IEC TR 63213

 

This set of standards can also be represented according to the design and operation phases, as shown in Figure 2.

Figure 2 – Relationship of selected standards and guidelines for building design and operations phases

If you are looking for more details, you can check out the following documents:

 

Theme Type Link
IEC TR 63213 Post IEC TR 63213: a Guide to Measuring applications on the supply and demand side
ISO 50001 ed 1 White Paper Recommendations for ISO 50001 compliance
White Paper Supplement Document to ISO50001 White Paper: Recommendations for Compliance
ISO 5001 ed 2 Post ISO 50001 Edition 2 Delivers More Clarity for Effective Energy Management
IEC 60364-8-1 Post IEC 60364-8-1 : Setting a New Standard for Efficient Buildings
EN 17267 Post Understanding the EN 17267 Standard That Helps You to make a “Planning to Energy Data Collection” as requested by ISO 50001
EN 15232 Post CO2 Reduction and Energy Performance – Setting the Standard for Building Automation with EN 15232
IEC 62974-1 Post Get the most of from your Energy Data with the IEC 62974-1 Standard and Ecostruxure Power

New options make metering easier

PMDs offer many advantages beyond power monitoring. They also can provide information on voltage, harmonics frequency – all critical factors in optimizing equipment efficiency and performance – along with remote load management. These functions are all accessible via dedicated touchscreen displays or via web browsers. Plus, in many cases, the panels’ integrated communications interfaces are ready to connect to existing energy-management platforms.

To learn more about Schneider Electric Smart Panels, please click here. Also, be sure to register for our Consulting Engineer portal for free access to additional tools, resources, and product information.

Tags: , , , , , , , , ,