How multi-voltage automatic transfer switches help electrical contractors avoid project delays

As power systems become more complex, one of the biggest opportunities to improve project execution is simplification. Electrical contractors are navigating compressed schedules, skilled labor shortages, evolving project requirements, and more complex electrical infrastructure. In that environment, each additional equipment variation can introduce another opportunity for specification errors, ordering mistakes, and installation challenges, leading to delays. Of course, delays mean added costs, lost productivity, and client dissatisfaction. Yet, something as simple as receiving an Automatic Transfer Switch (ATS) with the wrong voltage can put a project schedule at risk.

ATSs are the heart of power infrastructure for hospitals, commercial office buildings, education campuses, data centers, manufacturing facilities, and more. They deliver power resilience by selecting and accessing backup power sources to protect operations. ATSs also reconnect with the grid when power service is restored. But conventional single-voltage ATSs can have a downside.

The challenge with voltage-specific transfer switches

Speed matters, particularly for power system build-outs. Because subsequent phases of construction depend on power system completion, delays can have cascading effects that bring a project to a halt. Having the right ATS for the right voltage at the right time is critical for meeting deadlines.

But what if your distributor isn’t stocking the exact voltage-specific model? What if an ATS with the wrong voltage is delivered to the work site? What if a late-stage change means that the ATS you received no longer matches the project specification? Re-configuring an incorrect switch or obtaining a replacement can delay a project by days or weeks.

Multi-voltage transfer switches prevent delays

One of the most impactful ways contractors can mitigate delay risks is by adopting a multi-voltage strategy when procuring ATSs. A multi-voltage ATS provides all the functionality of a conventional transfer switch, without being limited to a single operating voltage. This one attribute—the ability to accommodate different operating voltages—reduces the risk of voltage mismatch between the ATS and the system it serves. For example, an electrical contractor orders a 208V ATS, but a late-stage change requires a 480V. With a conventional ATS, work may stop while a replacement is sourced, which can cause a domino effect in delaying other trades and commissioning. With a multi-voltage ATS, the electrical contractor can configure the voltage on site and keep the project moving.

Multi-voltage ATSs represent a major innovation in power system design and deployment, dramatically simplifying procurement and maximizing the probability that the correct model will be available. They also mitigate the risk of receiving an incorrect model because they can easily and quickly be reconfigured on the job site by your existing team.

The multi-voltage ATS built for faster project delivery

Contractors can reduce delay risks and streamline deployment with the ASCO 300 SERIES Multi-Voltage Power Transfer Switch. Field-configurable for most voltages from 208V to 480V, ASCO’s multi-voltage ATS enables electrical contractors to set the switch’s operating voltage onsite quickly and simply, before or during installation. Installers select the ATS’s operating voltage using simple, easy-to-access hardware controls—without waiting for a special technician or replacement switch. In minutes, your team can make the change and avoid days or even weeks of delays. And this can be done without powering the switch, so you won’t be left to discover a voltage mismatch only after powering an installed ATS.

Keep power projects moving forward

As power projects become more complex, the ability to simplify execution becomes a competitive advantage. Contractors can’t control every project variable, but they can reduce one of the most common causes of delays—voltage-specific equipment constraints. Multi-voltage ATS technology offers a more flexible approach, helping contractors quickly adapt to changing requirements. By leveraging the ASCO 300 SERIES Multi-Voltage Power Transfer Switch, contractors can remove unnecessary complexity, move faster, reduce risk, and enhance both scalability and resilience for their customers.

Frequently Asked Questions

What voltages can an ASCO 300 SERIES multi-voltage ATS be set to?

The ASCO 300 SERIES can be set to many voltages to meet project-specific needs, including 208, 220, 230, 240, 380, 400, 415, 440, 460, or 480 volts.

Does changing the voltage setting require special skills or technicians?

Selecting a voltage is accomplished through a simple and accessible dip switch located within the unit. It can be set by any qualified installer before or during installation.

Does the multi-voltage ATS need to be powered to select a voltage setting?

No. Unlike other multi-voltage ATSs, ASCO’s 300 SERIES Multi-Voltage ATS can be set without powering the unit. This has major advantages over competing models that auto-select voltage only after being powered up. If that auto-select feature fails, the project may be delayed until the issue can be corrected.

Add a comment

All fields are required.