AI factories driving economic growth though high-performance computing and AI manufacturing are becoming some of the world’s most energy-intensive facilities. What began as distributed server clusters has rapidly evolved into utility-scale loads demanding extreme uptime, tight power quality, and instant scalability.
For grid operators and data center owners alike, the question is no longer if the grid can keep up but rather how to scale rapidly and safely without compromising system stability. The answer is emerging in the form of a transformative strategy: Chip-to-Grid.
This approach reframes the electrical ecosystem as a single, continuous network stretching from high-voltage transmission infrastructure all the way down to the silicon powering AI workloads. By unifying how we model, analyze, and operate these interconnected layers, Chip-to-Grid planning unlocks a new era of reliability, precision, and growth.
This framework treats the electrical ecosystem as one continuous network, from transmission and substations to distribution, interconnection, and the facility’s on-site power system. By unifying how we model, plan, analyze, commission, operate, automate and comply across these layers, Chip-to-Grid planning enables faster decisions, lower risk, and more confident capacity expansion.
From point solutions to a platform strategy
The Chip-to-Grid vision championed by ETAP and NVIDIA moves far beyond incremental gains. Instead, it defines a physics validated blueprint built on:
- Accelerated computing
- AI-enabled decision-making
- High-fidelity electrical digital twins
Rather than solving isolated challenges, this integrated strategy modernizes the entire lifecycle of grid planning and operation. It is a long-term, scalable platform anchored in the GPU-accelerated libraries, now delivering up to 5X performance with NVIDIA cuDSS—and built on AI-ready infrastructure designed to grow in lockstep with the industry’s escalating power demands.

Carrying “engineering truth” from planning to operations
One of the most persistent challenges in power system engineering has been the disconnect between planning studies and real-time operations. Models developed during design often diverge from real operating conditions, thereby, limiting accuracy, slowing decision-making, and increasing risk.
ETAP Grid™ closes this gap.
By maintaining a live connection between the planning model and operational reality, ETAP Grid™ ensures that the “engineering truth” established early in the lifecycle remains consistent throughout ongoing operations. With synchronized, real-time visibility, grid teams can:
- Run high-fidelity what-if analyses
- Validate switching operations before execution
- Predict and mitigate risks
- Optimize performance at scale
This alignment is essential for managing the volatile and dynamic power behavior of modern AI workloads.
NVIDIA Omniverse DSX blueprint for AI factories
Modern AI factories require more than electrical schematics, rather they need a dynamic, real-world replica of an entire site. The NVIDIA OmniverseDSX blueprint enable by open standards including OpenUSD, allow for the development of digital twins of an AI factory to design and optimize for token production efficiency. Inside this environment:
- The full power system is modeled down to the rack and chip level
- Multi-domain interactions including thermal, mechanical, networking, and electrical are unified
- Teams can test configurations, resiliency strategies, and failure scenarios safely
At the heart of this environment, ETAP functions as the electrical backbone, providing the high-fidelity digital modeling required for accurate power flow analysis across the entire facility.
The future of energy management requires systems that can learn, adapt, and optimize in real time. ETAP Electrical Digital Twin brings this vision to life by merging real-time operational data with advanced AI assisted analytics.
Central to this capability are ETAP GPU-accelerated solver demonstrations, which show how software–hardware synchronization can yield massive performance improvements. Faster simulations enable teams to evaluate a wider range of scenarios, delivering deeper insight—and deeper insight means stronger system resilience. Not only has NVIDIA CUDA-X improved this capability significantly, but it also unlocks even more opportunity as we apply it to increasingly complex projects, pushing the boundaries of simulation depth, speed, and scalability.
A blueprint for the future
The AI era requires more than incremental improvements, it demands a reimagining of how we design, build, and operate the electrical infrastructure behind it. The Chip-to-Grid blueprint offers exactly that: a unified, intelligent, scalable approach to powering AI factories at the pace of innovation.
By combining accelerated computing, AI-driven insight, and precise digital twins, the industry now has a framework to deliver unprecedented reliability, operational clarity, and sustainable growth.
About the author

Tanuj Khandelwal, Chief Executive Officer – ETAP
Tanuj Khandelwal is the Chief Executive Officer of ETAP and has shaped and directed the development of ETAP’s solutions for over 20 years.
Before joining ETAP, he worked as an Associate Engineer at PricewaterhouseCoopers. A Senior Member of IEEE and co-chair of IEEE Standards 3002.2 & 3002.7, Tanuj is also a co-author of “Power System Dynamics with Computer-Based Modeling and Analysis” by Wiley publications and is the co-inventor of various ETAP technologies with 3 granted patents. Tanuj received his bachelor’s degree in Electronics and Telecommunications Engineering from University of Bombay in 1999 and his master’s degree in Electrical Engineering from California State University, Long Beach in 2001.
Add a comment