Discover our latest research, articles, and reports to understand how we’re helping to speed up a fair transition to net zero.

Discover more.

The synergy between digitization and sustainability: How mining and metals industries can benefit

Sustainability is back on top of the agenda in Mining & Metals. It is the “right thing to do”, but it is also driven by the need to respond to reputational crises, investor pressure and the evolving social license to operate.

The broadest and clearest definition says that sustainability focuses on meeting the needs of the present without compromising the ability of future generations to meet their needs. The concept of sustainability is composed of three pillars: economic, environmental, and social—also known informally as profits, planet, and people.

In very recent times, just a few examples of actions we have seen include:

Actions by major companies

Actions by investors

Actions by industry groups & researchers

  • The re-definition of the purpose of an organization to state shareholders no longer have primacy and are put on an equal footing with communities, workers, customers, and suppliers
  • The Responsible Steel initiative is building a standard whose mission is to give businesses and consumers globally the confidence that all steel has been sourced and produced responsibly at all levels of the supply chain, from raw materials suppliers to end users
  • Renewed academic work on the Circular Economy in Mining, first discussed on a Schneider Electric Blog in 2014

Sustainability + digital is the key

One of the key elements in sustainability today is the intersection of new digital capability with sustainability strategy. If the digital transformation and the sustainability transformation are aligned, it will enable movement in both the right direction and at an accelerated speed.

Let’s take energy and emissions for example. Some of the basic sustainability strategies are to improve energy efficiency, to use renewable energy sources and to manage the supply/demand dynamic via energy storage and load shedding. How does digital add more value? Two examples are process and energy analytics to determine the optimal energy operating point for process plants and microgrid optimization to forecast, schedule and execute when to store, produce, consume or sell energy from distributed energy resources.

Digital + sustainability framework

Generalizing, there are four parts of a digital + sustainability framework, from evolution to revolution:

  1. Be energy efficient – Improve energy efficiency by identifying and eliminating waste in energy usage and distribution
  1. Make the most of precious resources including water and valuable ore – Minimize resource waste by optimizing operations management processes
  1. Make the energy supply transition – Minimize scope 2 emissions by optimizing renewable power
  1. Zero carbon by design – New carbon zero processes eliminate scope 1 & 3 emissions
  • Replacement of gas and coal burning in processes by direct electric power or use of hydrogen

Taking a step-by-step approach, from evolutionary to revolutionary technologies, is a realistic strategy for the resources industry today. “Evolutionary technologies” exist and can easily be adopted today that can help cut emissions. While this is an important step to take, simply improving operational efficiencies and process optimization won’t be enough long term. “Revolutionary technologies” that act on decarbonization and circular economy are emerging and must eventually also be adopted.

Watch the panelists Innovation Talk “Sustainability at the Source: Getting it Right from the Start” where your industry peers discuss their sustainability strategies in a world where mining, steel and cement provide us with the essential raw materials we use in our everyday lives.

*Original blog was published September 2019 and has been updated December 2020.

Tags: , , , , , , , , , , ,