Open control meets intelligent motor management in water networks 

Water and wastewater operators are under pressure to do more with less. Aging infrastructure, rising energy costs, workforce shortages, stricter environmental compliance requirements, and increasing expectations for operational resilience are pushing utilities to rethink how pumping systems are designed and operated. However, modernizing operations does not always mean replacing existing control systems. 

For many utilities, a complete rip-and-replace approach is costly, disruptive, and impractical. Instead, the path forward lies in software-driven solutions that can operate across diverse hardware platforms, regardless of manufacturer. That’s why enabling utilities to modernize pumping operations with flexible, efficient, and resilient architectures is critical. Open, software-defined automation with intelligent motor management baked in helps operations maximize the value of existing assets while preparing for future challenges. 

Why pumping systems need a new approach 

Traditional pumping stations often rely on fragmented control systems, reactive maintenance practices, limited operational visibility, and proprietary architectures. These limitations create unnecessary downtime, higher lifecycle costs, inefficient energy consumption, and slower modernization projects. At the same time, motors remain the largest consumers of electrical energy, accounting for up to 80% of the total energy consumption, making motor management a strategic priority rather than a maintenance task. 

In Texas, when the City of Conroe’s population grew rapidly, delivering water without interruption became a challenge. EcoStruxure™ Automation Expert streamlined operations by simplifying data collection and regulatory compliance. It accelerated new water plant launches and supported a more resilient water system. 

As a result, the City of Conroe has seen a 70% increase in engineering efficiency and 80% faster recovery time after a system fault. This, along with the 24/7 reliable water service its residents need and expect. 

Open, software-defined pump stations: Flexibility built in

Open, software-defined pump station control introduces a hardware-agnostic, application-centric approach. Instead of tying critical control logic to a specific controller platform, the pump application can run on multiple hardware targets, including drive-embedded controllers, PLCs, RTUs, edge controllers, and industrial PCs. This makes modernization simpler and protects utilities from vendor lock-in. 

Pre-engineered pumping applications provide advanced functions such as anti-jam operation, overflow monitoring, clean-the-bottom routines, cavitation protection, automatic PID control, reservoir filling control, and booster station optimization. Utilities gain consistent operation across multiple sites while reducing engineering and commissioning effort. 

The motor management dimension 

While open, software-defined control optimizes process performance, Integrated motor management ensures the electrical and mechanical assets operate at peak reliability. Advanced motor management combines intelligent motor control centers, variable speed drives, digital diagnostics, predictive maintenance, power quality management, low harmonic solutions, and lifecycle services into a single architecture. 

The result is better asset performance, improved safety, enhanced energy efficiency, and faster recovery from faults. Predictive diagnostics help maintenance teams identify problems before failures occur, while digital monitoring provides continuous visibility into motor health and energy consumption. 

A powerful combination for water network applications

The greatest value emerges when these two approaches work together. Open, software-defined automation provides process intelligence at the pumping station level, while integrated motor management delivers intelligence at the equipment level. Together they create a connected, resilient pumping ecosystem with:

  • Reduced downtime through predictive maintenance and advanced diagnostics
  • Improved energy efficiency through optimized pump sequencing and variable speed control
  • Standardized engineering across lift stations, booster stations, and reservoir filling applications
  • Greater operational flexibility through hardware-independent automation architectures
  • Enhanced cybersecurity and easier IT/OT integration
  • Extended asset life through functions that reduce wear on pumps, valves, pipes, and motors

What this means for utility leaders

The benefits reach every level of the organization. Operations managers see fewer emergency callouts and more reliable service, while maintenance teams can focus on condition-based maintenance instead of firefighting failures. Engineering teams gain standardized, reusable applications that reduce project risk, and executives get clear progress toward sustainability, resilience, decarbonization, and cost goals.

Real outcomes beyond technology

Modern pumping solutions are no longer just about moving water. They are becoming digital platforms that combine automation, energy management, asset management, and operational analytics. Utilities that embrace software-defined control together with intelligent motor management can create a foundation for scalable digital transformation. This way, utilities maximize the value of existing infrastructure investments. 

Schneider brings together open, software-defined automation, intelligent motor management, energy expertise, and lifecycle services in a unified architecture for water and wastewater applications. 

By combining operational technology with digital innovation, Schneider helps utilities improve reliability, reduce energy consumption, simplify modernization projects, and support long-term sustainability goals. As water utilities prepare for the next generation of infrastructure challenges, success will depend on balancing operational efficiency, sustainability, reliability, and resilience. 

Open, software-defined pump station control delivers the flexibility and standardization required for modern operations. Meanwhile, integrated motor management delivers the intelligence and reliability required to keep critical assets performing. Together, they provide a practical roadmap toward smarter, more sustainable, and more resilient water and wastewater networks.

Add a comment

All fields are required.