Sometimes the safety systems that need to modernize the most are the ones that appear to need it the least. You know the ones—they’ve performed quietly and reliably for decades, protecting people, processes, equipment, and production without drawing attention to themselves.
That reliability deserves respect. Yet lifecycle status, supportability, and cybersecurity expectations can change long before a system fails. Plant teams need a clear view of their modernization options well before a constraint forces the issue. Urgency is also growing; there was a record 508 industrial control system advisories in 2025, underscoring the growing challenge of securing aging industrial systems.

Why a reliable safety instrumented system still needs modernization
Many safety instrumented systems (SIS) installed in the late 1980s and early 1990s continue to operate safely and reliably. That’s a credit to the engineering behind them. Still, it makes investment difficult to secure: when a system hasn’t caused an outage, why change it?
It’s a fair question. After all, legacy systems aren’t suddenly unsafe. But a more important question is whether their lifecycle status, support profile, cybersecurity capabilities, and long-term modernization path remain appropriate for the plant they serve.
Lifecycle policy helps customers answer that question. For example, a platform may remain eligible for repair or material exchange after it is no longer the preferred technology. Customers need to understand what support remains, what is becoming constrained, and how long they can reasonably rely on a given configuration.
The cybersecurity challenges of aging SIS platforms
Cybersecurity—from device to edge to cloud—is at the core of a connected future designed to drive efficiency and accelerate performance. Cybersecurity isn’t something you can add and forget. New vulnerabilities, advisories, and threat methods emerge continually. Modern safety platforms must be designed and maintained to address that changing environment, particularly where processors, communications cards, and other connected components are involved.
The stakes are material. The average cost of a data breach in the industrial sector is US $5.5 million. While this is a broad figure—not system intrusions specifically—it reinforces why cyber resilience has become an important part of lifecycle planning.
Older systems were engineered before many of today’s cybersecurity standards and practices existed. They may still perform their intended safety function, but they lack the cybersecure-by-design architecture and ongoing vulnerability-management capabilities a modern OT environment demands.
That doesn’t mean cybersecurity is the only reason to modernize. It is but one of several factors that a customer should evaluate alongside:
- Reliability
- Support costs
- Spares availability
- Compliance needs
- Maintenance burden
- Operational risk
- Timing of planned turnarounds
- Generations shifting and loss of expertise
Building a business case for SIS modernization
The most productive modernization conversations start with evidence, not alarm. Through a lifecycle assessment, a customer can:
- Review existing SIS infrastructure
- Identify each system’s lifecycle status
- Understand the availability of spares and support
- Evaluate the vendor’s upgrade technology
- Consider opportunities to improve reliability and compliance
Depending on the engagement, that assessment may also include cybersecurity and vulnerability considerations.
The result is a prioritized view of what needs attention and why, turning an abstract upgrade into an evidence-based case for risk reduction, cost avoidance, and business value.
That value may include:
- Reducing exposure to unplanned outages
- Resolving a known technical issue with an approved firmware or software update
- Improving supportability
- Preparing for evolving cyber expectations
- Aligning a safety-system modernization with a broader digital or operational initiative
How to plan SIS modernization around plant operations
Safety instrumented system modernization should be planned around a customer’s turnaround or shutdown schedule, making early assessment especially valuable. A well-developed roadmap gives operations, maintenance, engineering, IT, and management time to build consensus, define scope, secure funding, and select the right execution window.
Customers may consider an interim life-extension project, a phased upgrade, or a move to a new long-term platform. The right choice depends on:
- The age, condition, and lifecycle phase of the modules in the existing SIS
- Application, cybersecurity and functional safety requirements
- Operational constraints
- Long-term business value, including reliability, maintainability, cybersecurity, and lifecycle support, rather than purchase price aloneCreating a safety system modernization roadmap
Modernization decisions should also consider continuity. Some customers need to move beyond a legacy platform whose original supplier no longer provides a clear path forward. Others want to preserve the value of an existing installation while moving to the latest generation of technology.
For example, EcoStruxure™ Triconex supports its installed base through well-established generational migration paths, including fit-for-form replacement options for qualifying legacy systems. Drawing on decades of brownfield project experience, Schneider Electric™ helps customers transitioning from other legacy platforms develop migration strategies tailored to site-specific safety, operational, and turnaround priorities.
For organizations planning a longer-term modernization strategy, EcoStruxure Tricon CX offers a flexible and scalable foundation for safety and critical control applications across diverse operating environments. Designed to address evolving operational demands and cybersecurity expectations, the platform helps organizations enhance resilience while supporting long-term performance in critical industrial processes.
Choosing the right long-term SIS platform
A lifecycle assessment can help turn a complex technical decision into a practical modernization roadmap that balances safety, operational continuity, cybersecurity, and business value. It can:
- Confirm the lifecycle status, support profile, and spare-parts outlook for your installed SIS
- Assess reliability, cybersecurity, and compliance considerations alongside operational and maintenance priorities
- Identify the turnaround or shutdown window that could support a practical modernization plan
- Build the internal case around risk reduction, lifecycle value, and the benefits the modernized system can enable
Need to modernize your SIS? Read our seven-step eBook for building approval for safety-system modernization: Modernizing Safety Instrumented Systems.
Add a comment