What is intelligent motor management? | TeSys Tera

Intelligent motor management uses real-time motor data and predictive diagnostics to reduce unplanned downtime, optimize performance, and enable remote monitoring across industrial and commercial facilities.

Let’s break that down. In my years working alongside plant teams and system integrators, I’ve watched the same scene play out again and again: a production line jams up, an operator struggles to restart it, and a maintenance technician burns valuable hours hunting for the cause. Or a pump at a remote water facility quits without warning—and someone has to climb into a truck and drive out just to find out what went wrong.

These unplanned stoppages cost money, staff hours, and energy. And if you’ve ever run a facility, you know the worst part isn’t the failure itself, it’s not seeing it coming. What if you could predict potential failures before they occur?

Whether you’re a facility manager or system integrator, I believe an intelligent motor management system can save you time and improve efficiency. More than that, I think it changes the relationship teams have with their equipment—from reacting to whatever breaks to staying a step ahead of it.

Remote monitoring. Better productivity. TeSys Tera: Intelligent motor control.

The promise of a digital future

I’ve spent my career around industrial infrastructure, and I can tell you the pace of change right now is unlike anything I’ve seen before. Emerging technologies such as the internet of things (IoT) and AI are driving innovation in industrial operations and commercial buildings. Digitalization is a key trend, promising more efficiency through advanced analytics, as described in a recent Omdia white paper titled “Motor Management that Powers the Next Generation of Industrial Operations.”

In Omdia’s 2025 survey of machine builders and manufacturers,

  • Around 67% reported that digital transformation will have a high impact on machine performance in the next several years
  • 87% think digital technologies are “important” or “critically important” for operational efficiency
  • 91% have seen improvements in their motor management systems enabled by digitalization

But they also cite adoption challenges, such as:

  • Lack of in-house expertise
  • Integration with legacy equipment

It’s vital to engage the right partner with a track record of leadership and innovation in motor control and energy management.

Benefits of digital transformation according to survey respondents - 67% believe digital transformation will have a high impact on machine performance, 87% believe that it is important for operational efficiency, and 91% believe digitalization enables improvements in motor management. Adoption challenges include lack of in-house expertise and integration with legacy equipment.
Digital transformation improves machine performance, operational efficiency, and motor management, but lack of expertise and legacy equipment integration may pose challenges.

Traditional motor control limits efficiency

What I’ve come to believe is simple: when you can’t see what your motors are telling you, you’re competing on guesswork against teams who aren’t. That disadvantage rarely shows up as a single dramatic moment. It builds quietly, shut down by avoidable shutdown.

To sum up the situation, according to the white paper:

  • Fragmented data and limited system integration are major barriers to efficiency
  • Facilities often suffer from unreliable insights, reactive maintenance, and missed opportunities for energy savings
  • There is an urgent need for holistic, proactive, and intelligent systems that aggregate real-time and historical data across assets to drive smarter decisions

TeSys Tera: Intelligent motor management

For me, it all comes down to one word: visibility.

TeSysTM Tera is the next-generation motor management system from Schneider ElectricTM. It replaces TeSys T and modernizes motor monitoring, protection, and performance.

For years, the only way you knew a motor was failing was when it stopped and took a process down with it. TeSys Tera flips that. It gives every motor a way to tell you how it’s doing, so teams can act on real data instead of guesswork.

When paired with software like our EcoStruxureTM platform, this data empowers operators to:

  • Maximize uptime: Prevent shutdowns with predictive diagnostics
  • Be more productive: Improve motor performance and troubleshooting time
  • Improve sustainability: Monitor energy consumption and track sustainability KPIs
  • Reduce costs: Cut maintenance and operating expenses through advanced analytics
  • Monitor remotely: Save staff hours and reduce ineffective dispatches

TeSys: A century of innovation

I feel honored to be part of a legacy like this one. The TeSys brand represents more than a century of leadership in motor controls. With over 40 million TeSys controllers installed worldwide, we’ve learned a few things along the way—and that hard-won experience is exactly what we bring to helping you uplevel your motor management.

And if you’re a system integrator, I think you’ll appreciate how much complexity TeSys Tera takes off your plate:

  • Fewer parts to stock thanks to a modular, expandable design
  • Simplified PLC programming due to more onboard logic
  • Flexible installation options for new projects and retrofits

Integrate it into an existing motor control center (MCC), or have it pre-installed in a new intelligent motor control center (iMCC). 

But zoom out for a second, because this is the bigger picture I really want you to see: TeSys Tera is part of our vision for fully integrated power management systems, from the Schneider Electric motor controller portfolio and beyond. We support digital transformations by enabling:

  • Advanced diagnostics and waveform analysis
  • Custom dashboards and real-time alerts
  • Energy cost allocation and emissions tracking
  • Supports ISO 50001 energy management initiatives
Frequently Asked Questions

What is the difference between an intelligent MCC and a conventional MCC?

A traditional MCC requires physically wiring components to a PLC to turn motors off and on—you don’t know there’s a problem until a motor stops, halting a machine. Our iMCC reduces complex wiring and uses a single network cable for device communication, digitalizing operations. It enables real-time data and monitoring of equipment health to prevent problems before they cause downtime.

What is a smart motor controller?

This is one of many components housed in an iMCC. It provides traditional motor control functions like stopping and starting, as well as network communication for real-time data that enables predictive maintenance, advanced diagnostics, energy optimization, and other “smart” functions.

What are the advantages of an iMCC?

Digital communication enables real-time equipment health status, predictive maintenance, advanced diagnostics, energy use optimization, and remote monitoring and management. An iMCC reduces installation and programming time and complexity.  

Can I retrofit TeSys Tera into my current MCC? 

Yes, you can add TeSys Tera to an existing MCC. 

Intelligent motor management for a digital future 

Imagine the efficiency that’s possible with TeSys Tera: A technician monitors equipment on a smartphone. They do maintenance based on real-time data, reducing surprise shutdowns.  

Or a water facility monitors remote locations on a laptop. A pump stops suddenly, but they pinpoint the cause right away, so a technician arrives with the right knowledge and tools.   

That’s the future I’m genuinely excited to help build. TeSys Tera empowers you to improve operational efficiency now, and to be ready for whatever the next decade of industrial technology brings. That future is closer than you might think, and it starts with something simple: a clearer view of every motor you run. 

Add a comment

All fields are required.