Industrial plants today face pressures unlike any seen in decades. Nearly 44% of installed process control systems worldwide are more than 25 years old, creating a global modernization bottleneck as plants confront the energy transition, cybersecurity threats, workforce shifts, and the operational mandate to integrate AI. Traditional, hardware-defined distributed control system (DCS) architectures designed for a robust, stable, reliable environment are now among the most significant barriers to future-ready operations.
However, a new category of control system is emerging to break this bottleneck: the open, software-defined DCS. By decoupling proprietary control software from automation hardware, these systems give industrial plants the flexibility, interoperability, and future-readiness they need to modernize, improve efficiency, minimize cyber risk, and leverage AI at every level.

Why the traditional DCS model no longer fits
DCS systems were initially designed with proprietary foundations. Each system relied on vendor-specific controllers, networks, engineering tools, and HMIs. While this model delivered stability, it also created barriers that are increasingly difficult for plants to simplify processes and accel profitability. This is especially true as the industry heads toward data-driven operations, open ecosystems, AI-driven optimization, continuously evolving architectures and autonomous operations.
Challenges include:
- Vendor lock-in makes lifecycle cost higher and limits modernization options
- High architectural rigidity that slows new technology integration
- A steep learning curve for new engineers, most of whom are unfamiliar with legacy systems
- Complex maintenance requirements that strain aging workforces
- Limited interoperability with IT systems, cloud platforms, and smart devices
What’s driving the shift toward software-defined automation?
The shift toward software-defined automation is being driven by accelerating operational and economic pressures across process industries. Modernization cycles are tightening, project budgets are under greater scrutiny, and organizations need automation systems that can scale without locking them into long-term proprietary commitments. Workforce transitions further add urgency: new engineers expect modern development environments, simplified workflows, and tools that align with contemporary IT practices.
Digitalization initiatives expand the requirements placed on control systems and connectivity. Adoption of AI, predictive analytics, digital twins, and edge computing demand flexible compute models and open data access. Traditional systems can’t easily support these necessities that drive innovation. Licensors and EPC (engineering, procurement, and construction) companies face similar constraints when designing and building industrial facilities under compressed timelines and strict compliance requirements. They need solutions that reduce engineering effort, streamline commissioning, and minimize execution risk. Open, software-defined DCS models address these pressures by providing a more adaptable, open, and deployment-efficient foundation for modern operations.
Defining an open, software-defined DCS
At its core, an open, software-defined DCS decouples control software from the underlying hardware. This mitigates the issues with virtualization, which encapsulates old hardware instead of modernizing it. A virtualized system ties operations to a single vendor’s proprietary DCS stack. Inversely, an open, software-defined DCS allows plants to integrate best-of-breed hardware and software.
Instead of imposing proprietary vertical solutions, the same control runtime can run on multiple platforms (edge devices, industrial servers, or fit-for-purpose controllers) with a consistent engineering and operator experience. This shift unlocks capabilities that traditional systems cannot support, such as:
- Hardware independence: Plants are no longer tied to proprietary DCS hardware refresh cycles and can choose the hardware that best fits operational or financial requirements.
- A common runtime across platforms: The same runtime environment can execute on different hardware types, reducing errors and making engineering and deployment simpler and more scalable.
- Open, standards-based interoperability: Standard protocols to communicate with third-party equipment and software, eliminating custom, single-vendor integrations.
- Future-ready modernization: Designed to evolve in-step with technology like AI-driven optimization, IT integration, digital twins, advanced diagnostics, and flexible loops of innovation.
- Lower total cost of ownership: By removing rigid minimum infrastructures, simplifying network design, and reducing maintenance complexity, software-defined systems lower both CapEx and OpEx over time.
Why ‘open’ matters more than ever
In this context, “open” is a strategic enabler. For the modern plant, openness is essential for three reasons:
- Eliminates vendor lock-in: Closed systems force plants into expensive, proprietary upgrade paths. Open DCS architectures enable radical flexibility, reduce modernization effort, and give customers freedom of choice.
- Enables system-wide interoperability: Facilities depend on packaged units run by PLCs, energy management systems, safety instrumented systems, plant historians, MES and batch management software, analytics engines, and cloud services. An open DCS becomes the backbone of a connected plant.
- Achieves “secure-by-design” architectures: Cybersecurity is engineered into every layer: encryption, certificates, hardened devices, and compliance with standards such as IEC 62443.
What an open, software-defined future looks like
The DCS is not going away. Its role, ensuring safe, stable, high-availability control, remains fundamental. But the way DCS delivers that value is changing from:
- Proprietary to open
- Hardware-defined to hardware-agnostic
- Rigid architectures to adaptable ones
- Isolated control to deeply integrated IT-OT ecosystems
This makes plants more flexible, teams more capable, and modernization more practical.
A new chapter for industrial automation
The move toward open, software-defined automation is a technological shift, but it is also operational and strategic. It prepares industrial process plants for the next decade of challenges in cybersecurity, modernization, energy transition, and digital transformation.
This shift requires a new architectural foundation. Explore how Foxboro Software-Defined Automation (SDA) by Schneider Electric™ delivers openness, flexibility, and long-term resilience.
Add a comment