There is a paradox facing today’s industrial leaders. Many stand atop a mountain of data yet lack strategic insight. Globally, industrial segments will collect 4.4 zettabytes of data by 2030, more than double the 2023 total. Years of collecting operational technology (OT) data from sensors, machines, and production lines suggest the potential for predictive maintenance, energy efficiency, and autonomous operations. However, turning that data into insights and optimization opportunities can be challenging. The constraint is rarely analytics or ambition—it’s the strength of their OT data management foundation.
The missing link is not more analytics, but the infrastructure and approach required to make OT data usable beyond its original purpose. As a result, many industrial organizations are effectively data-rich and insight-poor: surrounded by operational data, yet unable to use it consistently at scale.
What is OT data?
OT data is the information generated by physical assets in operation, such as:
- Equipment states
- Process variables
- Events, alarms, and signals
Each describes how an industrial system behaves in real time. IT data is typically transactional and structured for business processes; OT data is continuous, heterogeneous, and often produced by assets that were never designed to broadly share information.
It may sound like nuance, but this distinction matters. In practice, organizations don’t actually “connect data,” they connect assets. Only once assets are connected can data be retrieved, contextualized, and reused. When OT data remains confined to individual machines or historians, its value is inherently limited.
Why OT data matters for industrial analytics
Industrial analytics depend on timely, contextualized, and reliable information about how operations perform. Yet much of the OT data collected today was designed for compliance, traceability, or basic monitoring, not for optimization.
Compliance-grade data answers questions such as whether a process stayed within acceptable limits or whether a batch met regulatory requirements. Analytics-grade data, by contrast, must support continuous analysis, comparison, and improvement. It requires different sampling rates, structures, and contextual information.
This gap explains why many analytics initiatives stall early. Organizations may have years of historical OT data yet still struggle to improve performance. The challenge is not the lack of data, but the lack of data that is ready for analysis.
The importance of OT data for AI
Artificial intelligence (AI) intensifies this challenge. While AI receives enormous attention, its success depends overwhelmingly on the quality and readiness of the data it consumes. In industrial environments, AI projects often fail or underperform not because of algorithmic limitations, but because OT data is incomplete, inconsistently structured, poorly contextualized, or difficult to access.
A common rule of thumb holds that 80% of an AI project is spent on data preparation. In that sense, AI is the finale, not the opening act. It magnifies existing data foundations; if OT data is not consistently modeled and exposed, AI becomes fragile, expensive, and difficult to scale. Rather than being the starting point, AI reveals whether an organization has done the foundational work required to make OT data usable across sites and use cases.
Why OT data management is mandatory for digital transformation
As digital ambitions grow from local analytics to enterprise-wide optimization, ad hoc approaches to OT data quickly reach their limits. Preparing data one use case at a time may work initially, but it does not scale.
A structured OT data management approach introduces consistency across sites, assets, and applications. It enables data to be reused, extended, and evolved over time rather than recreated repeatedly. This allows digital initiatives to move from experimentation to sustained industrial performance, aligning operations, engineering, and data teams around shared standards and objectives.
OT data collection infrastructure: The missing backbone
OT data collection infrastructure serves as the bridge between physical operations and digital ambition. It allows data to move reliably from assets to applications.
In practical terms, OT data readiness depends on at least four elements:
- Data availability
- Data access
- Data structuration and contextualization
- Data publishing
Together, these capabilities, supported by consistent software frameworks and operational methodologies, ensure that data can be retrieved from assets, structured consistently, and exposed in forms suited to different uses, including compliance, cybersecurity, analytics, and AI.
Without this backbone, digital initiatives remain isolated and difficult to scale. With it, organizations can absorb OT data from thousands of newly connected assets each year while maintaining consistency and control. Progress becomes incremental and measurable: assets are connected step by step, standards compound over time, and the value of data grows with every additional use.
Trustworthy OT data requires cybersecurity by design
As OT data pipelines expand (i.e., sensors and controllers at the edge, analytics, AI cloud applications), the integrity of that data becomes just as critical as its availability. Industrial data now flows across distributed devices, networks, and platforms that were never designed for open access or advanced analytics, increasing the risk of corruption, interception, or misuse. Embedding security into OT data collection and movement—protecting data at the edge, securing it in transit, and controlling access as it is shared—helps ensure that downstream analytics and AI are built on trusted, uncompromised information. In this way, cybersecurity is not a parallel initiative, but a foundational requirement for scaling industrial analytics, AI, and digital transformation with confidence.
Building foundations before acceleration
OT data readiness is not a one-time project, nor is it a “big bang” transformation. It is a sustained effort that rewards consistency and discipline, supported by strong internal alignment and effective data governance. Progress can be measured, expanded incrementally, and aligned with operational priorities.
Ready to design and execute OT data strategies that accelerate analytics, AI, and long-term performance? Visit our Industrial Digital Transformation Services and let us help you build a scalable OT data foundation.
About the author

Pierre Rol Milaguet
Marketing & Sales Engineer- Prosyst
Pierre has fourteen years of experience in sales and marketing, including twelve years with PROSYST, a French subsidiary of Schneider Electric. With a background in industrial engineering, he understands the technical aspects of his customers’ day-to-day operations and future challenges, allowing him to deliver high-value solutions with optimal ROI in automation standardization, machine simulation, and, increasingly, industrial data management.
About the author

Rafael Rossi
Industrial Digital Transformation Consulting Leader – Iberia & Middle East
Rafael is a global business transformation leader specializing in data management and data-powered innovation for industrial and utilities operations. With hands-on experience across Europe, the Americas, and the Middle East, he helps organizations boost efficiency, optimize energy consumption, and enable smarter decisions through digital transformation grounded in pragmatic data strategy and governance. As an Associated Researcher with the World Economic Forum (WEF) on Industrial Digitalization and Data Management, Rafael led development of the Industrial Data Management Maturity Index. Multilingual and educated at FIA Business School, he combines strategic vision and hands-on industry expertise to design scalable data architectures and governance that deliver measurable operational and energy outcomes in the Industry 4.0 era.
Add a comment