The holistic path: Designing water systems for the future

We live in an era where artificial intelligence can simulate entire universes, yet 2.2 billion people still lack access to safe drinking water. As industries push the frontiers of semiconductors, predictive algorithms, and digital infrastructure, a third of the global population remains without reliable access to one of life’s most fundamental necessities.

The paradox is striking: regions facing the most severe water stress are also those experiencing rapid population growth, industrial expansion, and the intensifying impacts of climate change. The question before us is not whether we have the technical capability to address these pressures, but whether we have the will to design water systems more holistically.

Water systems for the future
Designing water systems for the future requires us to take disconnected assets and reimagine them as an intelligent, adaptive system built on equity, access, and long-term resilience.

From assets to systems: The next era of water infrastructure

For our industry, this means rethinking the very way we manage water. We cannot continue treating it as a linear economy—extracted, treated, and discharged. We must steward it as a circular system—regenerated, reused, and reconnected. Water, sanitation, and environmental health are not separate silos; they are deeply interdependent outcomes of the choices we make in planning, infrastructure, and operations.

The technologies and tools are already at our disposal. Digital twins, advanced monitoring, smart treatment, and integrated data platforms are the enabling technologies already available. What’s lacking is true integration across utilities, sectors, and policy frameworks. To meet today’s challenges, the water sector must be reimagined—not as a collection of disconnected assets, but as an intelligent, adaptive system built on equity, access, and long-term resilience.

Seeing the whole picture: Why circular thinking matters for water systems

The problem with linear systems? They break under pressure. They assume steady supply and minimal disruption—assumptions we can no longer afford. Climate stress, rapid urbanization, and rising industrial water demand have exposed the limits of traditional water infrastructure. A truly circular approach treats water not as a one-time input, but as a resource that moves through multiple lifecycles—connecting drinking water, sanitation, wastewater treatment, green infrastructure, and the recovery of both nutrients and energy.

This also means addressing our blind spots. Take sanitation, for example: there is no right to water without safe, equitable access to it. And the same goes for clean green space and livable environments. These aren’t soft, secondary outcomes—they’re hard infrastructure. And they’re fundamental to human dignity.

Start with the data: The quickest win

“How do you manage the data?” is a deceptively simple question. Without good data, there is no visibility, no prioritization, no circularity. And yet many organizations are still flying blind on how to manage that data

It doesn’t take exotic tech—just intentional design. A robust data strategy that integrates operational performance, usage growth models, and future planning is a fast, achievable win for water systems. Add in a common data model, and you’ve created the conditions for teamwork across stakeholders, departments, and even borders. This common data model becomes a fundamental requirement to share context across processes, and throughout the lifecycle of water infrastructure.

Shoring up the foundations

Foundational improvements are often the most overlooked when it comes to quick efficiency wins. Take basic pump performance. If pumps aren’t optimized, they waste energy, inflate costs, and cannibalize capital that could otherwise be used to fund access, sanitation, or resilience upgrades. Variable speed drives (VSDs) are also an easy fix to implement. They’re proven to lower energy consumption, reduce wear, and increase reliability—yet many facilities still operate without them.

Solutions like Schneider Electric’s Altivar xxProcess Drive or EcoStruxure for Water and Wastewater make it easy to monitor, optimize, and automate pump systems in real time. These proven solutions are already in the field. But the most substantial obstacle is that the people responsible for implementing them are often so busy fighting fires that they can’t see the holistic approach. With a consolidated approach to sharing energy and process data, the biggest gains in pumping efficiency are easily identified, and these quick wins deliver the biggest returns with the least additional effort.

Tensions and trade-offs

Meanwhile, water demand is accelerating on both the technological and industrial fronts. Semiconductor fabs, AI data centers, and large-scale agricultural operations are often sited in regions already facing extreme water stress. These industries are critical, but without careful design and planning, they risk widening the gap between those with secure water access and those without.

Ironically, the force that accelerates water demand the most—artificial intelligence, whose models can gobble over 2 million liters per day—could also help mitigate it. When applied responsibly, AI can forecast demand, optimize distribution, and pinpoint maintenance needs based on risk and equity. For example, AI is being used to improve precision water use in agriculture, reducing water use and improving yields by up to 30%. But this requires a significant mindset shift: from AI as an efficiency engine to AI as a steward of shared resources. The efficacy of AI is directly linked to its access to quality and contextualized data. So, it all starts with that common data model that links data across silos and throughout the lifecycle.

Reclaiming capacity: From silos to stewardship

What utilities and planners need most isn’t just better tools—it’s breathing room. The water sector is overwhelmed. By embedding digital tools early in the design process and enabling their use throughout the infrastructure’s lifecycle rather than creating add-ons later, we can alleviate pressure, enhance decision-making, and achieve long-term savings. Schneider Electric is already helping partners do exactly that, building operational tools that incorporate design logic rather than just dashboards.

Water systems shouldn’t exist in silos. Neither should the people, plans, or technologies that support them. Integrating sanitation, green infrastructure, and water reuse into one data-driven ecosystem isn’t just possible—it is necessary.

Design like we know what’s coming—because we do

We can already map where water stress, population growth, and industrial expansion are colliding. The data is there. The question is whether we choose to act on it. And we don’t need to solve the whole system at once, but we do need to stop designing as if the parts are separate. The maps are clear. The warning signs are flashing, and the tools to do better already exist.

Active stewardship requires something from all of us:

  • Utilities and water operators: Ground decisions in data. Prioritize pump optimization and integrate circular design principles from the start—not as an afterthought.
  • Policymakers: Support the development of common data models and integrated planning frameworks.
  • Industry: Account for your water footprint. Commit to reuse, invest in monitoring, and adopt circular operations.
  • Everyone: Understand that water, sanitation, and environmental health are not separate issues—they are one interconnected conversation.

At Schneider Electric, we’ve seen how data-driven, integrated solutions can help utilities and industries move from reactive to proactive water stewardship. Discover how Schneider Electric is enabling partners to design water systems for the future.

Add a comment

All fields are required.