Energy bills have rarely dominated the conversation more than they do today. Whether it is the news, a chat with neighbours, or a quick look at your monthly statement, the pressure to reduce home energy costs has never felt more real or more urgent.
The good news is that reducing your energy bills does not have to mean sacrificing comfort. There are two core strategies for energy savings at home: using less energy overall or shifting when you use it to cheaper hours. When applied together and supported by the right technology – the impact on your bills can be significant.

Start with your tariff: The fastest energy savings win
One of the most overlooked opportunities for energy savings sits right inside your energy contract. Most homeowners have never fully examined which tariff they are on – and switching to a better-fit option can deliver savings before you change a single habit.
There are three main tariff types available to households today:
1. Flat tariff
A fixed rate for every unit of energy consumed, regardless of time of day. Even when demand on the grid is low and wholesale prices are cheaper, you pay the same rate. This predictability comes at a cost – it often means overpaying.
2. Variable (Time-of-Use) tariff
Energy prices vary throughout the day – higher during peak hours (typically daytime), lower during off-peak windows (late evening and early morning). Popular across Europe and increasingly common worldwide, this tariff rewards homeowners who can shift their consumption to cheaper hours.
3. Dynamic tariff
Prices change hourly in line with real-time grid demand – not just at pre-set peak and off-peak times. Common in markets like Norway, dynamic tariffs offer the greatest potential for energy savings, but they reward households that can respond flexibly. This is where smart home energy management technology makes a real difference.
If you are already on a variable or dynamic tariff, the next step is to make sure your home is actually taking advantage of those cheaper hours – automatically and intelligently.
The four big energy loads and how to manage them for savings
Four categories of electrical load account for the majority of energy consumption and therefore energy costs in most homes: heating and cooling, hot water, EV charging, and pool pumps. Managing these loads more intelligently, rather than simply using them less, is where the most meaningful energy savings are unlocked.

In a multiple-load home like this, truly optimising the usage is best done at property level, by integrating a home energy management solution (HEMS), which monitors data from the home using different types of sensors, and optimises load control with actuators.
Home Energy Intelligence: Automating your energy savings on EV charging and heating
Home energy intelligence is achieved thanks to a Home Energy Management System (HEMS) that orchestrates the energy-consuming devices throughout your home, monitors usage in real time, and automatically shifts loads to run during the cheapest available hours without any manual effort from you.
Solutions like Wiser by Schneider Electric, for example, automatically delay EV charging until off-peak tariff windows kick in, learn the thermal properties of your home to reduce unnecessary heating cycles, and schedule appliances around your lifestyle and energy prices.
The energy savings are tangible and measurable, delivering meaningful energy savings with zero inconvenience.
Consider a homeowner in France charging an EV with a 7kWh charger twice a week, for 5 hours each time – 70kWh of energy per week. Charging during peak hours at €0.246/kWh costs approximately €17.20 per week. Shift that same charge to off-peak hours at €0.183/kWh, and the weekly cost drops to €12.80 – a saving of €4.40 per week, or nearly €230 per year on charging alone.
Source: Schneider Electric / Wiser Energy

The same principle applies to heating. A HEMS like Wiser learns how well your home retains heat and optimizes heating cycles accordingly – keeping your home comfortable while calling for heat less often, reducing energy consumption without reducing warmth. Smart heating systems also learn your schedule and adjust automatically, reducing waste heating your home while you are away, while still maintaining your preferred temperature when at home.
Solar panels and battery storage: Generate your own cheap energy
Pairing rooftop solar with home battery storage fundamentally changes the energy savings equation. Rather than simply reducing what you draw from the grid, you generate your own energy during the day and store it for use in the evening. When integrated with a HEMS, the system automatically runs high-demand appliances – EV chargers, water tank heating when solar generation is at its peak, maximising self-consumption and reducing what you need to buy from the grid.
EV charging: Bi-directional can bring additional savings opportunity
Homeowners looking ahead are also exploring bidirectional (V2H) charging, which will eventually allow EV batteries to power the home during expensive peak periods, further reducing grid energy costs.
The future of home energy: AI is already here
The next generation of home energy management is already moving beyond scheduling and automation. AI-powered HEMS solutions now use predictive algorithms to anticipate peak pricing periods, adapt to changes in household behaviour in real time, and orchestrate energy intelligently across solar, battery storage, and appliances simultaneously. Homes using these systems are demonstrating reductions in overall consumption of 15–30% through smarter load management and peak pricing awareness.
Source: TechTimes — Smart Homes of the Future, December 2025
As this technology becomes more widely available, the gap between homes that are optimised for energy savings and those that are not will only grow wider
A practical roadmap for reducing your energy bills
If you are ready to start making meaningful energy savings at home, here is where to begin:
- Review your energy tariff – ask your supplier whether a variable or dynamic tariff could work for your household.
- Install a smart thermostat – a low-cost, high-impact first step that delivers energy savings quickly.
- Consider a HEMS – if you have an EV, solar panels, or significant heating costs, a Home Energy Management intelligence will orchestrate all of them autonomously.
- Explore solar and battery storage – assess whether your property is suitable; costs have continued to fall and payback periods have shortened.
- Look ahead to V2H – if replacing your EV, consider bidirectional charging compatibility for future energy savings.
Energy savings at home do not require dramatic lifestyle changes. With the right tariff, the right technology, and a system that works automatically in the background, it is possible to take genuine control of your energy costs and build a foundation for a more efficient, sustainable home.
To explore home energy management solutions like Wiser and understand how they could help you get the most from your tariff, visit our Home Energy Efficiency page.
Add a comment