Summer is peak solar season. But is it peak value?
For solar installers, summer represents the busiest and most rewarding time of the year. Systems are producing more energy than at any other moment.
But there’s a critical gap many installations still face:
Producing energy doesn’t automatically mean maximizing its value.
In fact, a significant share of residential solar energy is never used in the home. It’s exported to the grid instead of powering everyday needs.
That means missed savings for homeowners and missed opportunity for installers.
What’s the hidden challenge behind solar installations?
A typical home produces solar energy during the day, when the sun is strongest.

But consumption often happens later:
- In the evening
- At night
- When solar production has dropped
The result is a mismatch:
- Excess energy is sent to the grid
- The homeowner later buys electricity back
From installation to optimization
This is where the role of the installer evolves. Today, installing panels is only one part of the equation. Customers are increasingly looking for performance, savings, and simplicity. By integrating smart energy management, installers can transform a standard solar installation into a fully optimized energy system.
How Wiser Home helps optimize every installation
Wiser Home adds intelligence to solar systems by prioritizing self-consumption whenever this can be achieved without impacting homeowners’ comfort or energy needs.

Through Wiser Home AI, the system automatically favours the most cost-effective energy source. During summer, that means prioritizing solar energy that is generally more economically beneficial than exporting it to the grid and purchasing electricity later.
It automatically:
- Activates EV charging or water heating during the most cost-effective energy periods while ensuring homeowners’ needs are always met.
- Prioritizes the use of locally generated energy whenever consuming it is more financially beneficial than exporting it to the grid.
- Shifts flexible consumption to the lowest-tariff period when no solar surplus is available.
- Keeps consumption peaks within the home’s electrical capacity and contracted power limit to prevent power overloads and avoid tripping.
In practice, this means:
- Water heating and electric vehicle charging are automatically scheduled during the most cost-effective energy periods.
- Homeowners’ needs are always met.
- Electrical capacity limits are always respected, ensuring safety and continuity of power supply in the home.
More value for your customers
By maximizing self-consumption, Wiser helps homeowners:
- Reduce the amount of energy sent to the grid
- Increase the use of their own solar production
- Lower their electricity bills
In fact, optimizing solar usage during peak season can generate up to 37% in Germany and 33% in Denmark, both during summertime (Apr-Sept) for homes with dynamic tariffs (according to the savings simulations), additional savings compared to non-optimized consumption patterns
Instead of simply producing energy, their home becomes an intelligent system that uses it at the right moment.
A strong differentiator for your business
For installers, this creates a clear opportunity to stand out.
Adding Wiser to your offering allows you to:
- Deliver measurable added value to every project
- Move from installation to consultancy and optimization
- Position your business as future-ready
It also opens the door to:
- Higher-value projects
- Upsell opportunities
- Stronger customer satisfaction
A simple, scalable solution
Wiser Home is designed to integrate easily into residential installations and scale over time.
Wiser Home AI feature works with:
- Electric vehicle charging (Disclamier: “Compatible with Schneider Electric’s EV charger, Schneider Charge. Compatibility with additional brands will be available soon.”)
- Electric water heating systems
Its modular approach allows you to expand functionality as the home evolves, making it a long-term solution for both installers and homeowners.
Turn peak solar into real performance
Summer is when solar systems perform at their best. But without optimization, that performance is only partial.
By combining solar with smart energy management, you ensure that every installation delivers on its full promise:
- More efficiency
- More savings
- More value
Don’t just install solar. Maximize it.
This summer, go beyond installation and deliver smarter systems. Unlock more value for your customers and grow your business with solutions that make every watt count. Read more about it in the Be Energy Wise page.
Add a comment