Reduce your business running costs with KNX

Across Europe, there are approximately 12 million non-residential buildings, of which 84% are small buildings, many of them used by small and medium-sized businesses (SMBs). From convenience stores and office spaces to educational facilities, healthcare sites, hospitality venues, and wholesale and retail environments, these buildings form a critical backbone of Europe’s economy. In today’s fast-paced business environment, they all face mounting challenges- from fluctuating energy costs to the need for more efficient resource management and increasing regulatory pressure. 

Non-residential buildings are broadly distributed across sectors:  

So, it comes as no surprise that reducing business costs has become a top priority to stay competitive and ensure long-term sustainability, especially as SMBs can lack the time and money to streamline operations effectively when compared to larger businesses. When it comes to the running of the building, larger businesses are more likely to have facility managers and maintenance teams in-house to ensure the optimal running of the site, while SMBs are faced with two options: 

  1. Pay a monthly cost to appoint an external agency or business to handle building maintenance 
  2. Call out local tradesmen to deal with facility and equipment issues as and when they arise   

    With both options coming at a cost – both in terms of paying for the external service as well as any income lost from downtime while issues are dealt with – SMBs are more frequently looking towards technology that can be installed within the building to combat this and cut costs. Intelligent automation systems like KNX offer a solution for SMBs aiming to enhance efficiencies and reduce expenses in a variety of ways and can be easily managed by existing employees and business owners themselves.  

    Automation to reduce energy costs 

    Small to medium businesses have been some of the hardest hit by volatile energy costs and inflation, faced with a tough conundrum; do they increase the price of their products or services and pass the cost onto their customers, or do they absorb the impact?

    A report by the International Energy Agency found that Energy Management Systems can help businesses cut annual energy use by 10-17% by setting targets and tracking progress. 

    The SpaceLogic KNX system offers a wide range of control over various building functionalities, with the ability to automate key functions such as lighting, heating, and security. This centralised control not only ensures businesses can simplify operations and reduce the time and effort spent on managing different systems, but embracing automation technology is becoming an essential strategy for long-term cost savings and sustainability when it comes to energy management. 

    Automation through the KNX system can lead to substantial energy savings and improved sustainability. By optimising the control of lighting, HVAC, and other systems, KNX significantly reduces energy consumption, aligning with initiatives for net-zero energy buildings. This not only lowers utility bills but also supports corporate sustainability goals, enhancing the business’s reputation and appeal to environmentally conscious consumers and partners. 

    Fault detection 

    Fault detection and simplified maintenance are crucial aspects where the SpaceLogic KNX system excels. Thanks to its standardized protocol and interoperability, business owners can quickly identify and replace faulty components- often before a full breakdown occurs. This is reinforced by KNX’s decentralized architecture, where a single device failure does not impact the rest of the system, ensuring continuity of operations. In addition, built-in diagnostics, such as device status monitoring, offline detection, and cycle counting in actuators enable predictive maintenance by flagging wear and communication issues early. This significantly reduces downtime and maintenance costs, helping businesses maintain smooth and efficient operations. 

    Additionally, this is now a key mandate of the EPBD, requiring efficient fault detection and maintenance in buildings over 1,000 m², making it not just important, but essential for compliance. 

    Longevity and scalability 

    One of the standout features of the SpaceLogic KNX system is its backward compatibility. Products installed two decades ago are still compatible with current offerings, ensuring long-term usability and protection of investment. This feature is particularly beneficial for SMBs that may not have the resources for frequent system overhauls. This is the assurance that their investment will remain relevant and functional for years to come and it allows for a more strategic allocation of funds. 

    Interoperability is another key advantage of the system. As an open protocol used by over 500 manufacturers, KNX ensures that components from different brands work seamlessly together. This flexibility means that Schneider Electric products can seamlessly integrate with components from other brands without compatibility issues.  

    Building on this flexibility, SpaceLogic KNX is also highly scalable, making it suitable for both small installations like local restaurants to large projects such as stadiums or airports. This enables businesses to start with a tailored setup and expand over time, ensuring the system evolves with their needs without requiring complete overhaul. 

    KNX, the solution that helps SMBs save money 

    Operational efficiency is greatly improved by integrating various building control systems into a unified KNX network. KNX solutions, such as SpaceLogic KNX from Schneider Electric, allow users to manage and monitor all systems from a central point, simplifying building management tasks and improving response times to issues. This integration reduces the complexity of managing multiple standalone systems, leading to a more efficient and responsive operational environment. 

    Despite the upfront investment, the long-term benefits of KNX systems are clear. By reducing downtime, minimising maintenance needs, enhancing safety, and improving energy efficiency; businesses can achieve greater profitability. The initial costs are offset by the savings in operational expenses and the extended lifespan of the system, making KNX a robust and reliable solution for modern building automation. 

    For more information on Schneider Electric’s SpaceLogic KNX solutions for businesses, visit  the SpaceLogic KNX product page.

    Learn more about KNX through this brochure.

    Add a comment

    All fields are required.