How SMB’s can set and hit sustainability targets

For small and medium-sized businesses (SMBs), setting sustainability targets is more than a corporate social responsibility initiative, it’s a smart business strategy. With buildings responsible for 40% of global energy consumption and 33% of the world’s CO2 emissions, SMBs have a unique opportunity to drive meaningful change. Given their  share of buildings worldwide,  for instance in Europe where 84% of non-residential buildings are small buildings, the impact they can have on reducing carbon emissions is enormous. By aligning their operations with sustainable practices, SMBs not only contribute to global environmental goals but also enhance their long-term profitability. 

Why SMBs need sustainability targets 

SMBs are the backbone of our economy but often lack the resources and infrastructure that larger organisations have for sustainability initiatives. With rising energy costs and increasing regulatory pressure, such as the EPBD, tackling energy efficiency can feel daunting. Many rely on energy-intensive equipment like ovens and refrigerators, making bills a constant strain. However, improving energy use not only reduces costs but also cuts CO₂ emissions. By focusing on energy efficiency, SMBs can meet sustainability targets while boosting operational performance- a clear win-win. 

Then how do we tackle the energy challenge?

Buildings are one of the largest consumers of energy, with HVAC (Heating, Ventilation, and Air Conditioning) systems contributing to a significant portion of this consumption. For SMBs, HVAC can be particularly challenging. Many rely on residential-level solutions for their energy management, which are often inefficient and inadequate for their business needs. For example, these solutions often miss capabilities such as remote access, real-time monitoring, on-site data storage, and fault detection—controls that are essential for managing commercial spaces efficiently. As a result, businesses face wasted energy and higher operational costs. 

Fortunately, there are advanced building automation systems that are tailored to the specific needs of SMBs. They help businesses effectively monitor and control their energy consumption, particularly regarding HVAC systems, optimise performance and reduce operational expenses. 

Introducing SpaceLogic KNX—a smart solution for energy efficiency

KNX is an open protocol that allows different systems within a building—such as lighting, HVAC, and security—to communicate with one another, creating a unified energy management system. Unlike traditional, isolated devices, KNX solutions, such as SpaceLogic KNX from Schneider Electric, connects all systems into a single platform, allowing for real-time monitoring, automation, and control. 

For example, through intuitive, personalized visualizations accessible on a laptop or tablet, or directly via simple pushbuttons, businesses can easily manage heating, cooling, and lighting in their buildings. These systems can be operated either manually or automatically, depending on specific needs. Configured around operating hours, they help ensure that energy isn’t wasted when spaces are not in use. Powered by KNX sensors, the building can also respond automatically in real time, adjusting temperature and lighting based on occupancy to optimize comfort and efficiency. At the same time, owners and facility managers can monitor and fine-tune performance through these visual dashboards, maintaining full control. 

By using a solution like SpaceLogic KNX, SMBs can significantly reduce energy consumption, typically by up to 30%, while lowering their carbon footprint and energy costs. The system is scalable, making it easy for both small and medium-sized businesses that want to make incremental improvements over time. 

Practical steps for SMBs to set sustainability targets

Assess your energy usage 

The first step in setting sustainability targets is to understand where and how your business is consuming energy. Conduct an energy audit to identify inefficiencies, especially in HVAC systems, lighting, and other power-intensive equipment. 

Set measurable goals

Once you have a clear picture of your energy consumption, set specific, measurable goals. For example, aim to reduce your overall energy usage by 10% in the first year, or target a reduction in HVAC-related energy consumption by 15%. These targets should align with your overall business objectives. 

Invest in smart solutions

Technologies like SpaceLogic KNX can help you achieve your sustainability goals. By automating and optimising your energy usage, you can reduce waste and increase efficiency. KNX is not only energy-efficient but also future-proof, as it is fully backward compatible with previous installations, meaning it can evolve with your business needs. 

Leverage incentives

Many governments offer grants and incentives for businesses that invest in energy-efficient solutions. In Spain, EU-funded programs can cover 40–80% of renovation costs, including smart energy systems. In Germany, KfW schemes combine low-interest loans with repayment bonuses, while in France, programs like MaPrimeRénov’ can cover up to 90% of costs when combined with other incentives.1 

By leveraging these opportunities, SMBs can implement smart technologies such as KNX at a significantly lower upfront cost—accelerating both sustainability and ROI. 

Monitor and adjust

Achieving sustainability goals is an ongoing process. Use the data from your KNX system to monitor your progress and adjust as needed. Regularly reviewing your energy consumption will help you identify new opportunities for efficiency and ensure that you stay on track to meet your targets. 

Achieving long-term sustainability 

The benefits of setting and achieving sustainability targets go beyond energy savings. A more efficient building can improve employee comfort, enhance your company’s reputation, and even increase the value of your property. Additionally, as sustainability becomes more important to consumers and investors, having strong environmental credentials can give your business a competitive edge. 

Setting sustainability targets is not just about compliance or reputation—it’s about ensuring long-term business success. By investing in smart solutions like SpaceLogic KNX, SMBs can reduce their energy consumption, lower costs, and play a vital role in tackling the global climate crisis.

Know more about Spacelogic KNX.

1Sources

Add a comment

All fields are required.