You bought the smart thermostat. Maybe a voice assistant, a connected doorbell, and a set of app-controlled lights. On paper, your home is intelligent, but in reality, you’re managing four different apps, two incompatible hubs, and none of it integrates to work together. Sound familiar?

Across Europe, millions of homeowners are in exactly this position. Smart home device adoption has surged over recent years, but satisfaction has not kept pace. The reason is simple: we’ve been thinking about smart homes the wrong way.
The gadget-centric trap
For most of the past decade, ‘going smart’ meant adding individual devices to the home one at a time, from whichever brand was best rated or had a new launch at the time. The result? Homes that are technically connected.
This gadget-centric approach creates what engineers call ‘interoperability problems’, but what homeowners simply call frustration. Devices that don’t share data can’t make smart decisions together. A smart plug has no idea your heating has just come on. Your lighting scene doesn’t know if you’re in the room. Each device is ‘smart’ in isolation and collectively, they’re not intelligent at all.

More critically, none of this complexity has translated into the one thing most European households care about most right now, which is reducing energy consumption to combat rising energy costs.
Why energy bills are the real test of a smart home
European households have faced significant energy price volatility in recent years, with average electricity costs across the EU remaining well above pre-2020 levels. For homeowners, reducing energy bills is no longer a nice-to-have; it’s a genuine financial priority.
In fact, a survey by Schneider Electric found that nearly half (48%) of respondents cited energy efficiency as their foremost concern in light of recent global events, and 84% of people believed energy saving measures were the most important home improvement they could make in the future.

This is where the gap between gadget-centric and ecosystem-centric thinking becomes tangible. A single smart thermostat might trim 10-15% off your heating costs through its different features. But a genuinely integrated home energy system, one where your heating, hot water, EV charger, solar panels, and home battery all communicate through a single intelligent layer, can reduce household energy bills by up to 50-70%, according to Schneider Electric research.
That’s the difference between a smart device and a smart home.
The shift to ecosystem-centric thinking
The good news is that the industry has recognised this problem and is actively solving it. The shift happening right now is from devices that do things, to ecosystems that think and can make changes without even needing your manual input.
Two developments are accelerating this transition. First is Matter; backed by Apple, Google, Amazon and a host of manufacturers, it is creating a universal language for smart home devices, so products from different brands can finally work together reliably. Second, home energy management systems (HEMS) are emerging that treat your home as a single interconnected system, rather than a collection of independent gadgets.
At Schneider Electric, this is precisely the vision behind our HEMS approach. Rather than asking homeowners to manage complexity, the goal is for your home to automatically optimise energy use, prioritising renewable self-consumption to help you reduce energy bills without requiring you to become an electrical engineer.
What this looks like in practice
Imagine waking up on a cold February morning. Your HEMS, in this case our solution Wiser Home, already knows the overnight electricity tariff was lower, so it pre-heated the house at 3am. Your solar panels are generating power by 8am, which is being routed first to electrical devices and appliances in your home, then to your EV. Anything left over can either be sold back to the grid or could be used to pre-heat your hot water tank ready for the evening, so you don’t need to draw from the grid during peak hours.

You didn’t configure any of this. You just live in a home that’s been designed as an ecosystem from the ground up.
This is where residential buildings are headed. New builds across Europe are increasingly being designed with integrated electrical architectures , such as smart panels, connected wiring accessories, and energy management gateways, built in from the start, not retrofitted awkwardly after. This supports consumer attitudes towards housing construction, as our survey found that 74% believe new homes should be designed with sustainability in mind.
The future is already here
If your current smart home feels complicated, that’s not a reflection of the technology’s potential, it’s a reflection of where we’ve been. The transition from gadget-centric to ecosystem-centric smart homes is well underway, and for European homeowners currently navigating high energy bills and the push toward sustainable living, it cannot come soon enough.
The smartest thing your home can do isn’t turn the lights off when you leave a room. It’s eliminate the mental overhead of managing energy altogether and meaningfully reduce what you pay for it.
Add a comment