Safety in the Home: Why contractors should look beyond code compliance

Home electrification is accelerating. More homeowners than ever are investing in electric vehicles, induction stoves, heat pumps and smart systems to power their everyday lives.

While these technologies are transforming the comfort and efficiency of a property, they also increase the need for greater safety considerations, protection and energy reliance in the home.

While the National Electric Code (NEC) provides an essential foundation for electrical safety, code compliance alone only represents the minimum requirement for protecting people and property.

Many homes that technically ‘meet code’ may still be at risk from surges, overloads, or outdated equipment. As with any legislation, standards have evolved overtime and now include additional requirements to keep properties and people safe. There are millions of homes built after these changes, which may no longer be compliant.

This presents an opportunity for contractors to educate homeowners on these additional safety measures which may not be included in their homes but are increasingly installed as standard in newer build properties.

A skilled electrician installs recessed lighting in a new home during construction. He is wearing a safety helmet and vest according to code compliance.

What compliance covers – and what it misses

For contractors, code compliance means meeting baseline safety standards – protection from the most fundamental hazards like shock or fire.

However, meeting code doesn’t always mean a house’s electrical system is fully safe or achieving energy resilience.

Look out for the following safety gaps in homes, even ones that may have previously been code compliant.

Outdated electrical panels that are still operational but undersized for modern load requirements. According to Pelican Street, 48m single-family homes in the US may need panel upgrade to permit modern load demands.

Outlets or breakers that meet standards but lack advanced protection features. ESFI contractor surveys (2023–2024) show standard circuit breakers and fuses remain a large share of devices seen on service calls, while AFCI and dual-function breakers remain a smaller slice of what contractors encounter.

Uneven surge protection, as not all areas have adopted the latest Code requirements for home protection. Whole-house surge protection adoption is rising but not universal; the U.S. market was valued at roughly $0.96B in 2024 and is forecast to grow — indicating growing, but incomplete, penetration.

For contractors, the key takeaway is clear: by thinking beyond the bare minimum, they can deliver safer, smarter and more resilient electrical systems.

Barriers to advanced safety in the home

Despite the benefits of enhanced electrical safety, several factors can prevent homeowners from taking action:

Cost concerns: Some homeowners see advanced protection as an ‘extra’ rather than a necessary investment

Misconceptions: Many assume that meeting code automatically means total compliance. In fact, evolutions to the code means millions of homes may need upgrades to ensure their as safe and energy resilient as possible

Lack of awareness: Homeowners may simply be unaware of risks such as hidden surges or overloaded circuits Contractors can help bridge this knowledge gap by framing upgrades as essential protection, not as a ‘nice to have’ luxury. By acting as a homeowner’s trusted advisor, encouraging a culture of prevention – rather than reaction.

Safety beyond code: Key recommendations

We recommend the following for added home safety:

Panel and service upgrades: Older panels can conceal serious safety risks. Modern electrical panels provide larger capacity, more advanced breakers, and longer service life – ensuring that today’s electrified homes stay protected, even as their power demand grows.

Safer outlets: Replacing outdated outlets with advanced models – such as ground fault circuit interrupters (GFCI), tamper-resistant or smart outlets – extends safety through the home and can add remote access through various apps and voice command programs

Advanced breakers:  GFCI and Arc fault interrupters protect against ground and arc faults respectively, dramatically reducing fire and shock hazards. Even when not explicitly required by code, these technologies represent best practice for safety, efficiency and in the home.

Surge Protection Devices (SPDs): Whole-home surge protection defends against lightning strikes, grid fluctuations, and internal surges – safeguarding sensitive electronics and smart systems. For the modern home, SPDs are an essential solution for safety and promoting better energy resilience.  Today’s home has more electronic devices in them than ever before! Products such as appliances, TV’s / gaming consuls, and portable devices all need to be protected from transient surges.

Energy monitoring systems: Smart energy monitoring provides real-time visibility into household load patterns. In addition to identifying faults early, this insight can improve security awareness. For instance, if a garage door circuit draws power unexpectedly while occupants are away, or if key appliances activate outside normal usage windows, homeowners can receive alerts that prompt investigation or confirm activity within the property.

Portable power back-up: During outages, portable backup power helps keep critical systems running – such as medical devices, refrigeration units or home connectivity – offering an affordable layer of resilience without extensive retrofitting.

As mentioned previously, electrical contractors have an important role to play in promoting a preventative, rather than reactive, approach to safety. While smoke detectors and fire extinguishers address a problem once its underway, advanced breakers, GFCI outlets and SPDs help to safeguard against problems from occurring in the first place.

Safety beyond code: Key recommendations

Regular inspections and maintenance: Code does not require routine electrical inspections, but offering maintenance as a service helps homeowners stay proactive. Regular assessments allow contractors to identify wear, damage, or performance issues before they become dangerous.

Educating homeowners: Contractors can also promote safe habits—such as avoiding overloaded power strips, addressing tripped breakers promptly, and steering clear of DIY electrical repairs or unregulated online products. Education is a cornerstone of safety in the home.

Proper documentation: Maintaining up-to-date electrical records builds homeowner confidence and can even enhance property resale value by providing verifiable proof of safety upgrades.

Contractors as trusted advisors

Contractors are uniquely positioned to lead the conversation about safety in the home. By evaluating whether upgrades are needed, explaining the role of technologies like SPDs or smart breakers, and tailoring recommendations to each homeowner, contractors can position themselves as trusted advisors—not just installers.

This approach protects people, property, and professional reputation alike. In an era of rising electrical demand, the most successful contractors aren’t those who simply work to code — they’re those who work beyond it.

Add a comment

All fields are required.